<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: U-Boot Not Booting After Trying to Change Its Device Tree File Name in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/U-Boot-Not-Booting-After-Trying-to-Change-Its-Device-Tree-File/m-p/2080440#M236311</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Please copy&amp;nbsp;arch/arm/dts/imx8mp-evk-u-boot.dtsi to&amp;nbsp;arch/arm/dts/imx8mp-ifs-u-boot.dtsi and then try again.&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
    <pubDate>Tue, 15 Apr 2025 04:41:35 GMT</pubDate>
    <dc:creator>Zhiming_Liu</dc:creator>
    <dc:date>2025-04-15T04:41:35Z</dc:date>
    <item>
      <title>U-Boot Not Booting After Trying to Change Its Device Tree File Name</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/U-Boot-Not-Booting-After-Trying-to-Change-Its-Device-Tree-File/m-p/2079362#M236253</link>
      <description>&lt;P&gt;I am preparing to boot my custom board using the i.MX 8M Plus System on Chip (SoC) with Linux. To achieve this, I created a meta layer and established a custom-machine.conf file that builds upon the existing imx8mp-lpddr4-evk.conf. Additionally, I modified the SRC_URI variable in the u-boot-imx_2024.04.bbappend file to point to my GitHub repository, which contains the modified U-Boot source code based on the original u-boot-imx.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;In the initial stage of verifying that the new machine and U-Boot are functioning correctly, I copied or modified the files related to the i.MX 8MP EVK with minimal changes. I primarily changed the board name, addresses, and other necessary details to test its operation on the i.MX 8MP EVK. You can review all the modifications &lt;A href="https://github.com/PPKco/IFS-uboot/commit/e6f7168b9f328fc8dcf2b00bf338ce4740ebbc1d" target="_blank" rel="noopener"&gt;here&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I can successfully boot U-Boot on the evaluation kit (EVK) as long as no modifications are made to the custom_board_defconfig file, which is copied from imx8mp_evk_defconfig. However, when I attempt to change only the device tree name, U-Boot fails to boot on the EVK, and there is no output on the serial console.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The changes are as follows:&lt;BR /&gt;- &lt;STRONG&gt;CONFIG_DEFAULT_DEVICE_TREE&lt;/STRONG&gt;: Changed from "imx8mp-evk" to "imx8mp-ifs"&lt;BR /&gt;- &lt;STRONG&gt;CONFIG_DEFAULT_FDT_FILE&lt;/STRONG&gt;&lt;SPAN&gt;: Changed from "imx8mp-evk.dtb" to "imx8mp-ifs.dtb"&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 12 Apr 2025 06:48:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/U-Boot-Not-Booting-After-Trying-to-Change-Its-Device-Tree-File/m-p/2079362#M236253</guid>
      <dc:creator>Martiya</dc:creator>
      <dc:date>2025-04-12T06:48:41Z</dc:date>
    </item>
    <item>
      <title>Re: U-Boot Not Booting After Trying to Change Its Device Tree File Name</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/U-Boot-Not-Booting-After-Trying-to-Change-Its-Device-Tree-File/m-p/2080440#M236311</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Please copy&amp;nbsp;arch/arm/dts/imx8mp-evk-u-boot.dtsi to&amp;nbsp;arch/arm/dts/imx8mp-ifs-u-boot.dtsi and then try again.&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Tue, 15 Apr 2025 04:41:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/U-Boot-Not-Booting-After-Trying-to-Change-Its-Device-Tree-File/m-p/2080440#M236311</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2025-04-15T04:41:35Z</dc:date>
    </item>
  </channel>
</rss>