<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックCreating root fs</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Creating-root-fs/m-p/253505#M23628</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For a while I have been working with the rootfs provided by oneiric.tgz as supplied with the ubuntu distribution for the SabreSD board. I need to add my own files to the boot image namely, when I build the kernel I have noticed some of the modules are added to directories in /ltib/rootfs/ I have noticed that my rootfs folder is considerably smaller than the oneiric.tgz. How do I add the changes I made to the rootfs folder to oneiric.tgz. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I previously decompressed oneiric.tgz on my linux build system, copped the contets of rootfs over the top and re compressed the oneiric.tgz folder. This didn't work as the system was unbootable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Andrew&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 05 Apr 2013 17:47:52 GMT</pubDate>
    <dc:creator>andrewellis</dc:creator>
    <dc:date>2013-04-05T17:47:52Z</dc:date>
    <item>
      <title>Creating root fs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Creating-root-fs/m-p/253505#M23628</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For a while I have been working with the rootfs provided by oneiric.tgz as supplied with the ubuntu distribution for the SabreSD board. I need to add my own files to the boot image namely, when I build the kernel I have noticed some of the modules are added to directories in /ltib/rootfs/ I have noticed that my rootfs folder is considerably smaller than the oneiric.tgz. How do I add the changes I made to the rootfs folder to oneiric.tgz. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I previously decompressed oneiric.tgz on my linux build system, copped the contets of rootfs over the top and re compressed the oneiric.tgz folder. This didn't work as the system was unbootable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Andrew&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Apr 2013 17:47:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Creating-root-fs/m-p/253505#M23628</guid>
      <dc:creator>andrewellis</dc:creator>
      <dc:date>2013-04-05T17:47:52Z</dc:date>
    </item>
    <item>
      <title>Re: Creating root fs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Creating-root-fs/m-p/253506#M23629</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;what files are you trying to add? LTIB creates a filesystem and all pkgs are installed on ltib/rootfs folder. In the other hand, oneiric is an ubuntu filesystem, with different filesystem tree structure; if you need to install packages in Ubuntu, you need to use 'apt-get install' on the embedded device. In case you need to compile code, you need the developing tools (gcc, as, etc) and compile directly (no cross-compilation).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Leo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Apr 2013 15:33:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Creating-root-fs/m-p/253506#M23629</guid>
      <dc:creator>LeonardoSandova</dc:creator>
      <dc:date>2013-04-09T15:33:10Z</dc:date>
    </item>
    <item>
      <title>Re: Creating root fs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Creating-root-fs/m-p/253507#M23630</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Leo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I needed the video for linux modules, which were built as part of the kernel build. I have track them down and basically copied ltib/rootfs/lib/modules to my embedded system, and it seems to work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Andrew&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Apr 2013 16:25:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Creating-root-fs/m-p/253507#M23630</guid>
      <dc:creator>andrewellis</dc:creator>
      <dc:date>2013-04-09T16:25:04Z</dc:date>
    </item>
  </channel>
</rss>