<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Yocto Harpoon demo on eMMC</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Harpoon-demo-on-eMMC/m-p/2079376#M236257</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206442"&gt;@JosephAtNXP&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;Your suggestion was really useful. I am now able to get the demo working on the eMMC.&lt;/P&gt;&lt;P&gt;Thanks and best regards,&lt;/P&gt;&lt;P&gt;Khang.&lt;/P&gt;</description>
    <pubDate>Sat, 12 Apr 2025 16:18:15 GMT</pubDate>
    <dc:creator>khang_letruong</dc:creator>
    <dc:date>2025-04-12T16:18:15Z</dc:date>
    <item>
      <title>Yocto Harpoon demo on eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Harpoon-demo-on-eMMC/m-p/2074447#M235915</link>
      <description>&lt;P&gt;Hi Forum, CC &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206442"&gt;@JosephAtNXP&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;Recently, I was able to run the &lt;A href="https://community.nxp.com/t5/i-MX-Processors/iMX8MP-EVK-Unable-to-launch-jailhouse-mode-with-Yocto-Harpoon/m-p/2074315" target="_self"&gt;Harpoon demo on the iMX8MP-EVK&lt;/A&gt; as well as &lt;A href="https://community.nxp.com/t5/i-MX-Processors/Yocto-Harpoon-for-iMX8MN-custom-board/m-p/2073731" target="_self"&gt;an iMX8MN based custom board&lt;/A&gt;. Both require that the yocto harpoon image to be flashed to and executed from the micro-SD card.&lt;/P&gt;&lt;P&gt;I would like to have you advice on what should be done/modified in order to run the harpoon demo on the eMMC, please ?&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Khang&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 04 Apr 2025 18:31:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Harpoon-demo-on-eMMC/m-p/2074447#M235915</guid>
      <dc:creator>khang_letruong</dc:creator>
      <dc:date>2025-04-04T18:31:23Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto Harpoon demo on eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Harpoon-demo-on-eMMC/m-p/2075477#M236011</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products,&lt;/P&gt;
&lt;P&gt;You would need to flash the image (the one you copy using dd CLI command) to eMMC, you can do it using UUU, &lt;A href="https://github.com/nxp-imx/mfgtools" target="_self"&gt;download latest release&lt;/A&gt; and decompress the image until you have a .wic image (instead of .wic.zst).&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;$ sudo uuu -b emmc_all &amp;lt;image&amp;gt;.wic
&amp;gt; uuu -b emmc_all &amp;lt;image&amp;gt;.wic&lt;/LI-CODE&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Mon, 07 Apr 2025 22:14:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Harpoon-demo-on-eMMC/m-p/2075477#M236011</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2025-04-07T22:14:10Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto Harpoon demo on eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Harpoon-demo-on-eMMC/m-p/2075531#M236014</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206442"&gt;@JosephAtNXP&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;I know perfectly how to flash to and boot from the eMMC. Also, you might have noticed that I tested with both &lt;A href="https://community.nxp.com/t5/i-MX-Processors/iMX8MP-EVK-Unable-to-launch-jailhouse-mode-with-Yocto-Harpoon/m-p/2074441" target="_self"&gt;iMX8MP-EVK&lt;/A&gt; and our &lt;A href="https://community.nxp.com/t5/i-MX-Processors/Yocto-Harpoon-for-iMX8MN-custom-board/m-p/2074442" target="_self"&gt;custom iMX8MN-based board.&lt;/A&gt; They work very well with normal Linux (without jailhouse mode).&lt;/P&gt;&lt;P&gt;I found the &lt;A href="https://community.nxp.com/t5/i-MX-Processors/Harpoon-amp-eMMC/m-p/1828265" target="_self"&gt;following discussion about Harpoon and eMMC&lt;/A&gt; confirming the limitation.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;K.&lt;/P&gt;</description>
      <pubDate>Mon, 07 Apr 2025 23:57:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Harpoon-demo-on-eMMC/m-p/2075531#M236014</guid>
      <dc:creator>khang_letruong</dc:creator>
      <dc:date>2025-04-07T23:57:36Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto Harpoon demo on eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Harpoon-demo-on-eMMC/m-p/2078608#M236199</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/147542"&gt;@khang_letruong&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;You are right, usdhc3 interface is disabled in &lt;A href="https://github.com/nxp-imx/linux-imx/blob/37d02f4dcbbe6677dc9f5fc17f386c05d6a7bd7a/arch/arm64/boot/dts/freescale/imx8mp-evk-root.dts#L80" target="_self"&gt;8MP&lt;/A&gt; and &lt;A href="https://github.com/nxp-imx/linux-imx/blob/37d02f4dcbbe6677dc9f5fc17f386c05d6a7bd7a/arch/arm64/boot/dts/freescale/imx8mn-evk-root.dts#L90" target="_self"&gt;8MN&lt;/A&gt;, you could patch NXP BSP (the linked files) but the added layer would be in lower layers than Harpoon.&lt;/P&gt;
&lt;P&gt;The best option is to act upon Harpoon layer, either in the &lt;A href="https://github.com/NXP/meta-nxp-harpoon/blob/ef1e2b0f2c976d4a0e8dc2ccea3b283611755c04/recipes-kernel/linux/files/0016-arm64-dts-imx8m-m-n-p-evk-add-harpoon-device-tree-fo.patch#L105" target="_self"&gt;patch that includes such DTS&lt;/A&gt; from NXP BSP or create another patch as this one enabling usdhc3. You could quickly confirm enabling the node in that patch and rebuilding.&lt;/P&gt;
&lt;P&gt;Keep in mind that you cannot do that on EVK, but on your custom board.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 10 Apr 2025 20:23:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Harpoon-demo-on-eMMC/m-p/2078608#M236199</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2025-04-10T20:23:57Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto Harpoon demo on eMMC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Yocto-Harpoon-demo-on-eMMC/m-p/2079376#M236257</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206442"&gt;@JosephAtNXP&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;Your suggestion was really useful. I am now able to get the demo working on the eMMC.&lt;/P&gt;&lt;P&gt;Thanks and best regards,&lt;/P&gt;&lt;P&gt;Khang.&lt;/P&gt;</description>
      <pubDate>Sat, 12 Apr 2025 16:18:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Yocto-Harpoon-demo-on-eMMC/m-p/2079376#M236257</guid>
      <dc:creator>khang_letruong</dc:creator>
      <dc:date>2025-04-12T16:18:15Z</dc:date>
    </item>
  </channel>
</rss>