<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Enabling console using LPUART8 for imx93</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Enabling-console-using-LPUART8-for-imx93/m-p/2076509#M236073</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;All your changes are correct, you're missing some configuration for the clock to be enabled on the peripheral, since at boot time this is not being on by default.&lt;BR /&gt;&lt;BR /&gt;at /arch/arm/mach-imx/imx9/native/clock.c&amp;nbsp;&lt;BR /&gt;in&amp;nbsp;mxc_get_clock(enum mxc_clock clk) function add:&lt;BR /&gt;return ccm_clk_root_get_rate(LPUART8_CLK_ROOT);&lt;BR /&gt;&lt;BR /&gt;in void init_uart_clk(u32 index) function add:&lt;BR /&gt;case LPUART8_CLK_ROOT:&lt;BR /&gt;&amp;nbsp;/* 24M */&lt;BR /&gt;&amp;nbsp;ccm_lpcg_on(CCGR_URT8, false);&lt;BR /&gt;&amp;nbsp;ccm_clk_root_cfg(LPUART8_CLK_ROOT, OSC_24M_CLK, 1);&lt;BR /&gt;&amp;nbsp;ccm_lpcg_on(CCGR_URT8, true);&lt;BR /&gt;&amp;nbsp;break;&lt;BR /&gt;&lt;BR /&gt;Also at&amp;nbsp;/board/freescale/imx93_evk/imx93_evk.c&lt;BR /&gt;in function&amp;nbsp;int board_early_init_f(void) add:&lt;BR /&gt;init_uart_clk(LPUART8_CLK_ROOT);&lt;BR /&gt;&lt;BR /&gt;This changes have been made and tested by a colleague and are working correctly on the EVK.&lt;BR /&gt;&lt;BR /&gt;Best regards/Saludos,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
    <pubDate>Tue, 08 Apr 2025 23:18:02 GMT</pubDate>
    <dc:creator>AldoG</dc:creator>
    <dc:date>2025-04-08T23:18:02Z</dc:date>
    <item>
      <title>Enabling console using LPUART8 for imx93</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Enabling-console-using-LPUART8-for-imx93/m-p/2073770#M235849</link>
      <description>&lt;P&gt;Hi team,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;I'm trying to boot a board which uses&lt;STRONG&gt; LPUART8&lt;/STRONG&gt; as console but &lt;STRONG&gt;LPUART1&lt;/STRONG&gt; default console in i.MX93 EVK kit. So I had done the changes in &lt;STRONG&gt;u-boot dts, linux-imx dts,imx93_evk.c and&amp;nbsp;imx93_evk.h&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;But unable to watch serial logs and same I checked using EVK kit&lt;STRONG&gt; J1001 header pin32&amp;amp;33&lt;/STRONG&gt; which are ALT modes of LPUART8. This configuration also doesn't work. Please let me know the changes need to be applied and also let me know the path.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Robbi&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 03 Apr 2025 13:56:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Enabling-console-using-LPUART8-for-imx93/m-p/2073770#M235849</guid>
      <dc:creator>Robbi</dc:creator>
      <dc:date>2025-04-03T13:56:29Z</dc:date>
    </item>
    <item>
      <title>Re: Enabling console using LPUART8 for imx93</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Enabling-console-using-LPUART8-for-imx93/m-p/2074969#M235942</link>
      <description>Please help on this issue modified all paths.</description>
      <pubDate>Mon, 07 Apr 2025 08:31:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Enabling-console-using-LPUART8-for-imx93/m-p/2074969#M235942</guid>
      <dc:creator>Robbi</dc:creator>
      <dc:date>2025-04-07T08:31:15Z</dc:date>
    </item>
    <item>
      <title>Re: Enabling console using LPUART8 for imx93</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Enabling-console-using-LPUART8-for-imx93/m-p/2075536#M236015</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Could you share the changes you have made, so I could check those are made correctly?&lt;BR /&gt;Also, please share the Linux version you are working with.&lt;BR /&gt;&lt;BR /&gt;Best regards/Saludos,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Tue, 08 Apr 2025 00:18:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Enabling-console-using-LPUART8-for-imx93/m-p/2075536#M236015</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2025-04-08T00:18:32Z</dc:date>
    </item>
    <item>
      <title>Re: Enabling console using LPUART8 for imx93</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Enabling-console-using-LPUART8-for-imx93/m-p/2075717#M236030</link>
      <description>&lt;P&gt;Thanks&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/171173"&gt;@AldoG&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; For the response, i.MX93 EVK uses LPUART1 as default console port, but as my custom board is configured for LPUART8. I need to change my console from LPUART1 to LPUART8 and check in Header J1001. For that the modifications I had done:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;U&gt;u-boot-imx:&lt;/U&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Added lpuart8 node and disabled lpuart1 along with iomux.&lt;/LI&gt;&lt;LI&gt;changed&amp;nbsp;"console=&lt;STRONG&gt;ttyLP7&lt;/STRONG&gt;,115200 earlycon\0" \ from ttyLP0" in /configs/imx93_evk.h file.&lt;/LI&gt;&lt;LI&gt;Added&amp;nbsp;&lt;DIV&gt;static iomux_v3_cfg_t const uart_pads[] = {&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;// MX93_PAD_UART1_RXD__LPUART1_RX | MUX_PAD_CTRL(UART_PAD_CTRL),&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;// MX93_PAD_UART1_TXD__LPUART1_TX | MUX_PAD_CTRL(UART_PAD_CTRL),&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;STRONG&gt;&amp;nbsp; &amp;nbsp; MX93_PAD_GPIO_IO13__LPUART8_RX | MUX_PAD_CTRL(UART_PAD_CTRL),&lt;/STRONG&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;STRONG&gt;&amp;nbsp; &amp;nbsp; MX93_PAD_GPIO_IO12__LPUART8_TX | MUX_PAD_CTRL(UART_PAD_CTRL),&lt;/STRONG&gt;&lt;/DIV&gt;&lt;DIV&gt;}; in&amp;nbsp;/imx93_evk/imx93_evk.c file.&lt;/DIV&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;STRONG&gt;&lt;U&gt;linux-imx:&lt;/U&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Added lpuart8 node and disabled lpuart1 along with iomux.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;U&gt;imx-atf:&lt;/U&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;changed IMX_LPUART_BASE&amp;nbsp;&amp;nbsp;U(0x426a0000) from&amp;nbsp;&amp;nbsp;U(0x44380000) in&amp;nbsp;/include/platform_def.h file.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;meta-fresscale:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;changed&amp;nbsp;SERIAL_CONSOLES = "115200;ttyLP7" in&amp;nbsp;/conf/machine/imx93-11x11-lpddr4x-evk.conf which includes header&amp;nbsp;/conf/machine/include/imx93-evk.inc file.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;U&gt;optee-os:&lt;/U&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;changed set(CFG_UART_BASE UART1_BASE) to&amp;nbsp;set(CFG_UART_BASE UART8_BASE).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For more info add zip folder which contains images of changes done. Please go through it and let me know update.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Robbi&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;&lt;P&gt;Robbi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 08 Apr 2025 04:30:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Enabling-console-using-LPUART8-for-imx93/m-p/2075717#M236030</guid>
      <dc:creator>Robbi</dc:creator>
      <dc:date>2025-04-08T04:30:49Z</dc:date>
    </item>
    <item>
      <title>Re: Enabling console using LPUART8 for imx93</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Enabling-console-using-LPUART8-for-imx93/m-p/2076509#M236073</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;All your changes are correct, you're missing some configuration for the clock to be enabled on the peripheral, since at boot time this is not being on by default.&lt;BR /&gt;&lt;BR /&gt;at /arch/arm/mach-imx/imx9/native/clock.c&amp;nbsp;&lt;BR /&gt;in&amp;nbsp;mxc_get_clock(enum mxc_clock clk) function add:&lt;BR /&gt;return ccm_clk_root_get_rate(LPUART8_CLK_ROOT);&lt;BR /&gt;&lt;BR /&gt;in void init_uart_clk(u32 index) function add:&lt;BR /&gt;case LPUART8_CLK_ROOT:&lt;BR /&gt;&amp;nbsp;/* 24M */&lt;BR /&gt;&amp;nbsp;ccm_lpcg_on(CCGR_URT8, false);&lt;BR /&gt;&amp;nbsp;ccm_clk_root_cfg(LPUART8_CLK_ROOT, OSC_24M_CLK, 1);&lt;BR /&gt;&amp;nbsp;ccm_lpcg_on(CCGR_URT8, true);&lt;BR /&gt;&amp;nbsp;break;&lt;BR /&gt;&lt;BR /&gt;Also at&amp;nbsp;/board/freescale/imx93_evk/imx93_evk.c&lt;BR /&gt;in function&amp;nbsp;int board_early_init_f(void) add:&lt;BR /&gt;init_uart_clk(LPUART8_CLK_ROOT);&lt;BR /&gt;&lt;BR /&gt;This changes have been made and tested by a colleague and are working correctly on the EVK.&lt;BR /&gt;&lt;BR /&gt;Best regards/Saludos,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Tue, 08 Apr 2025 23:18:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Enabling-console-using-LPUART8-for-imx93/m-p/2076509#M236073</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2025-04-08T23:18:02Z</dc:date>
    </item>
    <item>
      <title>Re: Enabling console using LPUART8 for imx93</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Enabling-console-using-LPUART8-for-imx93/m-p/2076727#M236085</link>
      <description>&lt;P&gt;Thanks&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/171173"&gt;@AldoG&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; It is working now. Is &lt;STRONG&gt;i.mx93 Image compactible for imx91&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Robbi.&lt;/P&gt;</description>
      <pubDate>Wed, 09 Apr 2025 06:00:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Enabling-console-using-LPUART8-for-imx93/m-p/2076727#M236085</guid>
      <dc:creator>Robbi</dc:creator>
      <dc:date>2025-04-09T06:00:27Z</dc:date>
    </item>
    <item>
      <title>Re: Enabling console using LPUART8 for imx93</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Enabling-console-using-LPUART8-for-imx93/m-p/2077306#M236129</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Glad that it is working now, regarding image compatibility I would say no, since even if the processor is practically a downgrade of the other it would require to create your own image for the i.MX91 but you may reuse almost all of your changes.&lt;BR /&gt;&lt;BR /&gt;Best regards/Saludos,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Wed, 09 Apr 2025 16:49:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Enabling-console-using-LPUART8-for-imx93/m-p/2077306#M236129</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2025-04-09T16:49:55Z</dc:date>
    </item>
    <item>
      <title>Re: Enabling console using LPUART8 for imx93</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Enabling-console-using-LPUART8-for-imx93/m-p/2395691#M246008</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/171173"&gt;@AldoG&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;We are also using LPUART8&lt;/P&gt;&lt;P&gt;the issue is when we enable optee debug board hangs does not bootup, CFG_TEE_CORE_LOG_LEVEL=3&lt;/P&gt;&lt;P&gt;U-Boot SPL 2024.04 (Mar 27 2026 - 04:41:39 +0000)&lt;BR /&gt;SOC: 0xa1009300&lt;BR /&gt;LC: 0x2040010&lt;BR /&gt;PMIC: Over Drive Voltage Mode&lt;BR /&gt;Vx read count(2728) is greater than Vx threshold(1763) continue booting&lt;BR /&gt;DDR: 3733MTS&lt;BR /&gt;M33 prepare ok&lt;BR /&gt;Normal Boot&lt;BR /&gt;Trying to boot from BOOTROM&lt;BR /&gt;Boot Stage: Primary boot&lt;BR /&gt;image offset 0x0, pagesize 0x200, ivt offset 0x0&lt;BR /&gt;Load image from 0x54000 by ROM_API&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Rak**bleep**h&lt;/P&gt;</description>
      <pubDate>Thu, 16 Jul 2026 04:20:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Enabling-console-using-LPUART8-for-imx93/m-p/2395691#M246008</guid>
      <dc:creator>raks</dc:creator>
      <dc:date>2026-07-16T04:20:43Z</dc:date>
    </item>
  </channel>
</rss>