<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Qt5 application with eglfs</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Qt5-application-with-eglfs/m-p/253313#M23591</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Leonardo, see here: &lt;A href="https://community.nxp.com/message/369559"&gt;EGL Error creating egl surface, error = 0x300b&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;Einar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Dec 2013 09:23:42 GMT</pubDate>
    <dc:creator>EinarMar</dc:creator>
    <dc:date>2013-12-18T09:23:42Z</dc:date>
    <item>
      <title>Qt5 application with eglfs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Qt5-application-with-eglfs/m-p/253307#M23585</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have cross-compiled Qt5 with EGL support and now when I'm trying to run an application from the Qt examples like: &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#&amp;gt; ./hellogl_es2 -platform eglfs&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it returns straight away without any notice. The return code is 1.&amp;nbsp; &lt;/P&gt;&lt;P&gt;Even with other platform plugins the behavior is the same.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this a known issue to someone or do I need to provide something more in order to explain myself. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;Einar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Dec 2013 11:19:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Qt5-application-with-eglfs/m-p/253307#M23585</guid>
      <dc:creator>EinarMar</dc:creator>
      <dc:date>2013-12-10T11:19:02Z</dc:date>
    </item>
    <item>
      <title>Re: Qt5 application with eglfs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Qt5-application-with-eglfs/m-p/253308#M23586</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Einar,&lt;/P&gt;&lt;P&gt;when there is no useful (or no log at all) log, I run the app with 'strace' (strace ./hellogl_......). Give it a try and you may find the reason.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Dec 2013 18:51:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Qt5-application-with-eglfs/m-p/253308#M23586</guid>
      <dc:creator>LeonardoSandova</dc:creator>
      <dc:date>2013-12-10T18:51:51Z</dc:date>
    </item>
    <item>
      <title>Re: Re: Qt5 application with eglfs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Qt5-application-with-eglfs/m-p/253309#M23587</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Leonardo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I usually run with strace and I've tried it here but it didn't give me any further insight.&lt;/P&gt;&lt;P&gt;I will attach a file with strace output so you can look. Maybe you will be able to spot something.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;Einar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Dec 2013 08:29:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Qt5-application-with-eglfs/m-p/253309#M23587</guid>
      <dc:creator>EinarMar</dc:creator>
      <dc:date>2013-12-11T08:29:14Z</dc:date>
    </item>
    <item>
      <title>Re: Qt5 application with eglfs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Qt5-application-with-eglfs/m-p/253310#M23588</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there anyone willing to look into the strace file. I'm not sure what is happening just by reading it so I would need some help on this.&lt;/P&gt;&lt;P&gt;My program is not running 'main' and exits with status 1 without any printouts.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope somebody can look into the strace output hellogl_es2_strace.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;Einar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Dec 2013 07:58:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Qt5-application-with-eglfs/m-p/253310#M23588</guid>
      <dc:creator>EinarMar</dc:creator>
      <dc:date>2013-12-16T07:58:35Z</dc:date>
    </item>
    <item>
      <title>Re: Qt5 application with eglfs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Qt5-application-with-eglfs/m-p/253311#M23589</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have figured out what was causing this problem of my Qt5 application not starting and exiting with status 1. It was one library (libicudata.so.52.1) that was not hard-float compiled which caused the linker to exit without any other warning then status 1. &lt;/P&gt;&lt;P&gt;After that was fixed a was able to start the application but it crashed shortly after being started and the reason was incorrect EGL binaries. I was using some version of those libraries acquired from this forum earlier this year. &lt;/P&gt;&lt;P&gt;Now I downloaded from here: &lt;A href="http://repository.timesys.com/buildsources/g/gpu-viv-bin-mx6q/gpu-viv-bin-mx6q-3.0.35-4.0.0/"&gt;http://repository.timesys.com/buildsources/g/gpu-viv-bin-mx6q/gpu-viv-bin-mx6q-3.0.35-4.0.0/&lt;/A&gt; and then my application was not crashing. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My Qt5 application is still not able to run because it complains about: &lt;SPAN style="text-decoration: underline;"&gt;EGL Error : Could not create the egl surface: error = 0x300b&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;The application is executed like: &lt;STRONG&gt;hellogl_es2 -platform eglfs&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If anyone has some idea about that I would appreciate the input. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;Einar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Dec 2013 20:00:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Qt5-application-with-eglfs/m-p/253311#M23589</guid>
      <dc:creator>EinarMar</dc:creator>
      <dc:date>2013-12-16T20:00:55Z</dc:date>
    </item>
    <item>
      <title>Re: Qt5 application with eglfs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Qt5-application-with-eglfs/m-p/253312#M23590</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Einar, it would be good if you create a new discussion thread with this last issue.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Dec 2013 17:25:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Qt5-application-with-eglfs/m-p/253312#M23590</guid>
      <dc:creator>LeonardoSandova</dc:creator>
      <dc:date>2013-12-17T17:25:31Z</dc:date>
    </item>
    <item>
      <title>Re: Qt5 application with eglfs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Qt5-application-with-eglfs/m-p/253313#M23591</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Leonardo, see here: &lt;A href="https://community.nxp.com/message/369559"&gt;EGL Error creating egl surface, error = 0x300b&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;Einar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Dec 2013 09:23:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Qt5-application-with-eglfs/m-p/253313#M23591</guid>
      <dc:creator>EinarMar</dc:creator>
      <dc:date>2013-12-18T09:23:42Z</dc:date>
    </item>
    <item>
      <title>Re: Qt5 application with eglfs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Qt5-application-with-eglfs/m-p/253314#M23592</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Einar&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Had your orignal&amp;nbsp; issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help please feel free to contact Freescale.&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Feb 2014 05:48:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Qt5-application-with-eglfs/m-p/253314#M23592</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2014-02-19T05:48:13Z</dc:date>
    </item>
    <item>
      <title>Re: Qt5 application with eglfs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Qt5-application-with-eglfs/m-p/253315#M23593</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Einar&lt;/P&gt;&lt;P&gt;This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Feb 2014 06:36:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Qt5-application-with-eglfs/m-p/253315#M23593</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2014-02-27T06:36:10Z</dc:date>
    </item>
    <item>
      <title>Re: Qt5 application with eglfs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Qt5-application-with-eglfs/m-p/253316#M23594</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Issue closed, thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Mar 2014 15:48:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Qt5-application-with-eglfs/m-p/253316#M23594</guid>
      <dc:creator>EinarMar</dc:creator>
      <dc:date>2014-03-05T15:48:00Z</dc:date>
    </item>
  </channel>
</rss>