<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX93 - AHAB SecureBoot - SRK TABLE in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX93-AHAB-SecureBoot-SRK-TABLE/m-p/2072795#M235784</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/248332"&gt;@il_ciancio&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;can I flash also these eFuses (fuse from 8 to 15)?&lt;/P&gt;
&lt;P&gt;-&amp;gt; No, please have a reference&amp;nbsp;&lt;A href="https://github.com/nxp-imx/uboot-imx/blob/lf_v2024.04/doc/imx/ahab/guides/mx8ulp_9x_secure_boot.txt" target="_self"&gt;9x_secure_boot&lt;/A&gt;&amp;nbsp;for i.MX93&lt;/P&gt;
&lt;P&gt;Can I generate a SRK Table with only one certificate for my target?&lt;/P&gt;
&lt;P&gt;-&amp;gt;&amp;nbsp;In AHAB,&amp;nbsp;&lt;SPAN data-teams="true"&gt;it requires always 4 SRKs.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
    <pubDate>Wed, 02 Apr 2025 10:25:25 GMT</pubDate>
    <dc:creator>Harvey021</dc:creator>
    <dc:date>2025-04-02T10:25:25Z</dc:date>
    <item>
      <title>IMX93 - AHAB SecureBoot - SRK TABLE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX93-AHAB-SecureBoot-SRK-TABLE/m-p/2072159#M235741</link>
      <description>&lt;P&gt;Hello NXP experts,&lt;/P&gt;&lt;P&gt;I am studying AHAB SecureBoot on IMX93 processor, and I am using CST tool in order to generate certifcates.&lt;/P&gt;&lt;P&gt;A lot of example shows a PKI tree generation with 4 leafs (SRKn, n from 1 to 4).&lt;/P&gt;&lt;P&gt;After the generation, I have to generate the SRK_Table and the SRK_TableFuse.&lt;/P&gt;&lt;P&gt;The SRK_Table is appended on the image, and after I have to flash SRK_TableFuse into eFuse.&lt;/P&gt;&lt;P&gt;CST Tool generates&amp;nbsp;SRK_TableFuse as 16 words, but on the reference manual I have 16 fuse (OES_SRKHy with Y from 0 to 15), but some of them are RESERVED,&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;can I flash also these eFuses (fuse from 8 to 15)?&lt;/LI&gt;&lt;LI&gt;More over, Can I generate a SRK Table with only one certificate for my target?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks a lot!&lt;/P&gt;</description>
      <pubDate>Tue, 01 Apr 2025 15:34:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX93-AHAB-SecureBoot-SRK-TABLE/m-p/2072159#M235741</guid>
      <dc:creator>il_ciancio</dc:creator>
      <dc:date>2025-04-01T15:34:21Z</dc:date>
    </item>
    <item>
      <title>Re: IMX93 - AHAB SecureBoot - SRK TABLE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX93-AHAB-SecureBoot-SRK-TABLE/m-p/2072783#M235783</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;about the SRK table to be fused, i have found an error during the generation.&lt;/P&gt;&lt;P&gt;The correct command with CST tools for IMX9 is showed in:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;A href="https://github.com/nxp-imx/uboot-imx/blob/lf_v2024.04/doc/imx/ahab/introduction_ahab.txt" target="_blank"&gt;uboot-imx/doc/imx/ahab/introduction_ahab.txt at lf_v2024.04 · nxp-imx/uboot-imx&lt;/A&gt;&lt;/LI&gt;&lt;LI&gt;In i.MX 8ULP/9x, the expected SRK HASH is of 256 bit.&lt;UL&gt;&lt;LI&gt;$ cd ../crts/&lt;/LI&gt;&lt;LI&gt;$ ../linux64/bin/srktool -a -d sha256 -s sha384.&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Why is there&amp;nbsp;-s sha384&amp;nbsp; (-s, --sign_digest) ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 02 Apr 2025 10:13:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX93-AHAB-SecureBoot-SRK-TABLE/m-p/2072783#M235783</guid>
      <dc:creator>il_ciancio</dc:creator>
      <dc:date>2025-04-02T10:13:01Z</dc:date>
    </item>
    <item>
      <title>Re: IMX93 - AHAB SecureBoot - SRK TABLE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX93-AHAB-SecureBoot-SRK-TABLE/m-p/2072795#M235784</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/248332"&gt;@il_ciancio&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;can I flash also these eFuses (fuse from 8 to 15)?&lt;/P&gt;
&lt;P&gt;-&amp;gt; No, please have a reference&amp;nbsp;&lt;A href="https://github.com/nxp-imx/uboot-imx/blob/lf_v2024.04/doc/imx/ahab/guides/mx8ulp_9x_secure_boot.txt" target="_self"&gt;9x_secure_boot&lt;/A&gt;&amp;nbsp;for i.MX93&lt;/P&gt;
&lt;P&gt;Can I generate a SRK Table with only one certificate for my target?&lt;/P&gt;
&lt;P&gt;-&amp;gt;&amp;nbsp;In AHAB,&amp;nbsp;&lt;SPAN data-teams="true"&gt;it requires always 4 SRKs.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Wed, 02 Apr 2025 10:25:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX93-AHAB-SecureBoot-SRK-TABLE/m-p/2072795#M235784</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2025-04-02T10:25:25Z</dc:date>
    </item>
    <item>
      <title>Re: IMX93 - AHAB SecureBoot - SRK TABLE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX93-AHAB-SecureBoot-SRK-TABLE/m-p/2078244#M236171</link>
      <description>In the example from git, the certificates were generated with sha384!</description>
      <pubDate>Thu, 10 Apr 2025 10:25:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX93-AHAB-SecureBoot-SRK-TABLE/m-p/2078244#M236171</guid>
      <dc:creator>il_ciancio</dc:creator>
      <dc:date>2025-04-10T10:25:07Z</dc:date>
    </item>
  </channel>
</rss>