<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: How can I boot the Linux kernel with U-Boot when HAB is enabled?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-can-I-boot-the-Linux-kernel-with-U-Boot-when-HAB-is-enabled/m-p/2072414#M235755</link>
    <description>Resolved.&lt;BR /&gt;The reason was that bootargs was not configured.&lt;BR /&gt;</description>
    <pubDate>Wed, 02 Apr 2025 00:46:18 GMT</pubDate>
    <dc:creator>spthx</dc:creator>
    <dc:date>2025-04-02T00:46:18Z</dc:date>
    <item>
      <title>How can I boot the Linux kernel with U-Boot when HAB is enabled?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-can-I-boot-the-Linux-kernel-with-U-Boot-when-HAB-is-enabled/m-p/2070990#M235646</link>
      <description>&lt;P&gt;I am using the i.MX8M Nano.&lt;BR /&gt;I have read the uboot-imx documentation and other related materials, and I am now able to boot U-Boot with secure boot and encrypted boot enabled.&lt;/P&gt;&lt;P&gt;Now, I am trying to manually load a pre-built kernel and DTB and boot using the booti command. However, I encountered the following error:&lt;/P&gt;&lt;P&gt;I suspect that the error is due to the kernel image not being signed.&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;u-boot=&amp;gt; fatload mmc 2:1 ${loadaddr} Image
28013056 bytes read in 144 ms (185.5 MiB/s)
u-boot=&amp;gt; fatload mmc 2:1 ${fdt_addr} imx8mn-ddr3l-evk.dtb
40155 bytes read in 9 ms (4.3 MiB/s)
u-boot=&amp;gt; booti ${loadaddr} - ${fdt_addr}

Authenticate image from DDR location 0x40400000...
bad magic magic=0xff length=0xffff version=0xff
bad length magic=0xff length=0xffff version=0xff
Bad version magic=0xff length=0xffff version=0xff
Error: Invalid IVT structure
Authenticate Image Fail, Please check&lt;/LI-CODE&gt;&lt;P&gt;&lt;BR /&gt;How can I boot the Linux kernel with U-Boot when HAB is enabled?&lt;BR /&gt;If signing is required, how should I sign the kernel?&lt;/P&gt;&lt;P&gt;Additionally, the method described in the earlier guide seems to assume a standalone environment.&lt;BR /&gt;How can I generate an HAB-compatible image within Yocto?&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Mon, 31 Mar 2025 09:00:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-can-I-boot-the-Linux-kernel-with-U-Boot-when-HAB-is-enabled/m-p/2070990#M235646</guid>
      <dc:creator>spthx</dc:creator>
      <dc:date>2025-03-31T09:00:45Z</dc:date>
    </item>
    <item>
      <title>Re: How can I boot the Linux kernel with U-Boot when HAB is enabled?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-can-I-boot-the-Linux-kernel-with-U-Boot-when-HAB-is-enabled/m-p/2071582#M235687</link>
      <description>&lt;P&gt;Please have a reference to the &amp;lt;3. Authenticating additional boot images&amp;gt; of&amp;nbsp;&lt;A href="https://github.com/nxp-imx/uboot-imx/blob/lf_v2024.04/doc/imx/habv4/guides/mx8m_secure_boot.txt" target="_self"&gt;mx8m_secure_boot.txt&lt;/A&gt;&amp;nbsp;for kernel signing.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;About How can I generate an HAB-compatible image within Yocto?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;-&amp;gt; Please have a reference to &amp;lt;10.9 Security reference design&amp;gt; of&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/user-guide/IMX_LINUX_USERS_GUIDE.pdf" target="_self"&gt;IMX_LINUX_USERS_GUIDE.pdf&lt;/A&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Harvey&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 01 Apr 2025 02:57:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-can-I-boot-the-Linux-kernel-with-U-Boot-when-HAB-is-enabled/m-p/2071582#M235687</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2025-04-01T02:57:00Z</dc:date>
    </item>
    <item>
      <title>Re: How can I boot the Linux kernel with U-Boot when HAB is enabled?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-can-I-boot-the-Linux-kernel-with-U-Boot-when-HAB-is-enabled/m-p/2071811#M235703</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/192970"&gt;@Harvey021&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;BR /&gt;HAB authentication passes now, but I get a kernel panic.&lt;BR /&gt;Do you know what might be causing this?&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;</description>
      <pubDate>Tue, 01 Apr 2025 07:53:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-can-I-boot-the-Linux-kernel-with-U-Boot-when-HAB-is-enabled/m-p/2071811#M235703</guid>
      <dc:creator>spthx</dc:creator>
      <dc:date>2025-04-01T07:53:59Z</dc:date>
    </item>
    <item>
      <title>Re: How can I boot the Linux kernel with U-Boot when HAB is enabled?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-can-I-boot-the-Linux-kernel-with-U-Boot-when-HAB-is-enabled/m-p/2072414#M235755</link>
      <description>Resolved.&lt;BR /&gt;The reason was that bootargs was not configured.&lt;BR /&gt;</description>
      <pubDate>Wed, 02 Apr 2025 00:46:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-can-I-boot-the-Linux-kernel-with-U-Boot-when-HAB-is-enabled/m-p/2072414#M235755</guid>
      <dc:creator>spthx</dc:creator>
      <dc:date>2025-04-02T00:46:18Z</dc:date>
    </item>
  </channel>
</rss>