<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックPF8100 conversion efficiency</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PF8100-conversion-efficiency/m-p/2071106#M235650</link>
    <description>&lt;P&gt;HI NXP Teams&lt;/P&gt;&lt;P&gt;How should the conversion efficiency of the PF8100 Type 1 and Type 2 buck regulators be evaluated? Currently, when the load is below 10mA, the conversion efficiency is less than 50%. Is this normal, or are there any other suggested modifications?&lt;/P&gt;</description>
    <pubDate>Mon, 31 Mar 2025 11:23:20 GMT</pubDate>
    <dc:creator>kpoyuan</dc:creator>
    <dc:date>2025-03-31T11:23:20Z</dc:date>
    <item>
      <title>PF8100 conversion efficiency</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF8100-conversion-efficiency/m-p/2071106#M235650</link>
      <description>&lt;P&gt;HI NXP Teams&lt;/P&gt;&lt;P&gt;How should the conversion efficiency of the PF8100 Type 1 and Type 2 buck regulators be evaluated? Currently, when the load is below 10mA, the conversion efficiency is less than 50%. Is this normal, or are there any other suggested modifications?&lt;/P&gt;</description>
      <pubDate>Mon, 31 Mar 2025 11:23:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF8100-conversion-efficiency/m-p/2071106#M235650</guid>
      <dc:creator>kpoyuan</dc:creator>
      <dc:date>2025-03-31T11:23:20Z</dc:date>
    </item>
    <item>
      <title>Re: PF8100 conversion efficiency</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF8100-conversion-efficiency/m-p/2071320#M235678</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;There is no available benchmarks for PF8100, the efficiency should be measured using the relation between input and output power.&lt;/P&gt;
&lt;P&gt;To operate under the PMIC specifications please use the datasheet as reference for your design (component values, connections, layout, etc.).&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Mon, 31 Mar 2025 17:07:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF8100-conversion-efficiency/m-p/2071320#M235678</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2025-03-31T17:07:49Z</dc:date>
    </item>
    <item>
      <title>Re: PF8100 conversion efficiency</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF8100-conversion-efficiency/m-p/2071878#M235713</link>
      <description>&lt;P&gt;HI&lt;/P&gt;&lt;P&gt;The PF8100 also supports the autoskip mode, which seems to allow automatic adjustment between PWM and PFM based on load conditions. How can I determine when the IC will switch between these modes?&lt;/P&gt;</description>
      <pubDate>Tue, 01 Apr 2025 08:53:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF8100-conversion-efficiency/m-p/2071878#M235713</guid>
      <dc:creator>kpoyuan</dc:creator>
      <dc:date>2025-04-01T08:53:18Z</dc:date>
    </item>
    <item>
      <title>Re: PF8100 conversion efficiency</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF8100-conversion-efficiency/m-p/2072130#M235738</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;This can be verified in registers SWx_RUN_MODE and SWx_STBY_MODE, by default is configured with autoskip mode.&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Tue, 01 Apr 2025 14:50:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF8100-conversion-efficiency/m-p/2072130#M235738</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2025-04-01T14:50:56Z</dc:date>
    </item>
  </channel>
</rss>