<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックMX6Q-SDP problem with keyboard</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MX6Q-SDP-problem-with-keyboard/m-p/252994#M23533</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using MX6Q-SDP connectted with USB mouse,keyboard and LVDS.After linux run,the touch screen and usb mouse can &lt;/P&gt;&lt;P&gt;work well, but the keyboard can't work.And I got some error after boot up:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(EE) XKB: Couldn't open rules file /usr/share/X11/xkb/rules/base&lt;/P&gt;&lt;P&gt;(EE) XKB: No components provided for device Virtual core keyboard&lt;/P&gt;&lt;P&gt; unrecognised device identifier!&lt;/P&gt;&lt;P&gt;(EE) config/hal: NewInputDeviceRequest failed (2)&lt;/P&gt;&lt;P&gt;matchbox: keyboard does not appear to have a &amp;amp;1&lt;/P&gt;&lt;P&gt;if ; then&lt;/P&gt;&lt;P&gt; IS_BABBAGE=YES&lt;/P&gt;&lt;P&gt; Xfbdev -keybd keyboard,,device=/dev/input/keyboard0 -mouse mouse,2,device=/dev/input/mice &amp;amp;&lt;/P&gt;&lt;P&gt;fi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if ; then&lt;/P&gt;&lt;P&gt; Xfbdev -mouse tslib,2,device=/dev/input/ts0 -mouse mouse,2,device=/dev/input/mice&amp;amp;&lt;/P&gt;&lt;P&gt;else&lt;/P&gt;&lt;P&gt; Xfbdev -mouse mouse,2,device=/dev/input/mice&amp;amp;&lt;/P&gt;&lt;P&gt;fi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;sleep 8&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;matchbox-window-manager -d :smileyshocked: -use_lowlight no -use_titlebar yes -use_cursor yes&amp;amp;&lt;/P&gt;&lt;P&gt;matchbox-desktop&amp;amp;&lt;/P&gt;&lt;P&gt;matchbox-panel  --bgtrans yes  &amp;amp;&lt;/P&gt;&lt;P&gt;sleep 5&lt;/P&gt;&lt;OL&gt;&lt;LI level="1" type="ol"&gt;&lt;P&gt;Calibrate when using the rootfs the first time&lt;/P&gt;&lt;/LI&gt;&lt;LI level="1" type="ol"&gt;&lt;P&gt;Check whether the touch screen exists&lt;/P&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;if ; then&lt;/P&gt;&lt;P&gt; ls /usr/etc | grep pointercal &amp;gt; /dev/null 2&amp;gt;&amp;amp;1&lt;/P&gt;&lt;P&gt; if ; then&lt;/P&gt;&lt;P&gt;  ts_calibrate&lt;/P&gt;&lt;P&gt; fi&lt;/P&gt;&lt;P&gt;fi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 23 Feb 2014 08:09:03 GMT</pubDate>
    <dc:creator>xiaoqiangyang</dc:creator>
    <dc:date>2014-02-23T08:09:03Z</dc:date>
    <item>
      <title>MX6Q-SDP problem with keyboard</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX6Q-SDP-problem-with-keyboard/m-p/252994#M23533</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using MX6Q-SDP connectted with USB mouse,keyboard and LVDS.After linux run,the touch screen and usb mouse can &lt;/P&gt;&lt;P&gt;work well, but the keyboard can't work.And I got some error after boot up:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(EE) XKB: Couldn't open rules file /usr/share/X11/xkb/rules/base&lt;/P&gt;&lt;P&gt;(EE) XKB: No components provided for device Virtual core keyboard&lt;/P&gt;&lt;P&gt; unrecognised device identifier!&lt;/P&gt;&lt;P&gt;(EE) config/hal: NewInputDeviceRequest failed (2)&lt;/P&gt;&lt;P&gt;matchbox: keyboard does not appear to have a &amp;amp;1&lt;/P&gt;&lt;P&gt;if ; then&lt;/P&gt;&lt;P&gt; IS_BABBAGE=YES&lt;/P&gt;&lt;P&gt; Xfbdev -keybd keyboard,,device=/dev/input/keyboard0 -mouse mouse,2,device=/dev/input/mice &amp;amp;&lt;/P&gt;&lt;P&gt;fi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if ; then&lt;/P&gt;&lt;P&gt; Xfbdev -mouse tslib,2,device=/dev/input/ts0 -mouse mouse,2,device=/dev/input/mice&amp;amp;&lt;/P&gt;&lt;P&gt;else&lt;/P&gt;&lt;P&gt; Xfbdev -mouse mouse,2,device=/dev/input/mice&amp;amp;&lt;/P&gt;&lt;P&gt;fi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;sleep 8&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;matchbox-window-manager -d :smileyshocked: -use_lowlight no -use_titlebar yes -use_cursor yes&amp;amp;&lt;/P&gt;&lt;P&gt;matchbox-desktop&amp;amp;&lt;/P&gt;&lt;P&gt;matchbox-panel  --bgtrans yes  &amp;amp;&lt;/P&gt;&lt;P&gt;sleep 5&lt;/P&gt;&lt;OL&gt;&lt;LI level="1" type="ol"&gt;&lt;P&gt;Calibrate when using the rootfs the first time&lt;/P&gt;&lt;/LI&gt;&lt;LI level="1" type="ol"&gt;&lt;P&gt;Check whether the touch screen exists&lt;/P&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;if ; then&lt;/P&gt;&lt;P&gt; ls /usr/etc | grep pointercal &amp;gt; /dev/null 2&amp;gt;&amp;amp;1&lt;/P&gt;&lt;P&gt; if ; then&lt;/P&gt;&lt;P&gt;  ts_calibrate&lt;/P&gt;&lt;P&gt; fi&lt;/P&gt;&lt;P&gt;fi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 23 Feb 2014 08:09:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX6Q-SDP-problem-with-keyboard/m-p/252994#M23533</guid>
      <dc:creator>xiaoqiangyang</dc:creator>
      <dc:date>2014-02-23T08:09:03Z</dc:date>
    </item>
    <item>
      <title>Re: MX6Q-SDP problem with keyboard</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX6Q-SDP-problem-with-keyboard/m-p/252995#M23534</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are you using our Ubuntu BSP ?... have you tried with a different keyboard?, or just the keyboard (no mouse)?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Mar 2014 15:58:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX6Q-SDP-problem-with-keyboard/m-p/252995#M23534</guid>
      <dc:creator>SergioSolis</dc:creator>
      <dc:date>2014-03-03T15:58:47Z</dc:date>
    </item>
    <item>
      <title>Re: MX6Q-SDP problem with keyboard</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MX6Q-SDP-problem-with-keyboard/m-p/252996#M23535</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My keyboard and mouse can work well under ubuntu image downloaded from Freescale.But after I built 'fsl gnome release Package'with &lt;/P&gt;&lt;P&gt;ltib and boot,the problem with keyboard came to me.It seems that the keyboard layout has something wrong with 'ALT' key,&lt;/P&gt;&lt;P&gt;so the key shortcuts definitions in matchbox/kbdconfig can't work. But I don't know how to verify my guess and take action.&lt;/P&gt;&lt;P&gt;Only keyboard has the same phenomenon.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Mar 2014 01:14:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MX6Q-SDP-problem-with-keyboard/m-p/252996#M23535</guid>
      <dc:creator>xiaoqiangyang</dc:creator>
      <dc:date>2014-03-04T01:14:31Z</dc:date>
    </item>
  </channel>
</rss>