<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Kernel internal error with DART-MX8M-PLUS DSI with Raspberry PI display</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-internal-error-with-DART-MX8M-PLUS-DSI-with-Raspberry-PI/m-p/2065359#M235317</link>
    <description>Thank you for your reply. Unfortunately it does not solve the problem. With the device tree you suggested the system does boot but the display never shows. I believe the lcdif driver gets deferred infinitely. I suspect this is due to the ports declaration in the device tree overriding port 0 which connects to the lcdif.&lt;BR /&gt;&lt;BR /&gt;The other device tree you linked I have seen before and the device tree I originally wrote is based off of it.&lt;BR /&gt;&lt;BR /&gt;Do you perhaps have any other suggestions that might work?&lt;BR /&gt;&lt;BR /&gt;Thanks!</description>
    <pubDate>Thu, 20 Mar 2025 07:59:25 GMT</pubDate>
    <dc:creator>user38572</dc:creator>
    <dc:date>2025-03-20T07:59:25Z</dc:date>
    <item>
      <title>Kernel internal error with DART-MX8M-PLUS DSI with Raspberry PI display</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-internal-error-with-DART-MX8M-PLUS-DSI-with-Raspberry-PI/m-p/2059593#M234934</link>
      <description>&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am trying to get a Raspberry PI 7" display (dsi display with internal tc358762 dsi to dpi converter and microcontroller for initialization and backlight control) to work on a custom board with a&amp;nbsp;DART-MX8M-PLUS (&lt;SPAN&gt;i.MX 8M Plus)&lt;/SPAN&gt; on it, however I cannot get it to work. The device tree is based on the&amp;nbsp;imx8mp-var-dart-dt8mcustomboard.dts file from&amp;nbsp;&lt;A href="https://github.com/varigit/linux-imx/" target="_blank"&gt;https://github.com/varigit/linux-imx/&lt;/A&gt;. Below are the relevant changes made to this file to try and get the display to work (the full file is bigger):&lt;/P&gt;&lt;LI-CODE lang="c"&gt;// More stuff here

/ {
    // More stuff here
    
	panel@1 {
	    reg = &amp;lt;1&amp;gt;;
		compatible = "qiaodian,qd43003c0-40";
		//compatible = "raspberrypi,7inch-dsi";
		power-supply = &amp;lt;&amp;amp;attiny&amp;gt;;
		backlight = &amp;lt;&amp;amp;attiny&amp;gt;;

		port {
			panel_in: endpoint {
				remote-endpoint = &amp;lt;&amp;amp;bridge_out&amp;gt;;
			};
		};
	};
};

&amp;amp;lcdif1 {
	status = "okay";
};

&amp;amp;mipi_dsi {
	#address-cells = &amp;lt;1&amp;gt;;
	#size-cells = &amp;lt;0&amp;gt;;
	status = "okay";

	bridge@0 {
		compatible = "toshiba,tc358762";
		reg = &amp;lt;0&amp;gt;;
		vddc-supply = &amp;lt;&amp;amp;attiny&amp;gt;;

		ports {
			#address-cells = &amp;lt;1&amp;gt;;
			#size-cells = &amp;lt;0&amp;gt;;

			port@0 {
				reg = &amp;lt;0&amp;gt;;

				bridge_in: endpoint {
					remote-endpoint = &amp;lt;&amp;amp;dsi_out&amp;gt;;
				};
			};

			port@1 {
				reg = &amp;lt;1&amp;gt;;

				bridge_out: endpoint {
					remote-endpoint = &amp;lt;&amp;amp;panel_in&amp;gt;;
				};
			};
		};
	};
	
	port@1 {
		reg = &amp;lt;1&amp;gt;;

		dsi_out: endpoint {
			data-lanes = &amp;lt;1&amp;gt;;
			remote-endpoint = &amp;lt;&amp;amp;bridge_in&amp;gt;;
		};
	};
};

&amp;amp;i2c6 {
    clock-frequency = &amp;lt;400000&amp;gt;;
	pinctrl-names = "default", "gpio";
	pinctrl-0 = &amp;lt;&amp;amp;pinctrl_i2c6&amp;gt;;
	//pinctrl-1 = &amp;lt;&amp;amp;pinctrl_i2c6_gpio&amp;gt;;
	scl-gpios = &amp;lt;&amp;amp;gpio3 28 GPIO_ACTIVE_HIGH&amp;gt;;
	sda-gpios = &amp;lt;&amp;amp;gpio3 29 GPIO_ACTIVE_HIGH&amp;gt;;
	status = "okay";
	
    #address-cells = &amp;lt;1&amp;gt;;
    #size-cells = &amp;lt;0&amp;gt;;
    
    attiny: regulator@45 {
		compatible = "raspberrypi,7inch-touchscreen-panel-regulator";
		reg = &amp;lt;0x45&amp;gt;;
	};
};

// More stuff here&lt;/LI-CODE&gt;&lt;P&gt;Without these changes the board boots fine. With these changes I receive the following internal error during boot (only relevant part of boot log shown):&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;[    2.079254] gpio-144 (scl): enforced open drain please flag it properly in DT/ACPI DSDT/board file
[    2.089639] OF: graph: no port node found in /soc@0/bus@30800000/i2c@30a30000/ov5640_mipi@3c
[    2.098111] ov5640 1-003c: endpoint node not found
[    2.102914] ov5640: probe of 1-003c failed with error -22
[    2.108373] i2c i2c-1: IMX I2C adapter registered
[    2.113625] gpio-92 (scl): enforced open drain please flag it properly in DT/ACPI DSDT/board file
[    2.123483] imx_sec_dsim_drv 32e60000.mipi_dsi: Failed to create device link (0x180) with 5-0045
[    2.187563] imx_sec_dsim_drv 32e60000.mipi_dsi: Failed to create device link (0x180) with 5-0045
[    2.196609] i2c i2c-5: IMX I2C adapter registered
[    2.201763] imx8mq-usb-phy 381f0040.usb-phy: supply vbus not found, using dummy regulator
[    2.210407] imx8mq-usb-phy 382f0040.usb-phy: supply vbus not found, using dummy regulator
[    2.244025] panel-simple 100000003.panel: Specify missing connector_type
[    2.268172] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)
[    2.276236] imx_sec_dsim_drv 32e60000.mipi_dsi: version number is 0x1060200
[    2.283650] imx_sec_dsim_drv 32e60000.mipi_dsi: [drm] *ERROR* modalias failure on /soc@0/bus@32c00000/mipi_dsi@32e60000/port@1
[    2.295091] imx-drm display-subsystem: bound 32e60000.mipi_dsi (ops imx_sec_dsim_ops)
[    2.303817] [drm] Initialized imx-drm 1.0.0 20120507 for display-subsystem on minor 1
[    2.347202] Unable to handle kernel paging request at virtual address fffffffffffffe0b
[    2.355125] Mem abort info:
[    2.357918]   ESR = 0x0000000096000004
[    2.361675]   EC = 0x25: DABT (current EL), IL = 32 bits
[    2.366991]   SET = 0, FnV = 0
[    2.370053]   EA = 0, S1PTW = 0
[    2.373203]   FSC = 0x04: level 0 translation fault
[    2.378090] Data abort info:
[    2.380976]   ISV = 0, ISS = 0x00000004
[    2.384815]   CM = 0, WnR = 0
[    2.387790] swapper pgtable: 4k pages, 48-bit VAs, pgdp=0000000042097000
[    2.394498] [fffffffffffffe0b] pgd=0000000000000000, p4d=0000000000000000
[    2.401301] Internal error: Oops: 0000000096000004 [#1] PREEMPT SMP
[    2.407569] Modules linked in:
[    2.410627] CPU: 2 PID: 9 Comm: kworker/u8:0 Not tainted 6.1.36-imx8mp+g7248bd964cd9 #1
[    2.418633] Hardware name: Variscite DART-MX8M-PLUS on custom board (DT)
[    2.425335] Workqueue: events_unbound deferred_probe_work_func
[    2.431177] pstate: 60000005 (nZCv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[    2.438146] pc : drm_panel_get_modes+0x44/0xb0
[    2.442595] lr : drm_panel_get_modes+0x44/0xb0
[    2.447041] sp : ffff80000a1fb6a0
[    2.450356] x29: ffff80000a1fb6a0 x28: ffff0000c1566200 x27: 0000000000001000
[    2.457500] x26: 0000000000000023 x25: ffff800009fa64e0 x24: ffff0000c1286000
[    2.464644] x23: 00000000fffffffd x22: ffff0000c1287420 x21: 0000000000000000
[    2.471786] x20: ffff0000c12870a0 x19: fffffffffffffdfb x18: 0000000000000006
[    2.478930] x17: 6f206d6574737973 x16: 6275732d79616c70 x15: ffff80000a1fb1e0
[    2.486077] x14: 0000000000000000 x13: ffff800009ed2198 x12: 00000000000004bf
[    2.493219] x11: 0000000000000195 x10: ffff800009f2a198 x9 : ffff800009ed2198
[    2.500361] x8 : 00000000ffffefff x7 : ffff800009f2a198 x6 : 80000000fffff000
[    2.507505] x5 : 000000000000bff4 x4 : 0000000000000000 x3 : 0000000000000000
[    2.514648] x2 : 0000000000000000 x1 : ffff0000c00c0000 x0 : 0000000000000021
[    2.521794] Call trace:
[    2.524241]  drm_panel_get_modes+0x44/0xb0
[    2.528344]  sec_mipi_dsim_connector_get_modes+0x58/0x74
[    2.533663]  drm_helper_probe_single_connector_modes+0x1c4/0x510
[    2.539673]  drm_client_modeset_probe+0x204/0x1190
[    2.544472]  __drm_fb_helper_initial_config_and_unlock+0x44/0x540
[    2.550572]  drm_fbdev_client_hotplug+0x150/0x210
[    2.555282]  drm_fbdev_generic_setup+0xb4/0x194
[    2.559818]  imx_drm_bind+0x260/0x2e0
[    2.563484]  try_to_bring_up_aggregate_device+0x1dc/0x2d0
[    2.568891]  __component_add+0xa4/0x190
[    2.572735]  component_add+0x14/0x20
[    2.576315]  lcdifv3_crtc_probe+0x50/0xb0
[    2.580333]  platform_probe+0x68/0xc0
[    2.584000]  really_probe+0xc0/0x3dc
[    2.587583]  __driver_probe_device+0x7c/0x160
[    2.591947]  driver_probe_device+0x3c/0x110
[    2.596137]  __device_attach_driver+0xbc/0x160
[    2.600588]  bus_for_each_drv+0x7c/0xd4
[    2.604431]  __device_attach+0x9c/0x1c0
[    2.608274]  device_initial_probe+0x14/0x20
[    2.612464]  bus_probe_device+0x9c/0xa4
[    2.616307]  deferred_probe_work_func+0x94/0xe4
[    2.620841]  process_one_work+0x1d4/0x330
[    2.624857]  worker_thread+0x220/0x430
[    2.628613]  kthread+0x108/0x10c
[    2.631844]  ret_from_fork+0x10/0x20
[    2.635428] Code: aa1303e1 f0002d80 91338000 97ffd87b (f9400a61)
[    2.641524] ---[ end trace 0000000000000000 ]---
[    3.711705] Hot alarm is canceled. GPU3D clock will return to 64/64&lt;/LI-CODE&gt;&lt;P&gt;The display initialization works and the backlight comes on when I remove the panel and dsi parts from the device tree and leave only the attiny bit in the i2c port. Additionally I can see from the warning in the log that the panel driver loads.&lt;/P&gt;&lt;P&gt;I suspect this error could be a bug in the IMX DRM driver.&lt;/P&gt;&lt;P&gt;I have tried both linux kernel version 6.6.52 and 6.1.36. Both kernels come from the previously linked imx-linux github.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does anyone have any clue what could be wrong?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Tue, 11 Mar 2025 13:54:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-internal-error-with-DART-MX8M-PLUS-DSI-with-Raspberry-PI/m-p/2059593#M234934</guid>
      <dc:creator>user38572</dc:creator>
      <dc:date>2025-03-11T13:54:24Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel internal error with DART-MX8M-PLUS DSI with Raspberry PI display</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-internal-error-with-DART-MX8M-PLUS-DSI-with-Raspberry-PI/m-p/2059734#M234944</link>
      <description>&lt;P&gt;HI &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/247904"&gt;@user38572&lt;/a&gt;!&lt;/P&gt;
&lt;P&gt;Thank you for contacting NXP Support!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Can you try with this device tree?&lt;/P&gt;
&lt;P&gt;Only you have to add the driver of the panel that you will use.&lt;/P&gt;
&lt;P&gt;also You can refer to this &lt;A href="https://github.com/nxp-imx/linux-imx/blob/e0f9e2afd4cff3f02d71891244b4aa5899dfc786/arch/arm64/boot/dts/freescale/imx8mp-venice-gw74xx-rpidsi.dtso#L48" target="_self"&gt;device tree&lt;/A&gt;&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;// More stuff here

/ {
    // More stuff here
    
	panel {
		compatible = "";
		power-supply = &amp;lt;&amp;amp;attiny&amp;gt;;
		backlight = &amp;lt;&amp;amp;attiny&amp;gt;;

		port {
			panel_in: endpoint {
				remote-endpoint = &amp;lt;&amp;amp;bridge_out&amp;gt;;
			};
		};
	};
};

&amp;amp;lcdif1 {
	status = "okay";
};

&amp;amp;mipi_dsi {
	#address-cells = &amp;lt;1&amp;gt;;
	#size-cells = &amp;lt;0&amp;gt;;
	status = "okay";

	bridge@0 {
		compatible = "toshiba,tc358762";
		reg = &amp;lt;0&amp;gt;;
		vddc-supply = &amp;lt;&amp;amp;attiny&amp;gt;;

		ports {
			#address-cells = &amp;lt;1&amp;gt;;
			#size-cells = &amp;lt;0&amp;gt;;

			port@0 {
				reg = &amp;lt;0&amp;gt;;

				bridge_in: endpoint {
					remote-endpoint = &amp;lt;&amp;amp;dsi_out&amp;gt;;
				};
			};

			port@1 {
				reg = &amp;lt;1&amp;gt;;

				bridge_out: endpoint {
					remote-endpoint = &amp;lt;&amp;amp;panel_in&amp;gt;;
				};
			};
		};
	};
	
	ports {
		#address-cells = &amp;lt;1&amp;gt;;
		#size-cells = &amp;lt;0&amp;gt;;

		port@1 {
			reg = &amp;lt;1&amp;gt;;

			dsi_out: endpoint {
				data-lanes = &amp;lt;1 2&amp;gt;;
				remote-endpoint = &amp;lt;&amp;amp;bridge_in&amp;gt;;
			};
		};
	};
};

&amp;amp;i2c6 {
    clock-frequency = &amp;lt;400000&amp;gt;;
	pinctrl-names = "default", "gpio";
	pinctrl-0 = &amp;lt;&amp;amp;pinctrl_i2c6&amp;gt;;
	//pinctrl-1 = &amp;lt;&amp;amp;pinctrl_i2c6_gpio&amp;gt;;
	scl-gpios = &amp;lt;&amp;amp;gpio3 28 GPIO_ACTIVE_HIGH&amp;gt;;
	sda-gpios = &amp;lt;&amp;amp;gpio3 29 GPIO_ACTIVE_HIGH&amp;gt;;
	status = "okay";
	
    #address-cells = &amp;lt;1&amp;gt;;
    #size-cells = &amp;lt;0&amp;gt;;
    
    attiny: regulator@45 {
		compatible = "raspberrypi,7inch-touchscreen-panel-regulator";
		reg = &amp;lt;0x45&amp;gt;;
	};
};

// More stuff here&lt;/LI-CODE&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Unfortunately we don't have the board and that BSP is modified by Variscite if the proposed modification doesn't work please contact to Variscite Support.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards!&lt;/P&gt;
&lt;P&gt;Chavira&lt;/P&gt;</description>
      <pubDate>Tue, 11 Mar 2025 17:29:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-internal-error-with-DART-MX8M-PLUS-DSI-with-Raspberry-PI/m-p/2059734#M234944</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2025-03-11T17:29:54Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel internal error with DART-MX8M-PLUS DSI with Raspberry PI display</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-internal-error-with-DART-MX8M-PLUS-DSI-with-Raspberry-PI/m-p/2065359#M235317</link>
      <description>Thank you for your reply. Unfortunately it does not solve the problem. With the device tree you suggested the system does boot but the display never shows. I believe the lcdif driver gets deferred infinitely. I suspect this is due to the ports declaration in the device tree overriding port 0 which connects to the lcdif.&lt;BR /&gt;&lt;BR /&gt;The other device tree you linked I have seen before and the device tree I originally wrote is based off of it.&lt;BR /&gt;&lt;BR /&gt;Do you perhaps have any other suggestions that might work?&lt;BR /&gt;&lt;BR /&gt;Thanks!</description>
      <pubDate>Thu, 20 Mar 2025 07:59:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-internal-error-with-DART-MX8M-PLUS-DSI-with-Raspberry-PI/m-p/2065359#M235317</guid>
      <dc:creator>user38572</dc:creator>
      <dc:date>2025-03-20T07:59:25Z</dc:date>
    </item>
  </channel>
</rss>