<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.mx95 lvds in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-mx95-lvds/m-p/2065023#M235290</link>
    <description>Hello,&lt;BR /&gt;&lt;BR /&gt;Yes, the i.MX95 2x 4-lane LVDS display interface capable of 1080p60 resolution.&lt;BR /&gt;&lt;BR /&gt;Best regards/Saludos,&lt;BR /&gt;Aldo.</description>
    <pubDate>Wed, 19 Mar 2025 22:04:47 GMT</pubDate>
    <dc:creator>AldoG</dc:creator>
    <dc:date>2025-03-19T22:04:47Z</dc:date>
    <item>
      <title>i.mx95 lvds</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx95-lvds/m-p/2063855#M235215</link>
      <description>&lt;P&gt;HI NXP Teams&lt;/P&gt;&lt;P&gt;I am evaluating the I.MX95 for multi-camera and multi-display applications. Since two sets of MIPI-CSI are required simultaneously, DSI cannot be used for the display. I would like to know if the two 1x4 LVDS ports can output different display information separately? What is the supported bitrate and resolution?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;poyuan&lt;/P&gt;</description>
      <pubDate>Tue, 18 Mar 2025 14:01:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx95-lvds/m-p/2063855#M235215</guid>
      <dc:creator>kpoyuan</dc:creator>
      <dc:date>2025-03-18T14:01:43Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx95 lvds</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx95-lvds/m-p/2064003#M235223</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Please note that i.MX95 is still in pre-production stage so all information and specifications&amp;nbsp;&lt;SPAN&gt;herein are subject to change without notice.&lt;BR /&gt;&lt;BR /&gt;I.MX95 is capable of&amp;nbsp;a 2x 4-lane or 1x 8-lane LVDS display interface capable of 1080p60 resolution.&lt;BR /&gt;&lt;BR /&gt;On the EVK there is 2 combinations available either two single-channel LVDS-to-HDMI converter or&amp;nbsp;two BOE WXGA LVDS panel.&lt;BR /&gt;&lt;BR /&gt;Best regards/Saludos,&lt;BR /&gt;Aldo.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 18 Mar 2025 18:33:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx95-lvds/m-p/2064003#M235223</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2025-03-18T18:33:32Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx95 lvds</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx95-lvds/m-p/2064196#M235232</link>
      <description>&lt;P&gt;I understand the current status of the I.MX95. Can the two BOE WXGA LVDS panels on the EVK output different information? If I create my own adapter, can it output 1080P, 30FPS information?&lt;/P&gt;</description>
      <pubDate>Wed, 19 Mar 2025 01:38:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx95-lvds/m-p/2064196#M235232</guid>
      <dc:creator>kpoyuan</dc:creator>
      <dc:date>2025-03-19T01:38:15Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx95 lvds</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx95-lvds/m-p/2065023#M235290</link>
      <description>Hello,&lt;BR /&gt;&lt;BR /&gt;Yes, the i.MX95 2x 4-lane LVDS display interface capable of 1080p60 resolution.&lt;BR /&gt;&lt;BR /&gt;Best regards/Saludos,&lt;BR /&gt;Aldo.</description>
      <pubDate>Wed, 19 Mar 2025 22:04:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx95-lvds/m-p/2065023#M235290</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2025-03-19T22:04:47Z</dc:date>
    </item>
  </channel>
</rss>