<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: IMX8QXP jpeg decoder</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-jpeg-decoder/m-p/2062856#M235150</link>
    <description>&lt;P&gt;couldn't reproduce this on nxp board with official bsp&lt;/P&gt;
&lt;P&gt;I didnot reproduce any issue,&lt;/P&gt;
&lt;P&gt;below is cmd for make v4l2jpegdec plugin output fmt is NV12.&lt;/P&gt;
&lt;P&gt;root@imx8qxpc0mek:~# cat /proc/version&lt;BR /&gt;Linux version 6.6.23-lts-next-06236-gb586a521770e (oe-user@oe-host) (aarch64-poky-linux-gcc (GCC) 13.2.0, GNU ld (GNU Binutils) 2.42.0.20240216) #1 SMP PREEMPT Fri Jun 7 13:15:57 UTC 2024&lt;BR /&gt;root@imx8qxpc0mek:~# gst-launch-1.0 filesrc location=/root/thumbnail_image004.jpg ! jpegparse ! v4l2jpegdec ! "video/x-raw,format=NV12" ! filesink location=dmp.nv12&lt;BR /&gt;Setting pipeline to PAUSED ...&lt;/P&gt;
&lt;P&gt;====== V4L2DEC: 1.24.0 build on May 6 2024 08:51:28. ======&lt;BR /&gt;Pipeline is PREROLLING ...&lt;BR /&gt;Pipeline is PREROLLED ...&lt;BR /&gt;Setting pipeline to PLAYING ...&lt;BR /&gt;Redistribute latency...&lt;BR /&gt;New clock: GstSystemClock&lt;BR /&gt;Got EOS from element "pipeline0".&lt;BR /&gt;Execution ended after 0:00:00.007471000&lt;BR /&gt;Setting pipeline to NULL ...&lt;BR /&gt;Freeing pipeline .&lt;/P&gt;</description>
    <pubDate>Mon, 17 Mar 2025 08:21:31 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2025-03-17T08:21:31Z</dc:date>
    <item>
      <title>IMX8QXP jpeg decoder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-jpeg-decoder/m-p/2054130#M234618</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;We are experiencing an issue with the JPEG encoder on our IMX8QXP (var-som) system. We are using Yocto Scarthgap and require the encoder to convert JPEG images to raw NV12 or BGR24 formats.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Currently, we are only receiving YUV444 (YUV3) output. Previously, with Yocto Sumo, we were able to obtain NV12 output successfully.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The mxc-jpeg device driver appears to support multiple output formats, including BGR24, NV12, and NV12M. Furthermore, the command #v4l2-ctl --list-formats-ext -d /dev/video2 lists 13 compatible output types.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;We would appreciate assistance in understanding the specific requirements necessary to achieve NV12 or BGR24 output from the driver.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;A simplified version of our C code is attached for your reference.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Sincerely,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;//Saber&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 01 Mar 2025 13:36:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-jpeg-decoder/m-p/2054130#M234618</guid>
      <dc:creator>saber_hosseini</dc:creator>
      <dc:date>2025-03-01T13:36:46Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QXP jpeg decoder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-jpeg-decoder/m-p/2054639#M234655</link>
      <description>&lt;P&gt;did you test the gstreamer with jpeg encoder on the imx8qxp? do you have any log or print information to share? &lt;/P&gt;</description>
      <pubDate>Mon, 03 Mar 2025 10:21:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-jpeg-decoder/m-p/2054639#M234655</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2025-03-03T10:21:11Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QXP jpeg decoder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-jpeg-decoder/m-p/2054731#M234659</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks for your replay.&lt;BR /&gt;&lt;BR /&gt;I have attached the output from gstreamer. I used the command below, as you can see in the logs, gstreamer uses HW JPEG coder to convert the input image to V308 (YUV444) and then converts YUV444 to RGB using software.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;# GST_DEBUG=3 gst-launch-1.0 -v filesrc location=/ANPR/DPRGremlin1080p.jpg ! jpegparse ! v4l2jpegdec capture-io-mode=dmabuf ! videoconvert ! video/x-raw,format=RGB ! filesink location=output.rgb&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have also used the example code from&amp;nbsp;&lt;A href="https://github.com/nxp-imx/imx-test/tree/lf-6.6.23_2.0.0/test/mxc_jpeg_test" target="_self"&gt;https://github.com/nxp-imx/imx-test/tree/lf-6.6.23_2.0.0/test/mxc_jpeg_test&lt;/A&gt;&lt;/P&gt;&lt;P&gt;It seems like, when we want to use ioctl and VIDIOC_STREAMON, then the output format changes to YUV444.&lt;/P&gt;</description>
      <pubDate>Mon, 03 Mar 2025 12:46:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-jpeg-decoder/m-p/2054731#M234659</guid>
      <dc:creator>saber_hosseini</dc:creator>
      <dc:date>2025-03-03T12:46:33Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QXP jpeg decoder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-jpeg-decoder/m-p/2055179#M234688</link>
      <description>&lt;P&gt;what format of your jpg source is? do you mean you can output nv12 on&amp;nbsp;&lt;SPAN&gt;Yocto Sumo using the same command, right? if yes pls send your jpg file to me, and I checked the source code, it seems can support different format as output&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;A href="https://github.com/nxp-imx/linux-imx/blob/lf-6.6.y/drivers/media/platform/nxp/imx-jpeg/mxc-jpeg.c" target="_blank"&gt;linux-imx/drivers/media/platform/nxp/imx-jpeg/mxc-jpeg.c at lf-6.6.y · nxp-imx/linux-imx&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 04 Mar 2025 03:55:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-jpeg-decoder/m-p/2055179#M234688</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2025-03-04T03:55:44Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QXP jpeg decoder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-jpeg-decoder/m-p/2055309#M234697</link>
      <description>&lt;P&gt;Yes, you are correct. Our product has Sumo right now and it can convert JPEG to NV12. However, with Scarthgap (kernel 6.6.23) the only output we get is YUV444, despite of whatever we configure the decoder.&lt;/P&gt;&lt;P&gt;I have attached two images we are using for test.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 04 Mar 2025 07:43:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-jpeg-decoder/m-p/2055309#M234697</guid>
      <dc:creator>saber_hosseini</dc:creator>
      <dc:date>2025-03-04T07:43:54Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QXP jpeg decoder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-jpeg-decoder/m-p/2056295#M234732</link>
      <description>&lt;P&gt;My main question is, how do we get RGB (or BGR) out of decoder!&lt;/P&gt;</description>
      <pubDate>Wed, 05 Mar 2025 13:13:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-jpeg-decoder/m-p/2056295#M234732</guid>
      <dc:creator>saber_hosseini</dc:creator>
      <dc:date>2025-03-05T13:13:21Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QXP jpeg decoder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-jpeg-decoder/m-p/2062856#M235150</link>
      <description>&lt;P&gt;couldn't reproduce this on nxp board with official bsp&lt;/P&gt;
&lt;P&gt;I didnot reproduce any issue,&lt;/P&gt;
&lt;P&gt;below is cmd for make v4l2jpegdec plugin output fmt is NV12.&lt;/P&gt;
&lt;P&gt;root@imx8qxpc0mek:~# cat /proc/version&lt;BR /&gt;Linux version 6.6.23-lts-next-06236-gb586a521770e (oe-user@oe-host) (aarch64-poky-linux-gcc (GCC) 13.2.0, GNU ld (GNU Binutils) 2.42.0.20240216) #1 SMP PREEMPT Fri Jun 7 13:15:57 UTC 2024&lt;BR /&gt;root@imx8qxpc0mek:~# gst-launch-1.0 filesrc location=/root/thumbnail_image004.jpg ! jpegparse ! v4l2jpegdec ! "video/x-raw,format=NV12" ! filesink location=dmp.nv12&lt;BR /&gt;Setting pipeline to PAUSED ...&lt;/P&gt;
&lt;P&gt;====== V4L2DEC: 1.24.0 build on May 6 2024 08:51:28. ======&lt;BR /&gt;Pipeline is PREROLLING ...&lt;BR /&gt;Pipeline is PREROLLED ...&lt;BR /&gt;Setting pipeline to PLAYING ...&lt;BR /&gt;Redistribute latency...&lt;BR /&gt;New clock: GstSystemClock&lt;BR /&gt;Got EOS from element "pipeline0".&lt;BR /&gt;Execution ended after 0:00:00.007471000&lt;BR /&gt;Setting pipeline to NULL ...&lt;BR /&gt;Freeing pipeline .&lt;/P&gt;</description>
      <pubDate>Mon, 17 Mar 2025 08:21:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-jpeg-decoder/m-p/2062856#M235150</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2025-03-17T08:21:31Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QXP jpeg decoder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-jpeg-decoder/m-p/2062861#M235151</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Would you please try RGB or BGR?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Saber&lt;/P&gt;</description>
      <pubDate>Mon, 17 Mar 2025 08:24:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-jpeg-decoder/m-p/2062861#M235151</guid>
      <dc:creator>saber_hosseini</dc:creator>
      <dc:date>2025-03-17T08:24:23Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QXP jpeg decoder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-jpeg-decoder/m-p/2062985#M235167</link>
      <description>&lt;P&gt;"8QXP JPEG decoder only support such case of RGB format, for example if the input jpeg is encoding use RGB color space, then JPEG decoder output is RGB fmt; But if input jpeg is encoding use YUV color space, then output still is YUV fmt.If customer must use input YUV JPEG , but output need RGB fmt, suggest customer use hardware video convert, such as imxvideoconvert, other than software video convert."&lt;/P&gt;</description>
      <pubDate>Mon, 17 Mar 2025 10:23:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-jpeg-decoder/m-p/2062985#M235167</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2025-03-17T10:23:15Z</dc:date>
    </item>
  </channel>
</rss>