<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: bus speed of /dev/i2c-2 on imx6q in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/bus-speed-of-dev-i2c-2-on-imx6q/m-p/252859#M23511</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Attached is the porting guide. I hope this is useful for you. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 15 Aug 2013 09:28:05 GMT</pubDate>
    <dc:creator>jimmychan</dc:creator>
    <dc:date>2013-08-15T09:28:05Z</dc:date>
    <item>
      <title>bus speed of /dev/i2c-2 on imx6q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/bus-speed-of-dev-i2c-2-on-imx6q/m-p/252858#M23510</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone, &lt;/P&gt;&lt;P&gt;I am unaware as to who sets clock speed on the i2c bus and specifically on the /dev/i2c-2 which is exposed on the board so as to drive external equipment.&lt;/P&gt;&lt;P&gt;I am looking into the linux-boundary kernel files in yocto (dylan) build dir, but I cannot figure out where that is set.&lt;/P&gt;&lt;P&gt;To be honest I don't even know if i'll find that info there, but it seems like the right place to start (after googling about it of course).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So who determined the speed (standard mode, fast mode, etc) for the external i2c? if it is a driver , which one should I be looking for?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The reason is I am trying to drive some TMC222 low-power stepper motor control ICs, but they do not respond.&lt;/P&gt;&lt;P&gt;Note I have successfully connected a number of other i2c ICs (among others the pca9505x).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;An answer is not necessary. Any pointers as to how to go about it , so I can learn about this is more than welcome.&lt;/P&gt;&lt;P&gt;Thank you for your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Aug 2013 18:15:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/bus-speed-of-dev-i2c-2-on-imx6q/m-p/252858#M23510</guid>
      <dc:creator>synthnassizer</dc:creator>
      <dc:date>2013-08-13T18:15:08Z</dc:date>
    </item>
    <item>
      <title>Re: bus speed of /dev/i2c-2 on imx6q</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/bus-speed-of-dev-i2c-2-on-imx6q/m-p/252859#M23511</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Attached is the porting guide. I hope this is useful for you. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Aug 2013 09:28:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/bus-speed-of-dev-i2c-2-on-imx6q/m-p/252859#M23511</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2013-08-15T09:28:05Z</dc:date>
    </item>
  </channel>
</rss>