<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX8QXP RPMsg Device Tree Entries (Cortex-M4/A35) in linux 6.6 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-RPMsg-Device-Tree-Entries-Cortex-M4-A35-in-linux-6-6/m-p/2061334#M235059</link>
    <description>I have the same reset cause and no solution yet,&lt;BR /&gt;&lt;BR /&gt;I am using the scfw-1.17.0&lt;BR /&gt;&lt;BR /&gt;which one do you use ?</description>
    <pubDate>Thu, 13 Mar 2025 13:23:33 GMT</pubDate>
    <dc:creator>roodani</dc:creator>
    <dc:date>2025-03-13T13:23:33Z</dc:date>
    <item>
      <title>i.MX8QXP RPMsg Device Tree Entries (Cortex-M4/A35) in linux 6.6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-RPMsg-Device-Tree-Entries-Cortex-M4-A35-in-linux-6-6/m-p/2041905#M233884</link>
      <description>&lt;P&gt;Hello! I've run into an interesting problem with RPMsg communication between the Cortex-A35 and M4 cores on the IMX8QXP platform, and I could use some insights.&lt;/P&gt;&lt;P&gt;I'm working with Linux 6.6, and here's the situation: When I try to load the demo provided imx8qx_m4_TCM_rpmsg_lite_str_echo_rtos binary from U-boot, the system immediately restarts. Interestingly, the same setup works perfectly fine on Linux 5.15, which suggests something might have changed in the newer kernel version.&lt;/P&gt;&lt;P&gt;Here's my device tree configuration for reference:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;/ {

	reserved-memory {
		#address-cells = &amp;lt;2&amp;gt;;
		#size-cells = &amp;lt;2&amp;gt;;
		ranges;

		gpu_reserved: gpu_reserved@B0000000 {
			no-map;
			reg = &amp;lt;0 0xB0000000 0 0x08000000&amp;gt;;
		};

		vdev0vring0: vdev0vring0@90000000 {
			reg = &amp;lt;0 0x90000000 0 0x8000&amp;gt;;
			no-map;
		};

		vdev0vring1: vdev0vring1@90008000 {
			reg = &amp;lt;0 0x90008000 0 0x8000&amp;gt;;
			no-map;
		};

		vdev1vring0: vdev1vring0@90010000 {
			reg = &amp;lt;0 0x90010000 0 0x8000&amp;gt;;
			no-map;
		};

		vdev1vring1: vdev1vring1@90018000 {
			reg = &amp;lt;0 0x90018000 0 0x8000&amp;gt;;
			no-map;
		};

		rsc_table: rsc_table@900ff000 {
			reg = &amp;lt;0 0x900ff000 0 0x1000&amp;gt;;
			no-map;
		};

		vdevbuffer: vdevbuffer {
                        compatible = "shared-dma-pool";
			reg = &amp;lt;0 0x90400000 0 0x100000&amp;gt;;
 			no-map;
 		};

		dsp_reserved: dsp@92400000 {
			reg = &amp;lt;0 0x92400000 0 0x1000000&amp;gt;;
			no-map;
		};
		dsp_reserved_heap: dsp_reserved_heap {
			reg = &amp;lt;0 0x93400000 0 0xef0000&amp;gt;;
			no-map;
		};
		dsp_vdev0vring0: vdev0vring0@942f0000 {
			reg = &amp;lt;0 0x942f0000 0 0x8000&amp;gt;;
			no-map;
		};

		dsp_vdev0vring1: vdev0vring1@942f8000 {
			reg = &amp;lt;0 0x942f8000 0 0x8000&amp;gt;;
			no-map;
		};

		dsp_vdev0buffer: vdev0buffer@94300000 {
			compatible = "shared-dma-pool";
			reg = &amp;lt;0 0x94300000 0 0x100000&amp;gt;;
			no-map;
		};

		
		/* global autoconfigured region for contiguous allocations */
		linux,cma {
			compatible = "shared-dma-pool";
			reusable;
			size = &amp;lt;0 0x08000000&amp;gt;;
			alloc-ranges = &amp;lt;0 0xa8000000 0 0x08000000&amp;gt;;
			linux,cma-default;
		};
	};

	
	imx8x_cm4: imx8x_cm4@0 {
		compatible = "fsl,imx8qxp-cm4";
		rsc-da = &amp;lt;0x90000000&amp;gt;;
		mbox-names = "tx", "rx", "rxdb";
		mboxes = &amp;lt;&amp;amp;lsio_mu5 0 1
			  &amp;amp;lsio_mu5 1 1
			  &amp;amp;lsio_mu5 3 1&amp;gt;;
		memory-region = &amp;lt;&amp;amp;vdevbuffer&amp;gt;, &amp;lt;&amp;amp;vdev0vring0&amp;gt;, &amp;lt;&amp;amp;vdev0vring1&amp;gt;,
				&amp;lt;&amp;amp;vdev1vring0&amp;gt;, &amp;lt;&amp;amp;vdev1vring1&amp;gt;, &amp;lt;&amp;amp;rsc_table&amp;gt;;
		fsl,resource-id = &amp;lt;IMX_SC_R_M4_0_PID0&amp;gt;;
		fsl,entry-address = &amp;lt;0x34fe0000&amp;gt;;
		status = "okay";
		power-domains = &amp;lt;&amp;amp;pd IMX_SC_R_M4_0_PID0&amp;gt;,
				&amp;lt;&amp;amp;pd IMX_SC_R_M4_0_MU_1A&amp;gt;;
	};

	rpmsg: rpmsg@0 {
		compatible = "fsl,imx8qxp-rpmsg";
		mbox-names = "tx", "rx", "rxdb";
		mboxes = &amp;lt;&amp;amp;lsio_mu5 0 1
			  &amp;amp;lsio_mu5 1 1
			  &amp;amp;lsio_mu5 3 1&amp;gt;;
		memory-region = &amp;lt;&amp;amp;vdevbuffer&amp;gt;;
		mub-partition = &amp;lt;3&amp;gt;;
		status = "okay";
	};
};

&amp;amp;lsio_mu5 {
	status = "okay";
};&lt;/LI-CODE&gt;&lt;P&gt;My bootloader setup is straightforward:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;setenv m4_0_image "imx8qx_m4_TCM_rpmsg_lite_str_echo_rtos.bin"
run m4boot_0&lt;/LI-CODE&gt;&lt;P&gt;Has anyone encountered similar behaviour or have suggestions on what might be causing this regression in Linux 6.6? I'm particularly interested in:&lt;/P&gt;&lt;P&gt;- Changes in RPMsg handling between 5.15 and 6.6&lt;BR /&gt;- Potential memory mapping issues&lt;BR /&gt;- MU (Message Unit) configuration differences&lt;/P&gt;&lt;P&gt;Any insights or debugging suggestions would be greatly appreciated!&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;P.S : I noticed even if I run the sample demo&amp;nbsp;imx8qx_m4_TCM_hello_world.bin, I got the same issue.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 11 Feb 2025 15:52:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-RPMsg-Device-Tree-Entries-Cortex-M4-A35-in-linux-6-6/m-p/2041905#M233884</guid>
      <dc:creator>roodani</dc:creator>
      <dc:date>2025-02-11T15:52:57Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8QXP RPMsg Device Tree Entries (Cortex-M4/A35) in linux 6.6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-RPMsg-Device-Tree-Entries-Cortex-M4-A35-in-linux-6-6/m-p/2042881#M233942</link>
      <description>&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Fatload for M4 code load is usually used for mscale series M4 boot, A core will handle the load of M4 and start it. It is not suggested to be used in i.MX8/8X, because in 8/8X M core is parallel to A core. Fatload boot will break the relationship of A&amp;amp;M(A core and M core will be in one partition), and violate functions like Linux reboot(SCU will close the whole partition so M4 will be closed as well), board low power mode (SCU will handle this low power mode enter), etc…&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;&amp;nbsp;&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;For i.MX8QXP/QM, SCU_ROM will handle the load of M4 binary code, and we should inform SCU_ROM if we have M4 binary, in&amp;nbsp;imx-mkimage&amp;nbsp;by&amp;nbsp;soc.mak&amp;nbsp;file. SCU will create a seperate resource partition(generally partition 3) and based on that partition, there would be resource isolation(including memory region) between M core and A core.&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;&amp;nbsp;&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;To flash your own M4 image, please follow SDK doc "Getting Started with MCUXpresso SDK for MEK-MIMX8QXP" - "Run a demo using imx-mkimage".You need to build a flash.bin file with M4 by imx-mkimage, using "make SOC=iMX8QX REV=C0 flash_linux_m4". Then install the imx_rpmsg_tty.ko file by insmod command.&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;&amp;nbsp;&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;Best regards/Saludos,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Wed, 12 Feb 2025 22:01:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-RPMsg-Device-Tree-Entries-Cortex-M4-A35-in-linux-6-6/m-p/2042881#M233942</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2025-02-12T22:01:47Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8QXP RPMsg Device Tree Entries (Cortex-M4/A35) in linux 6.6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-RPMsg-Device-Tree-Entries-Cortex-M4-A35-in-linux-6-6/m-p/2060173#M234974</link>
      <description>&lt;BLOCKQUOTE&gt;&lt;P&gt;I also run into the same issue with Linux 6.6 on iMX8QuadMax. M4 firmware is loaded from U-boot. The M4 runs well if Linux kernel is not started. However, the entire system will reset if Linux kernel starts. The reset cause from U-boot is related to SCFW. But the same implement works on Linux 5.15.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Reset cause: SCFW fault reset&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Is it because of the SCFW upgrade?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Mar 2025 07:12:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-RPMsg-Device-Tree-Entries-Cortex-M4-A35-in-linux-6-6/m-p/2060173#M234974</guid>
      <dc:creator>Benjamin_Hu</dc:creator>
      <dc:date>2025-03-12T07:12:47Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8QXP RPMsg Device Tree Entries (Cortex-M4/A35) in linux 6.6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-RPMsg-Device-Tree-Entries-Cortex-M4-A35-in-linux-6-6/m-p/2061334#M235059</link>
      <description>I have the same reset cause and no solution yet,&lt;BR /&gt;&lt;BR /&gt;I am using the scfw-1.17.0&lt;BR /&gt;&lt;BR /&gt;which one do you use ?</description>
      <pubDate>Thu, 13 Mar 2025 13:23:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-RPMsg-Device-Tree-Entries-Cortex-M4-A35-in-linux-6-6/m-p/2061334#M235059</guid>
      <dc:creator>roodani</dc:creator>
      <dc:date>2025-03-13T13:23:33Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8QXP RPMsg Device Tree Entries (Cortex-M4/A35) in linux 6.6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-RPMsg-Device-Tree-Entries-Cortex-M4-A35-in-linux-6-6/m-p/2061649#M235077</link>
      <description>&lt;P&gt;It is 1.16.0 on my iMX8QM.&lt;/P&gt;</description>
      <pubDate>Fri, 14 Mar 2025 00:56:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-RPMsg-Device-Tree-Entries-Cortex-M4-A35-in-linux-6-6/m-p/2061649#M235077</guid>
      <dc:creator>Benjamin_Hu</dc:creator>
      <dc:date>2025-03-14T00:56:54Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8QXP RPMsg Device Tree Entries (Cortex-M4/A35) in linux 6.6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-RPMsg-Device-Tree-Entries-Cortex-M4-A35-in-linux-6-6/m-p/2062024#M235096</link>
      <description>&lt;P&gt;After a skim through the sdk user guide, I found that you can't use the bootaux command to run the m4 demos, It's surprising since I made it work in 5.15 fine.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot from 2025-03-14 10-19-26.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/328144i3AB2910575FBE9F6/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot from 2025-03-14 10-19-26.png" alt="Screenshot from 2025-03-14 10-19-26.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Screenshot from 2025-03-14 10-19-26.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I am trying to build my project, and see if I can run the M4 binary alongside u-boot. It will be run by scfw to my understanding.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I will update you as soon as I get something&lt;/P&gt;</description>
      <pubDate>Fri, 14 Mar 2025 10:21:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-RPMsg-Device-Tree-Entries-Cortex-M4-A35-in-linux-6-6/m-p/2062024#M235096</guid>
      <dc:creator>roodani</dc:creator>
      <dc:date>2025-03-14T10:21:59Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8QXP RPMsg Device Tree Entries (Cortex-M4/A35) in linux 6.6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-RPMsg-Device-Tree-Entries-Cortex-M4-A35-in-linux-6-6/m-p/2063442#M235191</link>
      <description>&lt;LI-SPOILER&gt;&lt;P&gt;can you explain in detail the cause of the problem from your knowledge and investigation so far? is the problem that running M4 Demo on the latest scfw is not the same way as linux 5.15 and below or is it just because the bootaux command can't work in this 6.6 version?&lt;/P&gt;&lt;P&gt;I'm quite interested to solve this problem too.&lt;/P&gt;&lt;/LI-SPOILER&gt;</description>
      <pubDate>Tue, 18 Mar 2025 05:30:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-RPMsg-Device-Tree-Entries-Cortex-M4-A35-in-linux-6-6/m-p/2063442#M235191</guid>
      <dc:creator>azkaaa</dc:creator>
      <dc:date>2025-03-18T05:30:28Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8QXP RPMsg Device Tree Entries (Cortex-M4/A35) in linux 6.6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-RPMsg-Device-Tree-Entries-Cortex-M4-A35-in-linux-6-6/m-p/2066253#M235382</link>
      <description>I am not sure what is the cause of the issue,&lt;BR /&gt;according to MCUExpresso documentation though, Bootaux is not longer supported because the A and M core must run on different partitions which is not the case when you run it from u-boot.&lt;BR /&gt;&lt;BR /&gt;Surprisingly, this worked just fine using the Linux 5.15 but in 6.6 SCFW detects an error reset the board (Reset cause: SCFW fault reset).&lt;BR /&gt;&lt;BR /&gt;With this info, I decided to launch the m4 binary using the SCFW, which can be achieved according to MCU_expresso docs using the flash_linux_m4 target in the imx_mkimage.&lt;BR /&gt;&lt;BR /&gt;For the sake of trial I managed to use the target flash_regression_linux_m4, which worked just fine, the M4 binary is loaded into memory and u-boot and linux are flashed, However after a power_cycle the M4 isn't launched which is expected because this target only loads in memory for the first time.&lt;BR /&gt;&lt;BR /&gt;The flash_linux_m4 uses spl but it gives an error at the moment :&lt;BR /&gt;SPL: failed to boot from all boot devices&lt;BR /&gt;### ERROR ### Please RESET the board ###&lt;BR /&gt;</description>
      <pubDate>Fri, 21 Mar 2025 10:03:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8QXP-RPMsg-Device-Tree-Entries-Cortex-M4-A35-in-linux-6-6/m-p/2066253#M235382</guid>
      <dc:creator>roodani</dc:creator>
      <dc:date>2025-03-21T10:03:26Z</dc:date>
    </item>
  </channel>
</rss>