<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx6ull i2c read and write failed in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6ull-i2c-read-and-write-failed/m-p/2060120#M234972</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks for the reply, with dmesg i checked the kernal log but i didnt see any error message related to i2c or camera.&lt;/P&gt;</description>
    <pubDate>Wed, 12 Mar 2025 06:38:45 GMT</pubDate>
    <dc:creator>Et_MM</dc:creator>
    <dc:date>2025-03-12T06:38:45Z</dc:date>
    <item>
      <title>imx6ull i2c read and write failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6ull-i2c-read-and-write-failed/m-p/2057559#M234801</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working on imx6ull based custom board. So in that board we have configured camera ov5640 under i2c.&lt;/P&gt;&lt;P&gt;root@imx6ul7d:~# i2cdetect -y 0&lt;BR /&gt;0 1 2 3 4 5 6 7 8 9 a b c d e f&lt;BR /&gt;00: -- -- -- -- -- -- -- --&lt;BR /&gt;10: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --&lt;BR /&gt;20: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --&lt;BR /&gt;30: -- -- -- -- -- -- -- -- -- -- -- -- &lt;STRONG&gt;UU&lt;/STRONG&gt; -- -- --&lt;BR /&gt;40: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --&lt;BR /&gt;50: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --&lt;BR /&gt;60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --&lt;BR /&gt;70: -- -- -- -- -- -- -- --&lt;/P&gt;&lt;P&gt;when i am trying to read or write showing failed.&lt;/P&gt;&lt;P&gt;root@imx6ul7d:~# i2cset -f -y 0 0x3c 0x32 0x12&lt;BR /&gt;Error: Write failed&lt;BR /&gt;&lt;BR /&gt;When i searched i saw like if we are loading driver we cant read or write. if driver not loaded&amp;nbsp; it should show slave address 3c but for me its not showing so can you give me solution for this is there any way i can write or read?&lt;/P&gt;&lt;P&gt;what all i have to write to i2c is there in the attachment. please have a look at it, hoping for your reply.&lt;/P&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 07 Mar 2025 06:20:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6ull-i2c-read-and-write-failed/m-p/2057559#M234801</guid>
      <dc:creator>Et_MM</dc:creator>
      <dc:date>2025-03-07T06:20:12Z</dc:date>
    </item>
    <item>
      <title>Re: imx6ull i2c read and write failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6ull-i2c-read-and-write-failed/m-p/2060051#M234963</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;The camera i2c is not loaded successfully by Linux, so the &lt;STRONG&gt;UU&lt;/STRONG&gt; showed and you can't control it. You can check the kernel boot log, there should be some errors.&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Wed, 12 Mar 2025 05:18:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6ull-i2c-read-and-write-failed/m-p/2060051#M234963</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2025-03-12T05:18:30Z</dc:date>
    </item>
    <item>
      <title>Re: imx6ull i2c read and write failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6ull-i2c-read-and-write-failed/m-p/2060120#M234972</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks for the reply, with dmesg i checked the kernal log but i didnt see any error message related to i2c or camera.&lt;/P&gt;</description>
      <pubDate>Wed, 12 Mar 2025 06:38:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6ull-i2c-read-and-write-failed/m-p/2060120#M234972</guid>
      <dc:creator>Et_MM</dc:creator>
      <dc:date>2025-03-12T06:38:45Z</dc:date>
    </item>
    <item>
      <title>Re: imx6ull i2c read and write failed</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6ull-i2c-read-and-write-failed/m-p/2064219#M235234</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;You can try to use v4l2-ctl to set or get specific registers.&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Wed, 19 Mar 2025 02:06:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6ull-i2c-read-and-write-failed/m-p/2064219#M235234</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2025-03-19T02:06:39Z</dc:date>
    </item>
  </channel>
</rss>