<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RS232 and USB detection is not happening at host side with imx6ull device in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RS232-and-USB-detection-is-not-happening-at-host-side-with/m-p/2059830#M234948</link>
    <description>&lt;P&gt;Please share the complete log of the issue in .txt format of the old and the new version.&lt;/P&gt;
&lt;P&gt;You are working with an old u-boot (2017), Is recommended to upgrade to&amp;nbsp;U-Boot v2024.04, if you have an EVK you can test it with the BSP in&amp;nbsp;&lt;A href="https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX" target="_blank"&gt;https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 11 Mar 2025 20:31:22 GMT</pubDate>
    <dc:creator>Oswalag</dc:creator>
    <dc:date>2025-03-11T20:31:22Z</dc:date>
    <item>
      <title>RS232 and USB detection is not happening at host side with imx6ull device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RS232-and-USB-detection-is-not-happening-at-host-side-with/m-p/2058689#M234860</link>
      <description>&lt;P&gt;I am trying to upgrade kernel from Linux kernel v4.1.15 to Linux kernel v6.6.36 for IMX6ULL ultralite. After upgrading Linux kernel with v6.6.36, RS232 and USB detection is not happening at host side while I am using u-boot version 2017.03.&lt;/P&gt;&lt;P&gt;Can anyone suggest what is wrong and in which direction I need to debug?&lt;/P&gt;</description>
      <pubDate>Mon, 10 Mar 2025 10:25:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RS232-and-USB-detection-is-not-happening-at-host-side-with/m-p/2058689#M234860</guid>
      <dc:creator>LoKi</dc:creator>
      <dc:date>2025-03-10T10:25:50Z</dc:date>
    </item>
    <item>
      <title>Re: RS232 and USB detection is not happening at host side with imx6ull device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RS232-and-USB-detection-is-not-happening-at-host-side-with/m-p/2058702#M234862</link>
      <description>&lt;P&gt;Device side RS232 and USB cable is able to identified.&lt;/P&gt;</description>
      <pubDate>Mon, 10 Mar 2025 10:46:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RS232-and-USB-detection-is-not-happening-at-host-side-with/m-p/2058702#M234862</guid>
      <dc:creator>LoKi</dc:creator>
      <dc:date>2025-03-10T10:46:18Z</dc:date>
    </item>
    <item>
      <title>Re: RS232 and USB detection is not happening at host side with imx6ull device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RS232-and-USB-detection-is-not-happening-at-host-side-with/m-p/2059830#M234948</link>
      <description>&lt;P&gt;Please share the complete log of the issue in .txt format of the old and the new version.&lt;/P&gt;
&lt;P&gt;You are working with an old u-boot (2017), Is recommended to upgrade to&amp;nbsp;U-Boot v2024.04, if you have an EVK you can test it with the BSP in&amp;nbsp;&lt;A href="https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX" target="_blank"&gt;https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 11 Mar 2025 20:31:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RS232-and-USB-detection-is-not-happening-at-host-side-with/m-p/2059830#M234948</guid>
      <dc:creator>Oswalag</dc:creator>
      <dc:date>2025-03-11T20:31:22Z</dc:date>
    </item>
  </channel>
</rss>