<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックCreate frame buffer without hdmi device</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Create-frame-buffer-without-hdmi-device/m-p/2057915#M234815</link>
    <description>&lt;UL&gt;&lt;LI&gt;Processor: iMX8M&lt;/LI&gt;&lt;LI&gt;System: Yocto with Wayland&amp;nbsp;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;I would like to play video immediately after the system starts. However, I encounter a problem when the HDMI cable isn't connected during system startup. In this situation, a frame buffer isn't created, which is correct in the normal situation. I can't start playing such situation.&amp;nbsp; Is there any way to create a frame buffer with specified resolution without detecting the HDMI device? The approach should continue to play the video after connecting the cable on a compatible screen.&lt;/P&gt;</description>
    <pubDate>Fri, 07 Mar 2025 13:46:46 GMT</pubDate>
    <dc:creator>kluszon</dc:creator>
    <dc:date>2025-03-07T13:46:46Z</dc:date>
    <item>
      <title>Create frame buffer without hdmi device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Create-frame-buffer-without-hdmi-device/m-p/2057915#M234815</link>
      <description>&lt;UL&gt;&lt;LI&gt;Processor: iMX8M&lt;/LI&gt;&lt;LI&gt;System: Yocto with Wayland&amp;nbsp;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;I would like to play video immediately after the system starts. However, I encounter a problem when the HDMI cable isn't connected during system startup. In this situation, a frame buffer isn't created, which is correct in the normal situation. I can't start playing such situation.&amp;nbsp; Is there any way to create a frame buffer with specified resolution without detecting the HDMI device? The approach should continue to play the video after connecting the cable on a compatible screen.&lt;/P&gt;</description>
      <pubDate>Fri, 07 Mar 2025 13:46:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Create-frame-buffer-without-hdmi-device/m-p/2057915#M234815</guid>
      <dc:creator>kluszon</dc:creator>
      <dc:date>2025-03-07T13:46:46Z</dc:date>
    </item>
    <item>
      <title>Re: Create frame buffer without hdmi device</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Create-frame-buffer-without-hdmi-device/m-p/2059050#M234889</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Unfortunately no, for video to continue to be played needs a sink (display).&lt;BR /&gt;&lt;BR /&gt;Best regards/Saludos,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Mon, 10 Mar 2025 22:48:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Create-frame-buffer-without-hdmi-device/m-p/2059050#M234889</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2025-03-10T22:48:02Z</dc:date>
    </item>
  </channel>
</rss>