<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Nitrogen6 SOM can not boot from SD card in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Nitrogen6-SOM-can-not-boot-from-SD-card/m-p/2056448#M234743</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Ezurio uses two different tools to flash the image,&amp;nbsp;via zcat and dd under Linux and&amp;nbsp;balenaEtcher.&lt;/P&gt;
&lt;P&gt;I suggest you follow the instructions recommended by the manufacturer.&lt;/P&gt;
&lt;P&gt;Also, please confirm that the processor part number of your board matches with the flashed image, if you are using the incorrect image can cause the issue you are seeing.&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
    <pubDate>Wed, 05 Mar 2025 16:50:42 GMT</pubDate>
    <dc:creator>JorgeCas</dc:creator>
    <dc:date>2025-03-05T16:50:42Z</dc:date>
    <item>
      <title>Nitrogen6 SOM can not boot from SD card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Nitrogen6-SOM-can-not-boot-from-SD-card/m-p/2056381#M234737</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;I am using the Nitrogen6 SOM V2&amp;nbsp; with the Nitrogen6 carrier board. I am following these instructions&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.ezurio.com/resources/software-announcements/yocto-gatesgarth-release-for-i-mx6-i-mx7-platforms" target="_blank"&gt;https://www.ezurio.com/resources/software-announcements/yocto-gatesgarth-release-for-i-mx6-i-mx7-platforms&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I use image&lt;BR /&gt;&lt;BR /&gt;&lt;A href="https://ezurio.com/eula?file=20210315-boundary-image-multimedia-full-nitrogen6x.wic.gz" target="_blank"&gt;20210315-boundary-image-multimedia-full-nitrogen6x.wic.gz&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;on the SD card. When I try to boot I get the error&lt;BR /&gt;&lt;BR /&gt;Press SPACE to abort autoboot in 0 seconds&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc0 is current device&lt;BR /&gt;Scanning mmc 0:1...&lt;BR /&gt;Found U-Boot script boot.scr&lt;BR /&gt;4898 bytes read in 15 ms (318.4 KiB/s)&lt;BR /&gt;## Executing script at 10008000&lt;BR /&gt;cpu2=6Q&lt;BR /&gt;cpu3=6Q&lt;BR /&gt;** Unable to read file uEnv.txt **&lt;BR /&gt;** Unable to read file imx6q-vml_cci.dtb **&lt;BR /&gt;!!!! Error loading imx6q-vml_cci.dtb&lt;BR /&gt;SCRIPT FAILED: continuing...&lt;BR /&gt;Found U-Boot script boot.scr&lt;BR /&gt;4898 bytes read in 15 ms (318.4 KiB/s)&lt;BR /&gt;## Executing script at 10008000&lt;BR /&gt;cpu2=6Q&lt;BR /&gt;cpu3=6Q&lt;BR /&gt;** Unable to read file uEnv.txt **&lt;BR /&gt;** Unable to read file imx6q-vml_cci.dtb **&lt;BR /&gt;!!!! Error loading imx6q-vml_cci.dtb&lt;BR /&gt;SCRIPT FAILED: continuing...&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 05 Mar 2025 15:18:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Nitrogen6-SOM-can-not-boot-from-SD-card/m-p/2056381#M234737</guid>
      <dc:creator>jbutler</dc:creator>
      <dc:date>2025-03-05T15:18:17Z</dc:date>
    </item>
    <item>
      <title>Re: Nitrogen6 SOM can not boot from SD card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Nitrogen6-SOM-can-not-boot-from-SD-card/m-p/2056448#M234743</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Ezurio uses two different tools to flash the image,&amp;nbsp;via zcat and dd under Linux and&amp;nbsp;balenaEtcher.&lt;/P&gt;
&lt;P&gt;I suggest you follow the instructions recommended by the manufacturer.&lt;/P&gt;
&lt;P&gt;Also, please confirm that the processor part number of your board matches with the flashed image, if you are using the incorrect image can cause the issue you are seeing.&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Wed, 05 Mar 2025 16:50:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Nitrogen6-SOM-can-not-boot-from-SD-card/m-p/2056448#M234743</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2025-03-05T16:50:42Z</dc:date>
    </item>
    <item>
      <title>Re: Nitrogen6 SOM can not boot from SD card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Nitrogen6-SOM-can-not-boot-from-SD-card/m-p/2059606#M234935</link>
      <description>&lt;P&gt;&lt;EM&gt;&amp;nbsp;&lt;/EM&gt;I am using the Nitrogen 6 SoM V2 and the image&lt;/P&gt;&lt;P&gt;&lt;A href="https://ezurio.com/eula?file=20220204-nitrogen6x-4.14.x_2.0.1_ga-bionic-en_US-console_armhf.img.gz" target="_blank" rel="noopener"&gt;20220204-nitrogen6x-4.14.x_2.0.1_ga-bionic-en_US-console_armhf.img.gz&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;I did&lt;/P&gt;&lt;P&gt;gunzip &lt;A href="https://ezurio.com/eula?file=20220204-nitrogen6x-4.14.x_2.0.1_ga-bionic-en_US-console_armhf.img.gz" target="_blank" rel="noopener"&gt;20220204-nitrogen6x-4.14.x_2.0.1_ga-bionic-en_US-console_armhf.img.gz&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;&lt;SPAN class=""&gt;sudo ddrescue -D --force &lt;A href="https://ezurio.com/eula?file=20220204-nitrogen6x-4.14.x_2.0.1_ga-bionic-en_US-console_armhf.img.gz" target="_blank" rel="noopener"&gt;20220204-nitrogen6x-4.14.x_2.0.1_ga-bionic-en_US-console_armhf.img&amp;nbsp;/dev/sda&lt;/A&gt;&lt;/SPAN&gt;&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;BR /&gt;as stated on the page&lt;BR /&gt;&lt;BR /&gt;&lt;A href="https://www.ezurio.com/resources/software-announcements/ubuntu-bionic-18-04-3-lts-for-i-mx6-7-boards-august-2019-kernel-4-14-x" target="_blank" rel="noopener"&gt;https://www.ezurio.com/resources/software-announcements/ubuntu-bionic-18-04-3-lts-for-i-mx6-7-boards-august-2019-kernel-4-14-x&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 11 Mar 2025 14:21:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Nitrogen6-SOM-can-not-boot-from-SD-card/m-p/2059606#M234935</guid>
      <dc:creator>jbutler</dc:creator>
      <dc:date>2025-03-11T14:21:23Z</dc:date>
    </item>
    <item>
      <title>Re: Nitrogen6 SOM can not boot from SD card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Nitrogen6-SOM-can-not-boot-from-SD-card/m-p/2117861#M238308</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;This is because you are trying to load a device tree which is not a standard device tree from Boundary Devices / Ezurio ( imx6q-vml_cci.dtb).&lt;BR /&gt;Please erase your U-Boot environment and you'll see the OS booting.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;</description>
      <pubDate>Tue, 17 Jun 2025 14:16:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Nitrogen6-SOM-can-not-boot-from-SD-card/m-p/2117861#M238308</guid>
      <dc:creator>gary_bisson</dc:creator>
      <dc:date>2025-06-17T14:16:48Z</dc:date>
    </item>
  </channel>
</rss>