<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックSuggest Dual Camera Solution</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Suggest-Dual-Camera-Solution/m-p/2055402#M234702</link>
    <description>&lt;P&gt;Hi iMX Champ !&lt;/P&gt;&lt;P&gt;A customer is looking for an MCU/MPU solution that can accept 2 or more channels of fisheye multi-camera (parallel or mipi csi) input and apply functions such as dewarping, crop, resize, rotate, etc.&lt;BR /&gt;They will be using automotive grade parts and are looking for chipsets from the iMX RT117x, iMX8X, and i.MX8 series that can meet their requirements.&lt;/P&gt;&lt;P&gt;I've looked through the datasheets and RMs on nxp.com, but I can't find any devices that support dewarping HW-wise, so if you have any recommendations for us to try, please let me know.&lt;/P&gt;&lt;P&gt;If certain features can't be handled HW, it would be nice to see how they can be partially implemented in SW. i.e. opencv, opencl, pxp&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;Best Regards, Jack&lt;/P&gt;</description>
    <pubDate>Tue, 04 Mar 2025 09:33:05 GMT</pubDate>
    <dc:creator>JK-IMX</dc:creator>
    <dc:date>2025-03-04T09:33:05Z</dc:date>
    <item>
      <title>Suggest Dual Camera Solution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Suggest-Dual-Camera-Solution/m-p/2055402#M234702</link>
      <description>&lt;P&gt;Hi iMX Champ !&lt;/P&gt;&lt;P&gt;A customer is looking for an MCU/MPU solution that can accept 2 or more channels of fisheye multi-camera (parallel or mipi csi) input and apply functions such as dewarping, crop, resize, rotate, etc.&lt;BR /&gt;They will be using automotive grade parts and are looking for chipsets from the iMX RT117x, iMX8X, and i.MX8 series that can meet their requirements.&lt;/P&gt;&lt;P&gt;I've looked through the datasheets and RMs on nxp.com, but I can't find any devices that support dewarping HW-wise, so if you have any recommendations for us to try, please let me know.&lt;/P&gt;&lt;P&gt;If certain features can't be handled HW, it would be nice to see how they can be partially implemented in SW. i.e. opencv, opencl, pxp&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;Best Regards, Jack&lt;/P&gt;</description>
      <pubDate>Tue, 04 Mar 2025 09:33:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Suggest-Dual-Camera-Solution/m-p/2055402#M234702</guid>
      <dc:creator>JK-IMX</dc:creator>
      <dc:date>2025-03-04T09:33:05Z</dc:date>
    </item>
    <item>
      <title>Re: Suggest Dual Camera Solution</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Suggest-Dual-Camera-Solution/m-p/2055677#M234711</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/191000"&gt;@JK-IMX&lt;/a&gt;!&lt;BR /&gt;Thank you for contacting NXP Support!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For your application I can recommend the iMX8 or the iMX95.&lt;/P&gt;
&lt;P&gt;If you want to run Machine Learning Models you should use the iMX95 due to the iMX95 has an NPU to accelerate the ML models.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please check the specs of the&lt;A href="https://www.nxp.com/products/iMX95" target="_self"&gt; i.MX95 Processor.&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards!&lt;/P&gt;
&lt;P&gt;Chavira&lt;/P&gt;</description>
      <pubDate>Tue, 04 Mar 2025 17:13:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Suggest-Dual-Camera-Solution/m-p/2055677#M234711</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2025-03-04T17:13:24Z</dc:date>
    </item>
  </channel>
</rss>