<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: [iMX8QM-MEK] How to stop: Power Mode Switch Application in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-How-to-stop-Power-Mode-Switch-Application/m-p/2054345#M234632</link>
    <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/246856"&gt;@ChrisC05&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm not currently evaluate this, so I haven't tested it, but please try the following method.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Enter commands on the serial console&lt;/P&gt;&lt;P&gt;- Stop the application&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;systemctl stop power-mode-switch&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- Stop the application from starting automatically&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;systemctl disable power-mode-switch&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Similarly, you can write&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;exec systemctl stop power-mode-switch&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;in the on boot section of init.rc.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please let me know if there are any developments.&lt;/P&gt;</description>
    <pubDate>Mon, 03 Mar 2025 04:13:35 GMT</pubDate>
    <dc:creator>sushi_happy</dc:creator>
    <dc:date>2025-03-03T04:13:35Z</dc:date>
    <item>
      <title>[iMX8QM-MEK] How to stop: Power Mode Switch Application</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-How-to-stop-Power-Mode-Switch-Application/m-p/1459585#M190484</link>
      <description>&lt;P&gt;Hi,all.&lt;/P&gt;&lt;P&gt;When connecting to the RS-232C connector (J37) of imx8qm-mek, a message about the "Power Mode Switch" application is output.&lt;BR /&gt;I want to stop this application.&lt;BR /&gt;What should I do?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;#################### Power Mode Switch Task ####################&lt;/P&gt;&lt;P&gt;Build Time: Aug 10 2021--13:43:40&lt;BR /&gt;Core Clock: 264000000Hz&lt;BR /&gt;Power mode: RUN&lt;/P&gt;&lt;P&gt;Select the desired operation&lt;/P&gt;&lt;P&gt;Press A for enter: RUN - Normal RUN mode&lt;BR /&gt;Press B for enter: WAIT - Wait mode&lt;BR /&gt;Press C for enter: STOP - Stop mode&lt;BR /&gt;Press D for enter: VLPR - Very Low Power Run mode&lt;BR /&gt;Press E for enter: VLPW - Very Low Power Wait mode&lt;BR /&gt;Press F for enter: VLPS - Very Low Power Stop mode&lt;BR /&gt;Press G for enter: LLS - Low Leakage Stop mode&lt;BR /&gt;Press H for enter: VLLS - Very Low Leakage Stop mode&lt;BR /&gt;Press R for using WDOG trigger M4 partition reset.&lt;/P&gt;&lt;P&gt;Waiting for power mode select..&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 18 May 2022 01:31:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-How-to-stop-Power-Mode-Switch-Application/m-p/1459585#M190484</guid>
      <dc:creator>sushi_happy</dc:creator>
      <dc:date>2022-05-18T01:31:03Z</dc:date>
    </item>
    <item>
      <title>Re: [iMX8QM-MEK] How to stop: Power Mode Switch Application</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-How-to-stop-Power-Mode-Switch-Application/m-p/1482747#M192066</link>
      <description>&lt;P&gt;Sorry for miss your thread and late reply.&lt;/P&gt;
&lt;DIV id="bodyDisplay_6" class="lia-message-body lia-component-message-view-widget-body lia-component-body-signature-highlight-escalation lia-component-message-view-widget-body-signature-highlight-escalation"&gt;
&lt;DIV class="lia-message-body-content"&gt;
&lt;P&gt;The ttyLP2 is enabled by default BSP. You can test it.&lt;/P&gt;
&lt;P&gt;The hardware for ttyLP2 is on the base board as J37(DB9 connector).&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;The hardware for&amp;nbsp;ttyLP2 is on the base board as J37(DB9 connector).&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;you need a usb to&amp;nbsp; uart DB9 to connect the J37(DB9 connector).&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;/DIV&gt;
&lt;/DIV&gt;</description>
      <pubDate>Thu, 30 Jun 2022 11:35:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-How-to-stop-Power-Mode-Switch-Application/m-p/1482747#M192066</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2022-06-30T11:35:19Z</dc:date>
    </item>
    <item>
      <title>Re: [iMX8QM-MEK] How to stop: Power Mode Switch Application</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-How-to-stop-Power-Mode-Switch-Application/m-p/1483163#M192090</link>
      <description>&lt;P&gt;Thank you&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/57740"&gt;@Rita_Wang&lt;/a&gt;&amp;nbsp;.&lt;/P&gt;&lt;P&gt;But,I know that.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please tell me how to disable it.&lt;/P&gt;</description>
      <pubDate>Fri, 01 Jul 2022 03:58:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-How-to-stop-Power-Mode-Switch-Application/m-p/1483163#M192090</guid>
      <dc:creator>sushi_happy</dc:creator>
      <dc:date>2022-07-01T03:58:58Z</dc:date>
    </item>
    <item>
      <title>Re: [iMX8QM-MEK] How to stop: Power Mode Switch Application</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-How-to-stop-Power-Mode-Switch-Application/m-p/2052970#M234543</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any update to this? I am running into the same issue.&lt;/P&gt;</description>
      <pubDate>Thu, 27 Feb 2025 12:52:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-How-to-stop-Power-Mode-Switch-Application/m-p/2052970#M234543</guid>
      <dc:creator>ChrisC05</dc:creator>
      <dc:date>2025-02-27T12:52:16Z</dc:date>
    </item>
    <item>
      <title>Re: [iMX8QM-MEK] How to stop: Power Mode Switch Application</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-How-to-stop-Power-Mode-Switch-Application/m-p/2054345#M234632</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/246856"&gt;@ChrisC05&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm not currently evaluate this, so I haven't tested it, but please try the following method.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Enter commands on the serial console&lt;/P&gt;&lt;P&gt;- Stop the application&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;systemctl stop power-mode-switch&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- Stop the application from starting automatically&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;systemctl disable power-mode-switch&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Similarly, you can write&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;exec systemctl stop power-mode-switch&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;in the on boot section of init.rc.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please let me know if there are any developments.&lt;/P&gt;</description>
      <pubDate>Mon, 03 Mar 2025 04:13:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-How-to-stop-Power-Mode-Switch-Application/m-p/2054345#M234632</guid>
      <dc:creator>sushi_happy</dc:creator>
      <dc:date>2025-03-03T04:13:35Z</dc:date>
    </item>
    <item>
      <title>Re: [iMX8QM-MEK] How to stop: Power Mode Switch Application</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-How-to-stop-Power-Mode-Switch-Application/m-p/2054500#M234647</link>
      <description>&lt;P&gt;Hey &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/200167"&gt;@sushi_happy&lt;/a&gt;&lt;/P&gt;&lt;P&gt;Thank you for responding.&lt;/P&gt;&lt;P&gt;I tried your instructions however the power mode switch application seems to be loaded on the M4 core before U-boot even gives me the chance to enter auto-boot, and using `systemctl disable power-mode-service` returns "Failed to disable unit: Unit file power-mode-switch.service does not exist." in the kernel.&lt;/P&gt;&lt;P&gt;I'm not quite sure how to proceed from here.&lt;/P&gt;</description>
      <pubDate>Mon, 03 Mar 2025 07:55:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-How-to-stop-Power-Mode-Switch-Application/m-p/2054500#M234647</guid>
      <dc:creator>ChrisC05</dc:creator>
      <dc:date>2025-03-03T07:55:46Z</dc:date>
    </item>
    <item>
      <title>Re: [iMX8QM-MEK] How to stop: Power Mode Switch Application</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-How-to-stop-Power-Mode-Switch-Application/m-p/2054594#M234653</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/246856"&gt;@ChrisC05&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sorry.&lt;/P&gt;&lt;P&gt;By default, resources are assigned to User CM4_1 for Power_Mode_Switch and the settings cannot be changed.&lt;/P&gt;&lt;P&gt;m4_1_image.bin&amp;nbsp; (\android_build\vender\nxp-opensource\imx-mkimage\iMX8QM)&lt;/P&gt;&lt;P&gt;I Think this file contains information about Power_Mode_Switch.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Download the MCUXpresso SDK, build an empty source code like&lt;/P&gt;&lt;LI-CODE lang="c"&gt;main()
{
    while(1){
    }
}&lt;/LI-CODE&gt;&lt;P&gt;and replace it with the generated .bin file.&lt;/P&gt;&lt;P&gt;Power_Mode_Switch should stop.&lt;/P&gt;&lt;P&gt;If you write something like&lt;/P&gt;&lt;LI-CODE lang="c"&gt;printf("Hello World\n");&lt;/LI-CODE&gt;&lt;P&gt;A string will be output.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, this is information from an older version, so there may be differences.&lt;/P&gt;&lt;P&gt;Also, if you want to use ttyLP2, etc., it is assigned to a different M4 core, so communication will not be possible with just the above changes.&lt;/P&gt;</description>
      <pubDate>Mon, 03 Mar 2025 09:30:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QM-MEK-How-to-stop-Power-Mode-Switch-Application/m-p/2054594#M234653</guid>
      <dc:creator>sushi_happy</dc:creator>
      <dc:date>2025-03-03T09:30:09Z</dc:date>
    </item>
  </channel>
</rss>