<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 IMX8MP - Delay between two consecutive SPI write</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-Delay-between-two-consecutive-SPI-write/m-p/2053274#M234568</link>
    <description>&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;I am interfacing a DAC module through SPI (ECSPI-1) with MPU. The clock is setup at 30MHz and what I have observed between two immediate consecutive calls (without any delay) of spi_write (implemented within kernel device driver for DAC) I am observing a delay of 4us between the clocks of these two transfers. The data that I am writing is 24 bits long and according to my application I need to write this data continuously and more frequently for which I need to bring this delay down to some ~800-900ns.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Below are my queries :&lt;BR /&gt;&amp;nbsp;1. If I am not implementing any API calls or specifically adding any delays what is the reason for this idle time of 4us?&lt;/P&gt;&lt;P&gt;2. How can I overcome this delay and meet my requirement?&lt;BR /&gt;&lt;BR /&gt;Any help or suggestions would be greatly appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Bhavin&lt;BR /&gt;&lt;BR /&gt;&lt;LI-PRODUCT title="IMX8MPLUS" id="IMX8MPLUS"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 27 Feb 2025 20:09:30 GMT</pubDate>
    <dc:creator>Bhavin-Sharma</dc:creator>
    <dc:date>2025-02-27T20:09:30Z</dc:date>
    <item>
      <title>IMX8MP - Delay between two consecutive SPI write</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-Delay-between-two-consecutive-SPI-write/m-p/2053274#M234568</link>
      <description>&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;I am interfacing a DAC module through SPI (ECSPI-1) with MPU. The clock is setup at 30MHz and what I have observed between two immediate consecutive calls (without any delay) of spi_write (implemented within kernel device driver for DAC) I am observing a delay of 4us between the clocks of these two transfers. The data that I am writing is 24 bits long and according to my application I need to write this data continuously and more frequently for which I need to bring this delay down to some ~800-900ns.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Below are my queries :&lt;BR /&gt;&amp;nbsp;1. If I am not implementing any API calls or specifically adding any delays what is the reason for this idle time of 4us?&lt;/P&gt;&lt;P&gt;2. How can I overcome this delay and meet my requirement?&lt;BR /&gt;&lt;BR /&gt;Any help or suggestions would be greatly appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Bhavin&lt;BR /&gt;&lt;BR /&gt;&lt;LI-PRODUCT title="IMX8MPLUS" id="IMX8MPLUS"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 27 Feb 2025 20:09:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-Delay-between-two-consecutive-SPI-write/m-p/2053274#M234568</guid>
      <dc:creator>Bhavin-Sharma</dc:creator>
      <dc:date>2025-02-27T20:09:30Z</dc:date>
    </item>
  </channel>
</rss>