<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX8MP: Get unique ID to set FIELD RETURN UID in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-Get-unique-ID-to-set-FIELD-RETURN-UID/m-p/2051964#M234500</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;The i.MX8MP reference says the unique ID is split over several fuses, but specifically 0x420 seems a bit off. Is 0x420[10:0] leading, or is UNIQUE_ID[42:0] leading? If the former, where are the missing 31 bits?&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
    <pubDate>Wed, 26 Feb 2025 16:58:00 GMT</pubDate>
    <dc:creator>Bayou</dc:creator>
    <dc:date>2025-02-26T16:58:00Z</dc:date>
    <item>
      <title>i.MX8MP: Get unique ID to set FIELD RETURN UID</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-Get-unique-ID-to-set-FIELD-RETURN-UID/m-p/2051964#M234500</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;The i.MX8MP reference says the unique ID is split over several fuses, but specifically 0x420 seems a bit off. Is 0x420[10:0] leading, or is UNIQUE_ID[42:0] leading? If the former, where are the missing 31 bits?&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Wed, 26 Feb 2025 16:58:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-Get-unique-ID-to-set-FIELD-RETURN-UID/m-p/2051964#M234500</guid>
      <dc:creator>Bayou</dc:creator>
      <dc:date>2025-02-26T16:58:00Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8MP: Get unique ID to set FIELD RETURN UID</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-Get-unique-ID-to-set-FIELD-RETURN-UID/m-p/2053115#M234556</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products,&lt;/P&gt;
&lt;P&gt;The 42:0 is the correct value, seems like they missed it and it's an error. But the correct value is 42:0.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 27 Feb 2025 16:22:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-Get-unique-ID-to-set-FIELD-RETURN-UID/m-p/2053115#M234556</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2025-02-27T16:22:29Z</dc:date>
    </item>
  </channel>
</rss>