<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックiMX8MP - WebGPU has been disabled via blocklist or the command line</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-WebGPU-has-been-disabled-via-blocklist-or-the-command/m-p/2050668#M234418</link>
    <description>&lt;P&gt;From chromium v117 running on iMX8MP I see the following item in the chrome://gpu page:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;WebGPU has been disabled via blocklist or the command line.&lt;/LI&gt;&lt;/UL&gt;&lt;P class="lia-indent-padding-left-30px"&gt;Disabled Features: webgpu&lt;/P&gt;&lt;P&gt;Is this expected?&lt;/P&gt;&lt;P&gt;I see &lt;A href="https://developer.chrome.com/docs/web-platform/webgpu/troubleshooting-tips" target="_self"&gt;here&lt;/A&gt; some possible reasons, but I don't know which ones apply to the iMX8MP hardware architecture.&lt;/P&gt;&lt;P&gt;Should I pass&lt;/P&gt;&lt;PRE&gt;&lt;SPAN class=""&gt;--enable-unsafe-webgpu&lt;/SPAN&gt;&lt;/PRE&gt;&lt;P&gt;command line parameter to chromium?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Or is this feature unsupported on the iMX8MP hardware?&lt;/P&gt;</description>
    <pubDate>Tue, 25 Feb 2025 09:29:45 GMT</pubDate>
    <dc:creator>vix</dc:creator>
    <dc:date>2025-02-25T09:29:45Z</dc:date>
    <item>
      <title>iMX8MP - WebGPU has been disabled via blocklist or the command line</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-WebGPU-has-been-disabled-via-blocklist-or-the-command/m-p/2050668#M234418</link>
      <description>&lt;P&gt;From chromium v117 running on iMX8MP I see the following item in the chrome://gpu page:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;WebGPU has been disabled via blocklist or the command line.&lt;/LI&gt;&lt;/UL&gt;&lt;P class="lia-indent-padding-left-30px"&gt;Disabled Features: webgpu&lt;/P&gt;&lt;P&gt;Is this expected?&lt;/P&gt;&lt;P&gt;I see &lt;A href="https://developer.chrome.com/docs/web-platform/webgpu/troubleshooting-tips" target="_self"&gt;here&lt;/A&gt; some possible reasons, but I don't know which ones apply to the iMX8MP hardware architecture.&lt;/P&gt;&lt;P&gt;Should I pass&lt;/P&gt;&lt;PRE&gt;&lt;SPAN class=""&gt;--enable-unsafe-webgpu&lt;/SPAN&gt;&lt;/PRE&gt;&lt;P&gt;command line parameter to chromium?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Or is this feature unsupported on the iMX8MP hardware?&lt;/P&gt;</description>
      <pubDate>Tue, 25 Feb 2025 09:29:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-WebGPU-has-been-disabled-via-blocklist-or-the-command/m-p/2050668#M234418</guid>
      <dc:creator>vix</dc:creator>
      <dc:date>2025-02-25T09:29:45Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8MP - WebGPU has been disabled via blocklist or the command line</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-WebGPU-has-been-disabled-via-blocklist-or-the-command/m-p/2050985#M234441</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Currently WebGPU are not supported by MX8MP in latest BSP, but is pure software.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Tue, 25 Feb 2025 16:37:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-WebGPU-has-been-disabled-via-blocklist-or-the-command/m-p/2050985#M234441</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2025-02-25T16:37:57Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8MP - WebGPU has been disabled via blocklist or the command line</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-WebGPU-has-been-disabled-via-blocklist-or-the-command/m-p/2051646#M234481</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/34846"&gt;@Bio_TICFSL&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;do you mean that even with the flags suggested by your colleague &lt;A href="https://community.nxp.com/t5/i-MX-Graphics/WebGPU-Vulkan-Support-on-i-MX8MP-QtWebEngine-6-7-0/m-p/2027230" target="_self"&gt;here&lt;/A&gt;, the implementation is full software?&lt;/P&gt;</description>
      <pubDate>Wed, 26 Feb 2025 10:08:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-WebGPU-has-been-disabled-via-blocklist-or-the-command/m-p/2051646#M234481</guid>
      <dc:creator>vix</dc:creator>
      <dc:date>2025-02-26T10:08:32Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8MP - WebGPU has been disabled via blocklist or the command line</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-WebGPU-has-been-disabled-via-blocklist-or-the-command/m-p/2051933#M234498</link>
      <description>&lt;P&gt;That;s correct!&lt;/P&gt;</description>
      <pubDate>Wed, 26 Feb 2025 16:24:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-WebGPU-has-been-disabled-via-blocklist-or-the-command/m-p/2051933#M234498</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2025-02-26T16:24:12Z</dc:date>
    </item>
  </channel>
</rss>