<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMX8ULP A core Wake up using GPIO in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8ULP-A-core-Wake-up-using-GPIO/m-p/2049692#M234361</link>
    <description>&lt;DIV class=""&gt;Hello,&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;I'm using the i.MX8ULP and have connected two push buttons to PTE11 and PTE14. Now A core is in sleep mode and M core is Running, and I want to wake up the A core when a button is pressed.&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;However, after checking the reference manual, I found that PTE11 and PTE14 are not linked to WUU1. So, is it possible to wake up the A core using these pins? If yes, how can I do that?&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;If not, can I at least get an interrupt on the M core when these buttons are pressed? Is there any way to use these pins on the M core?&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;Thanks!&lt;/DIV&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;</description>
    <pubDate>Mon, 24 Feb 2025 07:40:09 GMT</pubDate>
    <dc:creator>YashParekh</dc:creator>
    <dc:date>2025-02-24T07:40:09Z</dc:date>
    <item>
      <title>IMX8ULP A core Wake up using GPIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8ULP-A-core-Wake-up-using-GPIO/m-p/2049692#M234361</link>
      <description>&lt;DIV class=""&gt;Hello,&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;I'm using the i.MX8ULP and have connected two push buttons to PTE11 and PTE14. Now A core is in sleep mode and M core is Running, and I want to wake up the A core when a button is pressed.&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;However, after checking the reference manual, I found that PTE11 and PTE14 are not linked to WUU1. So, is it possible to wake up the A core using these pins? If yes, how can I do that?&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;If not, can I at least get an interrupt on the M core when these buttons are pressed? Is there any way to use these pins on the M core?&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;Thanks!&lt;/DIV&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Mon, 24 Feb 2025 07:40:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8ULP-A-core-Wake-up-using-GPIO/m-p/2049692#M234361</guid>
      <dc:creator>YashParekh</dc:creator>
      <dc:date>2025-02-24T07:40:09Z</dc:date>
    </item>
  </channel>
</rss>