<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Reducing ECSPI CS High Time Without Using DMA in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Reducing-ECSPI-CS-High-Time-Without-Using-DMA/m-p/2048945#M234314</link>
    <description>&lt;P&gt;Please find below an inline answer.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is your 2.2 us / 5 us at the beginning of the SPI burst, or are you seeing those between byte transmissions?&lt;/P&gt;&lt;P&gt;Ans. in between byte transfers, we have observed this delay&amp;nbsp;&lt;/P&gt;&lt;P&gt;What is the SCLK that SPI is working with?&lt;BR /&gt;Ans. 30 MHz&lt;/P&gt;&lt;P&gt;How to eliminate this delay to increase spi sampling due to this delay, it is adding ~5 us delay in every transaction. We are not able to achieve the SPI-required speed.&lt;/P&gt;</description>
    <pubDate>Fri, 21 Feb 2025 09:16:08 GMT</pubDate>
    <dc:creator>mehul_dabhi</dc:creator>
    <dc:date>2025-02-21T09:16:08Z</dc:date>
    <item>
      <title>Reducing ECSPI CS High Time Without Using DMA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reducing-ECSPI-CS-High-Time-Without-Using-DMA/m-p/2047203#M234204</link>
      <description>&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;I am facing an issue where the Chip Select (CS) remains high for approximately 5 µs.&lt;/P&gt;&lt;P&gt;Initially, while using DMA, I observed an extended CS low time of around 2.2 µs before the SCLK (Serial Clock) starts. I received a suggestion to use native CS with DMA disabled.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;[Here is the&amp;nbsp;&lt;/SPAN&gt;&lt;A title="link" href="https://community.nxp.com/t5/i-MX-Processors/Reducing-CS-Low-Time-Before-Starting-SCLK-in-SPI-Communication/m-p/2020938#M232510" target="_blank" rel="noopener"&gt;link&lt;/A&gt;&lt;SPAN&gt;&amp;nbsp; to the entire discussion.]&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Now, I have disabled DMA and am using native CS for the SPI peripheral, but I still observe that CS remains high for approximately 5 µs.&lt;/P&gt;&lt;P&gt;Even when I increase the SPI clock speed, the idle time of CS remains almost unchanged, while the low time (transaction time) improves.&lt;/P&gt;&lt;P&gt;Can you please tell what's causing this issue? And any steps to resolve it?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any help / suggestions would be appreciated&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Mehul&lt;/P&gt;</description>
      <pubDate>Wed, 19 Feb 2025 09:57:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reducing-ECSPI-CS-High-Time-Without-Using-DMA/m-p/2047203#M234204</guid>
      <dc:creator>mehul_dabhi</dc:creator>
      <dc:date>2025-02-19T09:57:44Z</dc:date>
    </item>
    <item>
      <title>Re: Reducing ECSPI CS High Time Without Using DMA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reducing-ECSPI-CS-High-Time-Without-Using-DMA/m-p/2048464#M234294</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products,&lt;/P&gt;
&lt;P&gt;Is your 2.2 us / 5 us at the beginning of the SPI burst or are you seeing those between byte transmissions?&lt;/P&gt;
&lt;P&gt;What is the SCLK that SPI is working with?&lt;/P&gt;
&lt;P&gt;Seems like it's a natural delay since the time is really short, but we will confirm it.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 20 Feb 2025 18:19:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reducing-ECSPI-CS-High-Time-Without-Using-DMA/m-p/2048464#M234294</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2025-02-20T18:19:24Z</dc:date>
    </item>
    <item>
      <title>Re: Reducing ECSPI CS High Time Without Using DMA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reducing-ECSPI-CS-High-Time-Without-Using-DMA/m-p/2048945#M234314</link>
      <description>&lt;P&gt;Please find below an inline answer.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is your 2.2 us / 5 us at the beginning of the SPI burst, or are you seeing those between byte transmissions?&lt;/P&gt;&lt;P&gt;Ans. in between byte transfers, we have observed this delay&amp;nbsp;&lt;/P&gt;&lt;P&gt;What is the SCLK that SPI is working with?&lt;BR /&gt;Ans. 30 MHz&lt;/P&gt;&lt;P&gt;How to eliminate this delay to increase spi sampling due to this delay, it is adding ~5 us delay in every transaction. We are not able to achieve the SPI-required speed.&lt;/P&gt;</description>
      <pubDate>Fri, 21 Feb 2025 09:16:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reducing-ECSPI-CS-High-Time-Without-Using-DMA/m-p/2048945#M234314</guid>
      <dc:creator>mehul_dabhi</dc:creator>
      <dc:date>2025-02-21T09:16:08Z</dc:date>
    </item>
    <item>
      <title>Re: Reducing ECSPI CS High Time Without Using DMA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Reducing-ECSPI-CS-High-Time-Without-Using-DMA/m-p/2050023#M234380</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206442"&gt;@JosephAtNXP&lt;/a&gt;&amp;nbsp;,&lt;BR /&gt;&lt;BR /&gt;The issue was related to the burst transfer initialisation, not in the byte transfer.&lt;BR /&gt;And for your reference, I am attaching the snap of the 2us delay too.&lt;BR /&gt;&lt;BR /&gt;The Blue one is SCLK signal&lt;BR /&gt;and the yellow one is CS signal.&lt;BR /&gt;&lt;BR /&gt;Let me know if you require anything to recreate the issue and to debug it further.&lt;/P&gt;</description>
      <pubDate>Mon, 24 Feb 2025 14:54:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Reducing-ECSPI-CS-High-Time-Without-Using-DMA/m-p/2050023#M234380</guid>
      <dc:creator>mehul_dabhi</dc:creator>
      <dc:date>2025-02-24T14:54:44Z</dc:date>
    </item>
  </channel>
</rss>