<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Directly connected output of the microprocessor B25 (RTC_XTALO) to the 0V8 power supply</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Directly-connected-output-of-the-microprocessor-B25-RTC-XTALO-to/m-p/2046655#M234158</link>
    <description>&lt;P&gt;Hello.&lt;/P&gt;
&lt;P&gt;It is correct,&amp;nbsp;&lt;SPAN&gt;0Ohm resistor is used for testing purposes on the EVK.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;According to the datasheet, RTC_XTALO should be directly connected to VDD_SNVS_0P8, then 1k ohm is not necessary.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Regards.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 18 Feb 2025 20:20:02 GMT</pubDate>
    <dc:creator>Oswalag</dc:creator>
    <dc:date>2025-02-18T20:20:02Z</dc:date>
    <item>
      <title>Directly connected output of the microprocessor B25 (RTC_XTALO) to the 0V8 power supply</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Directly-connected-output-of-the-microprocessor-B25-RTC-XTALO-to/m-p/2044515#M234020</link>
      <description>&lt;P&gt;Have a nice day!&lt;/P&gt;&lt;P&gt;During a detailed study of the demo board electrical scheme for the IMX8MMini, I noticed that the output of the microprocessor B25 (RTC_XTALO) is directly connected to the 0V8 power supply.&lt;/P&gt;&lt;P&gt;Based on the above, please respond:&lt;/P&gt;&lt;P&gt;1) is this a mistake ?&lt;/P&gt;&lt;P&gt;2) is it allowed to connect the output of the RTC_XTALO microprocessor directly to the 0V8 power supply via a 0Ohm resistor ?&lt;/P&gt;&lt;P&gt;I think it's best to connect this pin B25 (RTC_XTALO) to the 0V8 power supply via a 1kOhm resistor !&lt;/P&gt;&lt;P&gt;What do you think about it ?&lt;/P&gt;&lt;P&gt;Looking forward to hearing from you.&lt;/P&gt;&lt;P&gt;Thanks a lot,&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Andrey Myachkov&lt;/P&gt;</description>
      <pubDate>Fri, 14 Feb 2025 11:25:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Directly-connected-output-of-the-microprocessor-B25-RTC-XTALO-to/m-p/2044515#M234020</guid>
      <dc:creator>AndreyMyachkov</dc:creator>
      <dc:date>2025-02-14T11:25:42Z</dc:date>
    </item>
    <item>
      <title>Re: Directly connected output of the microprocessor B25 (RTC_XTALO) to the 0V8 power supply</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Directly-connected-output-of-the-microprocessor-B25-RTC-XTALO-to/m-p/2046655#M234158</link>
      <description>&lt;P&gt;Hello.&lt;/P&gt;
&lt;P&gt;It is correct,&amp;nbsp;&lt;SPAN&gt;0Ohm resistor is used for testing purposes on the EVK.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;According to the datasheet, RTC_XTALO should be directly connected to VDD_SNVS_0P8, then 1k ohm is not necessary.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Regards.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 18 Feb 2025 20:20:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Directly-connected-output-of-the-microprocessor-B25-RTC-XTALO-to/m-p/2046655#M234158</guid>
      <dc:creator>Oswalag</dc:creator>
      <dc:date>2025-02-18T20:20:02Z</dc:date>
    </item>
    <item>
      <title>Re: Directly connected output of the microprocessor B25 (RTC_XTALO) to the 0V8 power supply</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Directly-connected-output-of-the-microprocessor-B25-RTC-XTALO-to/m-p/2047235#M234209</link>
      <description>&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;Thanks a lot for your reply.&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;P&gt;Andrew&lt;/P&gt;</description>
      <pubDate>Wed, 19 Feb 2025 10:32:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Directly-connected-output-of-the-microprocessor-B25-RTC-XTALO-to/m-p/2047235#M234209</guid>
      <dc:creator>AndreyMyachkov</dc:creator>
      <dc:date>2025-02-19T10:32:14Z</dc:date>
    </item>
  </channel>
</rss>