<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックiMX93evk RemoteProc</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX93evk-RemoteProc/m-p/2046403#M234140</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have an iMX93evk board, with a single boot (both A55 and M33 are running), with rpmsg dts and also rpmsg in the M33.&lt;/P&gt;&lt;P&gt;I am also able to use remoteproc to stop the M33 after the board full boot.&lt;/P&gt;&lt;P&gt;I followed the steps to set the path to the .elf file:&lt;/P&gt;&lt;P&gt;- &lt;STRONG&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;echo ~/x.elf &amp;gt; /sys/devices/platform/imx93-cm33/remoteproc/remoteproc0/firmware&lt;/FONT&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;followed by an echo start &amp;gt; state.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;In the kernel output:&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;remoteproc0: Booting fw image /usr/lib/firmware/imx93-11x11-evk_m33_TCM_rpmsg_lite_pingpong_rtos_linux_remote.elf&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;SError Interrupt on CPU1, code 0x00000000be000011 -- SError&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;....&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;pc : __memcpy+0x13c/0x240&lt;BR /&gt;lr : rproc_start+0x64/0x1b4 &lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The problem seems to be in the rproc_start which causes the kernel panic during a memcpy.&lt;/P&gt;&lt;P&gt;Any idea of may be causing this? I looked to the M33 linker file, memory is aligned. Do you have ideas on how to proceed debugging?&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 18 Feb 2025 13:42:12 GMT</pubDate>
    <dc:creator>rti</dc:creator>
    <dc:date>2025-02-18T13:42:12Z</dc:date>
    <item>
      <title>iMX93evk RemoteProc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX93evk-RemoteProc/m-p/2046403#M234140</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have an iMX93evk board, with a single boot (both A55 and M33 are running), with rpmsg dts and also rpmsg in the M33.&lt;/P&gt;&lt;P&gt;I am also able to use remoteproc to stop the M33 after the board full boot.&lt;/P&gt;&lt;P&gt;I followed the steps to set the path to the .elf file:&lt;/P&gt;&lt;P&gt;- &lt;STRONG&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;echo ~/x.elf &amp;gt; /sys/devices/platform/imx93-cm33/remoteproc/remoteproc0/firmware&lt;/FONT&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;followed by an echo start &amp;gt; state.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;In the kernel output:&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;remoteproc0: Booting fw image /usr/lib/firmware/imx93-11x11-evk_m33_TCM_rpmsg_lite_pingpong_rtos_linux_remote.elf&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;SError Interrupt on CPU1, code 0x00000000be000011 -- SError&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;....&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;pc : __memcpy+0x13c/0x240&lt;BR /&gt;lr : rproc_start+0x64/0x1b4 &lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The problem seems to be in the rproc_start which causes the kernel panic during a memcpy.&lt;/P&gt;&lt;P&gt;Any idea of may be causing this? I looked to the M33 linker file, memory is aligned. Do you have ideas on how to proceed debugging?&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 18 Feb 2025 13:42:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX93evk-RemoteProc/m-p/2046403#M234140</guid>
      <dc:creator>rti</dc:creator>
      <dc:date>2025-02-18T13:42:12Z</dc:date>
    </item>
  </channel>
</rss>