<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to use UUU for standalone kernel build? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-use-UUU-for-standalone-kernel-build/m-p/2044967#M234050</link>
    <description>&lt;P&gt;I have successfully used UUU to install a yocto built kernel I don't know how to use it to install a &lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/How-to-compile-Linux-Kernel-Image-and-device-tree-using-Yocto/ta-p/2022759" target="_self"&gt;standalone kernel build&lt;/A&gt;.&amp;nbsp;Although there is more than a little information on how to use it (&lt;A href="https://github.com/nxp-imx/mfgtools/wiki" target="_blank"&gt;https://github.com/nxp-imx/mfgtools/wiki&lt;/A&gt;&amp;nbsp;and the PDF that is linked in the github release area), I find the information lacking. There are lots of example, but none seem to be what I'm trying to do. What I want is a reference not a long list of examples. What exactly are all the command options and what exactly does each one do/mean/imply?&lt;/P&gt;&lt;P&gt;(FWIW, some think that examples are better than reference, but I disagree. Reference is better IMO and examples are useful for reinforcing reference info. Further, sometimes people use the term reference implementation when they mean example.)&lt;/P&gt;&lt;P&gt;It seems that a standalone build produces a kernel image and a DTB; well several versions of both. I think Image is the kernel image (based on the name) and I find an imx8mn-evk.dtb which seems like the DTB I want to use.&amp;nbsp;I don't think that standalone build generates uboot; don't know if I need that to use UUU.&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, how do I use UUU to put that onto a board? One of these?&lt;/P&gt;&lt;P&gt;uuu emmc Image&lt;/P&gt;&lt;P&gt;uuu emmc_all Image&lt;/P&gt;&lt;P&gt;How do I specify the DTB?&lt;/P&gt;</description>
    <pubDate>Sun, 16 Feb 2025 19:14:42 GMT</pubDate>
    <dc:creator>chillinwithscb</dc:creator>
    <dc:date>2025-02-16T19:14:42Z</dc:date>
    <item>
      <title>How to use UUU for standalone kernel build?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-use-UUU-for-standalone-kernel-build/m-p/2044967#M234050</link>
      <description>&lt;P&gt;I have successfully used UUU to install a yocto built kernel I don't know how to use it to install a &lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/How-to-compile-Linux-Kernel-Image-and-device-tree-using-Yocto/ta-p/2022759" target="_self"&gt;standalone kernel build&lt;/A&gt;.&amp;nbsp;Although there is more than a little information on how to use it (&lt;A href="https://github.com/nxp-imx/mfgtools/wiki" target="_blank"&gt;https://github.com/nxp-imx/mfgtools/wiki&lt;/A&gt;&amp;nbsp;and the PDF that is linked in the github release area), I find the information lacking. There are lots of example, but none seem to be what I'm trying to do. What I want is a reference not a long list of examples. What exactly are all the command options and what exactly does each one do/mean/imply?&lt;/P&gt;&lt;P&gt;(FWIW, some think that examples are better than reference, but I disagree. Reference is better IMO and examples are useful for reinforcing reference info. Further, sometimes people use the term reference implementation when they mean example.)&lt;/P&gt;&lt;P&gt;It seems that a standalone build produces a kernel image and a DTB; well several versions of both. I think Image is the kernel image (based on the name) and I find an imx8mn-evk.dtb which seems like the DTB I want to use.&amp;nbsp;I don't think that standalone build generates uboot; don't know if I need that to use UUU.&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, how do I use UUU to put that onto a board? One of these?&lt;/P&gt;&lt;P&gt;uuu emmc Image&lt;/P&gt;&lt;P&gt;uuu emmc_all Image&lt;/P&gt;&lt;P&gt;How do I specify the DTB?&lt;/P&gt;</description>
      <pubDate>Sun, 16 Feb 2025 19:14:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-use-UUU-for-standalone-kernel-build/m-p/2044967#M234050</guid>
      <dc:creator>chillinwithscb</dc:creator>
      <dc:date>2025-02-16T19:14:42Z</dc:date>
    </item>
    <item>
      <title>Re: How to use UUU for standalone kernel build?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-use-UUU-for-standalone-kernel-build/m-p/2046779#M234170</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;You can find the uuu script in the demo image, which can be used to update the bootloader, kernel image, dtb, and rootfs, update all of them or parts of them.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Zhiming_Liu_0-1739930758845.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/324622iB29871240B45ACD2/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Zhiming_Liu_0-1739930758845.png" alt="Zhiming_Liu_0-1739930758845.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Here you can copy from below.&amp;nbsp;fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.zst.u-boot can be got from demo image.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;uuu_version 1.2.39

# Please Replace below items with actually file names
# @_flash.bin			| boot loader
# @_Image			| kernel image, arm64 is Image, arm32 it is zImage
# @_board.dtb			| board dtb file
# @_initramfs.cpio.zst.uboot	| mfgtool init ramfs
# @_rootfs.tar.zst		| rootfs
# @_uTee.tar			| optee image, put dummy _uTee.tar file here if platform is not MX6/MX7*

# This command will be run when i.MX6/7 i.MX8MM, i.MX8MQ
SDP: boot -f _flash.bin

# This command will be run when ROM support stream mode
# i.MX8QXP, i.MX8QM
SDPS: boot -f _flash.bin

# These commands will be run when use SPL and will be skipped if no spl
# SDPU will be deprecated. please use SDPV instead of SDPU
# {
SDPU: delay 1000
SDPU: write -f _flash.bin -offset 0x57c00
SDPU: jump
# }

# These commands will be run when use SPL and will be skipped if no spl
# if (SPL support SDPV)
# {
SDPV: delay 1000
SDPV: write -f _flash.bin -skipspl
SDPV: jump
# }

# use uboot burn bootloader to eMMC
# becaue difference chip, offset is difference
# you can use kernel to do that for specific boards
FB: ucmd setenv fastboot_dev mmc
FB: ucmd setenv mmcdev ${emmc_dev}
FB: flash bootloader _flash.bin

FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi;

FB: ucmd setenv emmc_cmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0
FB: ucmd if test "${emmc_skip_fb}" != "yes"; then run emmc_cmd; fi
FB: ucmd setenv emmc_cmd mmc bootbus ${emmc_dev} 2 0 1;
FB: ucmd if test "${emmc_skip_fb}" != "yes"; then run emmc_cmd; fi

FB: ucmd setenv fastboot_buffer ${loadaddr}
FB: download -f _Image
FB: ucmd setenv fastboot_buffer ${fdt_addr}
FB: download -f _board.dtb
FB: ucmd setenv fastboot_buffer ${initrd_addr}
FB: download -f _initramfs.cpio.zst.uboot
#FB: ucmd setenv bootargs console=${console},${baudrate} earlycon=${earlycon},${baudrate}
FB: acmd ${kboot} ${loadaddr} ${initrd_addr} ${fdt_addr}

# get mmc dev number from kernel command line
# Wait for emmc
FBK: ucmd while [ ! -e /dev/mmcblk*boot0 ]; do sleep 1; echo "wait for /dev/mmcblk*boot* appear"; done;

# serach emmc device number, if your platform have more than two emmc chip, please echo dev number &amp;gt;/tmp/mmcdev 
FBK: ucmd dev=`ls /dev/mmcblk*boot*`; dev=($dev); dev=${dev[0]}; dev=${dev#/dev/mmcblk}; dev=${dev%boot*}; echo $dev &amp;gt; /tmp/mmcdev;

# dd to clear the possible MBR
FBK: ucmd mmc=`cat /tmp/mmcdev`; dd if=/dev/zero of=/dev/mmcblk${mmc} bs=512 count=1
# create partition
FBK: ucmd mmc=`cat /tmp/mmcdev`; PARTSTR=$'10M,500M,0c\n600M,,83\n'; echo "$PARTSTR" | sfdisk --force /dev/mmcblk${mmc}

FBK: ucmd mmc=`cat /tmp/mmcdev`; dd if=/dev/zero of=/dev/mmcblk${mmc} bs=1k seek=4096 count=1
FBK: ucmd sync
# you can enable below command to write boot partition. but offset is difference at difference platform
#FBK: ucmd mmc=`cat /tmp/mmcdev`; echo 0 &amp;gt; /sys/block/mmcblk${mmc}boot0/force_ro
#FBK: ucp  _flash.bin t:/tmp
#FBK: ucmd mmc=`cat /tmp/mmcdev`; dd if=/tmp/_flash.bin of=/dev/mmc${mmc}boot0 bs=1K seek=32
#FBK: ucmd mmc=`cat /tmp/mmcdev`; echo 1 &amp;gt; /sys/block/mmcblk${mmc}boot0/force_ro
FBK: ucmd mmc=`cat /tmp/mmcdev`; while [ ! -e /dev/mmcblk${mmc}p1 ]; do sleep 1; done
FBK: ucmd mmc=`cat /tmp/mmcdev`; mkfs.vfat /dev/mmcblk${mmc}p1
FBK: ucmd mmc=`cat /tmp/mmcdev`; mkdir -p /mnt/fat
FBK: ucmd mmc=`cat /tmp/mmcdev`; mount -t vfat /dev/mmcblk${mmc}p1 /mnt/fat
FBK: ucp  _Image t:/mnt/fat
FBK: ucp  _board.dtb t:/mnt/fat
FBK: ucp  _uTee.tar t:/tmp/op.tar
FBK: ucmd tar --no-same-owner -xf /tmp/op.tar -C /mnt/fat
FBK: ucmd umount /mnt/fat
FBK: ucmd mmc=`cat /tmp/mmcdev`; mkfs.ext3 -F -E nodiscard /dev/mmcblk${mmc}p2
FBK: ucmd mkdir -p /mnt/ext3
FBK: ucmd mmc=`cat /tmp/mmcdev`; mount /dev/mmcblk${mmc}p2 /mnt/ext3
FBK: acmd export EXTRACT_UNSAFE_SYMLINKS=1; tar --zstd --warning=no-timestamp -x -C /mnt/ext3
FBK: ucp  _rootfs.tar.zst t:-
FBK: Sync
FBK: ucmd umount /mnt/ext3
FBK: DONE

&lt;/LI-CODE&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Wed, 19 Feb 2025 02:08:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-use-UUU-for-standalone-kernel-build/m-p/2046779#M234170</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2025-02-19T02:08:38Z</dc:date>
    </item>
  </channel>
</rss>