<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックandroid UI format not match issue on imx7d android-pie</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/android-UI-format-not-match-issue-on-imx7d-android-pie/m-p/2039619#M233711</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;I'm porting a new LCD to my imx7d DIY development board.&lt;/P&gt;&lt;P&gt;kernel: 4.14&lt;/P&gt;&lt;P&gt;android: 9&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; Screen size is 320x240, physical format is RGB565. And I get a very weird issue. The main screen and some android applications can showing correctly. But some android applications are not refresh.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; If I do further debugging, I can find in FbDisplay.cpp, the updateScreen() function report buffer format is RGBA8888 but config format is RGB565, so the refresh operation is stopped.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;If I force the&amp;nbsp;&lt;/P&gt;&lt;P&gt;getBE().mRenderEngine =&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;RE::impl::RenderEngine::create(HAL_PIXEL_FORMAT_RGBA_8888&amp;nbsp;&lt;/P&gt;&lt;P&gt;to be&amp;nbsp;&lt;/P&gt;&lt;P&gt;getBE().mRenderEngine =&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; RE::impl::RenderEngine::create(HAL_PIXEL_FORMAT_RGB_565&lt;/P&gt;&lt;P&gt;those android application can show on the screen, but red and blue pixel are oppsite. If I use this method, I can't monitor the screen on my PC.&lt;/P&gt;&lt;P&gt;I want to know what thing cause this format not match issue and how do I perfectly fix it?&lt;/P&gt;</description>
    <pubDate>Fri, 07 Feb 2025 00:25:16 GMT</pubDate>
    <dc:creator>patrickzhang1024</dc:creator>
    <dc:date>2025-02-07T00:25:16Z</dc:date>
    <item>
      <title>android UI format not match issue on imx7d android-pie</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android-UI-format-not-match-issue-on-imx7d-android-pie/m-p/2039619#M233711</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;I'm porting a new LCD to my imx7d DIY development board.&lt;/P&gt;&lt;P&gt;kernel: 4.14&lt;/P&gt;&lt;P&gt;android: 9&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; Screen size is 320x240, physical format is RGB565. And I get a very weird issue. The main screen and some android applications can showing correctly. But some android applications are not refresh.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; If I do further debugging, I can find in FbDisplay.cpp, the updateScreen() function report buffer format is RGBA8888 but config format is RGB565, so the refresh operation is stopped.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;If I force the&amp;nbsp;&lt;/P&gt;&lt;P&gt;getBE().mRenderEngine =&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;RE::impl::RenderEngine::create(HAL_PIXEL_FORMAT_RGBA_8888&amp;nbsp;&lt;/P&gt;&lt;P&gt;to be&amp;nbsp;&lt;/P&gt;&lt;P&gt;getBE().mRenderEngine =&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; RE::impl::RenderEngine::create(HAL_PIXEL_FORMAT_RGB_565&lt;/P&gt;&lt;P&gt;those android application can show on the screen, but red and blue pixel are oppsite. If I use this method, I can't monitor the screen on my PC.&lt;/P&gt;&lt;P&gt;I want to know what thing cause this format not match issue and how do I perfectly fix it?&lt;/P&gt;</description>
      <pubDate>Fri, 07 Feb 2025 00:25:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android-UI-format-not-match-issue-on-imx7d-android-pie/m-p/2039619#M233711</guid>
      <dc:creator>patrickzhang1024</dc:creator>
      <dc:date>2025-02-07T00:25:16Z</dc:date>
    </item>
    <item>
      <title>Re: android UI format not match issue on imx7d android-pie</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android-UI-format-not-match-issue-on-imx7d-android-pie/m-p/2040550#M233784</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;This may have something to do with the code of the application that is having problems, the application is using 32bit data, so in the HAL layer code the return is RGB888. You need to look at the code of the application again to try to fix the problem.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://github.com/nxp-imx-android/android-imx_platform_hardware_imx/blob/p9.0.0_2.3.4/display/display/FbDisplay.cpp#L457C1-L462C6" target="_blank"&gt;https://github.com/nxp-imx-android/android-imx_platform_hardware_imx/blob/p9.0.0_2.3.4/display/display/FbDisplay.cpp#L457C1-L462C6&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Mon, 10 Feb 2025 03:07:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android-UI-format-not-match-issue-on-imx7d-android-pie/m-p/2040550#M233784</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2025-02-10T03:07:20Z</dc:date>
    </item>
    <item>
      <title>Re: android UI format not match issue on imx7d android-pie</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android-UI-format-not-match-issue-on-imx7d-android-pie/m-p/2040580#M233786</link>
      <description>&lt;P&gt;Hi Zhiming,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; Do you mean it might be something wrong in the android kotlin application? The config.format in Fbdisplay is all right, and I think the issue is comes from surfaceflinger. The buffer.format remains RGBA8888.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Patrick Zhang&lt;/P&gt;</description>
      <pubDate>Mon, 10 Feb 2025 03:57:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android-UI-format-not-match-issue-on-imx7d-android-pie/m-p/2040580#M233786</guid>
      <dc:creator>patrickzhang1024</dc:creator>
      <dc:date>2025-02-10T03:57:55Z</dc:date>
    </item>
    <item>
      <title>Re: android UI format not match issue on imx7d android-pie</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android-UI-format-not-match-issue-on-imx7d-android-pie/m-p/2042109#M233892</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;As my understanding about &lt;SPAN&gt;surfaceflinger&lt;/SPAN&gt;, the&amp;nbsp;&lt;SPAN&gt;surfaceflinger is a Render Engine, it receives the operations from application layer&amp;nbsp; and then call the fbdisplay to display. So the issue could from application layer, the app tells Render Engine how to render a frame. I don't think the Render Engine is designed for one pixel format, the pixel format should be set from the app layer.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Wed, 12 Feb 2025 01:30:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android-UI-format-not-match-issue-on-imx7d-android-pie/m-p/2042109#M233892</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2025-02-12T01:30:44Z</dc:date>
    </item>
    <item>
      <title>Re: android UI format not match issue on imx7d android-pie</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/android-UI-format-not-match-issue-on-imx7d-android-pie/m-p/2042174#M233900</link>
      <description>&lt;P&gt;Hi Zhiming,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; Thank you with your suggestion. I already find out a solution to fix that issue. By rotate the screen orientation in kotlin project. Probably, layout height is too long for android framework to resize. I should change the width:height in my layout.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;PatrickZ&lt;/P&gt;</description>
      <pubDate>Wed, 12 Feb 2025 03:13:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/android-UI-format-not-match-issue-on-imx7d-android-pie/m-p/2042174#M233900</guid>
      <dc:creator>patrickzhang1024</dc:creator>
      <dc:date>2025-02-12T03:13:53Z</dc:date>
    </item>
  </channel>
</rss>