<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.MX93 Linux reboot not working</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-Linux-reboot-not-working/m-p/2039359#M233698</link>
    <description>&lt;P&gt;We have a custom board based on i.MX93 running with Linux 6.6.52, and in principle everything works fine.&lt;/P&gt;&lt;P&gt;But calling &lt;EM&gt;reboot&lt;/EM&gt; stuck at the end and does not restart the CPU and the board.&lt;/P&gt;&lt;P&gt;In U-Boot the command &lt;EM&gt;reset&lt;/EM&gt; works perfect.&lt;/P&gt;&lt;P&gt;I followed the calls and can see, both, U-Boot and Linux kernel, calls&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp; invoke_psci_fn(PSCI_0_2_FN_SYSTEM_RESET, 0, 0, 0);&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;In U-Boot the CPU restarts, in Linux nothing is happening after that PSCI call.&lt;/P&gt;&lt;P&gt;I tried &lt;EM&gt;CONFIG_ARM_PSCI_CHECKER &lt;/EM&gt;to see if PSCI is working and the tests done during Linux boot finished with success.&lt;/P&gt;&lt;P&gt;So it looks like the according PSCI call &lt;EM&gt;PSCI_0_2_FN_SYSTEM_RESET&lt;/EM&gt; is not working correct under Linux.&lt;/P&gt;&lt;P&gt;Any idea what could be the reason?&lt;/P&gt;</description>
    <pubDate>Thu, 06 Feb 2025 14:29:58 GMT</pubDate>
    <dc:creator>PBoerner</dc:creator>
    <dc:date>2025-02-06T14:29:58Z</dc:date>
    <item>
      <title>i.MX93 Linux reboot not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-Linux-reboot-not-working/m-p/2039359#M233698</link>
      <description>&lt;P&gt;We have a custom board based on i.MX93 running with Linux 6.6.52, and in principle everything works fine.&lt;/P&gt;&lt;P&gt;But calling &lt;EM&gt;reboot&lt;/EM&gt; stuck at the end and does not restart the CPU and the board.&lt;/P&gt;&lt;P&gt;In U-Boot the command &lt;EM&gt;reset&lt;/EM&gt; works perfect.&lt;/P&gt;&lt;P&gt;I followed the calls and can see, both, U-Boot and Linux kernel, calls&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp; invoke_psci_fn(PSCI_0_2_FN_SYSTEM_RESET, 0, 0, 0);&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;In U-Boot the CPU restarts, in Linux nothing is happening after that PSCI call.&lt;/P&gt;&lt;P&gt;I tried &lt;EM&gt;CONFIG_ARM_PSCI_CHECKER &lt;/EM&gt;to see if PSCI is working and the tests done during Linux boot finished with success.&lt;/P&gt;&lt;P&gt;So it looks like the according PSCI call &lt;EM&gt;PSCI_0_2_FN_SYSTEM_RESET&lt;/EM&gt; is not working correct under Linux.&lt;/P&gt;&lt;P&gt;Any idea what could be the reason?&lt;/P&gt;</description>
      <pubDate>Thu, 06 Feb 2025 14:29:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX93-Linux-reboot-not-working/m-p/2039359#M233698</guid>
      <dc:creator>PBoerner</dc:creator>
      <dc:date>2025-02-06T14:29:58Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX93 Linux reboot not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-Linux-reboot-not-working/m-p/2061998#M235094</link>
      <description>&lt;P&gt;Solved!&lt;/P&gt;&lt;P&gt;In old version of imx93.dtsi only watchdog 3 (wdog3) is available and activated by default. In newer version several watchdogs are available and disabled by default. So you have to activate them explicitly by setting status to okay.&lt;/P&gt;&lt;P&gt;And it seems that wdog3 is needed for the reboot in the Linux system.&lt;/P&gt;&lt;P&gt;So after explicitly activating wdog3 via the device tree reboot is working.&lt;/P&gt;</description>
      <pubDate>Fri, 14 Mar 2025 10:02:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX93-Linux-reboot-not-working/m-p/2061998#M235094</guid>
      <dc:creator>PBoerner</dc:creator>
      <dc:date>2025-03-14T10:02:20Z</dc:date>
    </item>
  </channel>
</rss>