<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Internal error: Oops - Undefined instruction: 0000000002000000 [#1] PREEMPT SMP</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Internal-error-Oops-Undefined-instruction-0000000002000000-1/m-p/2026738#M232936</link>
    <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/231093"&gt;@srinivas_123&lt;/a&gt;Hello, have you solved this problem? I'm facing samilar problem with mainline kernel for imx93, this happens on every boot&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;[ 0.135496] nxp-pca9450 1-0025: No IRQ configured?&lt;BR /&gt;[ 0.434467] SError Interrupt on CPU0, code 0x00000000be000011 -- SError&lt;BR /&gt;[ 0.434479] CPU: 0 PID: 0 Comm: swapper/0 Not tainted 6.1.124 #4&lt;BR /&gt;[ 0.434484] Hardware name: ATK-DLIMX93 Development board (DT)&lt;BR /&gt;[ 0.434487] pstate: 404000c9 (nZcv daIF +PAN -UAO -TCO -DIT -SSBS BTYPE=--)&lt;BR /&gt;[ 0.434492] pc : tick_handle_oneshot_broadcast+0x0/0x250&lt;BR /&gt;[ 0.434504] lr : sysctr_timer_interrupt+0x34/0x40&lt;BR /&gt;[ 0.434511] sp : ffff800008003f20&lt;BR /&gt;[ 0.434513] x29: ffff800008003f20 x28: ffff800009fc3f80 x27: ffff8000096c8a38&lt;BR /&gt;[ 0.434522] x26: 0000000000000000 x25: 0000000019e52f48 x24: 0000000018644585&lt;BR /&gt;[ 0.434528] x23: ffff00000001b200 x22: 000000000000000e x21: 0000000000000000&lt;BR /&gt;[ 0.434534] x20: ffff00000001b2dc x19: ffff000000004b00 x18: fffffffffffe3ce0&lt;BR /&gt;[ 0.434539] x17: ffff8000363c2000 x16: ffff800008000000 x15: 0000000000000038&lt;BR /&gt;[ 0.434545] x14: 0000000000000197 x13: 0000000000000000 x12: 0000000000000000&lt;BR /&gt;[ 0.434551] x11: 0000000000000040 x10: ffff000000008170 x9 : ffff000000008168&lt;BR /&gt;[ 0.434556] x8 : ffff000002800948 x7 : 0000000000000000 x6 : 0000000000000000&lt;BR /&gt;[ 0.434562] x5 : ffff000002800920 x4 : ffff8000363c2000 x3 : ffff8000097d6500&lt;BR /&gt;[ 0.434567] x2 : 0000000000000000 x1 : ffff800008127e94 x0 : ffff80000a2ea840&lt;BR /&gt;[ 0.434575] Kernel panic - not syncing: Asynchronous SError Interrupt&lt;BR /&gt;[ 0.434578] CPU: 0 PID: 0 Comm: swapper/0 Not tainted 6.1.124 #4&lt;BR /&gt;[ 0.434582] Hardware name: ATK-DLIMX93 Development board (DT)&lt;/P&gt;&lt;P&gt;[ 0.434584] Call trace:&lt;BR /&gt;[ 0.434586] dump_backtrace.part.0+0xd8/0xe4&lt;BR /&gt;[ 0.434594] show_stack+0x14/0x20&lt;BR /&gt;[ 0.434599] dump_stack_lvl+0x60/0x78&lt;BR /&gt;[ 0.434605] dump_stack+0x14/0x2c&lt;BR /&gt;[ 0.434609] panic+0x17c/0x33c&lt;BR /&gt;[ 0.434615] add_taint+0x0/0xbc&lt;BR /&gt;[ 0.434620] arm64_serror_panic+0x68/0x74&lt;BR /&gt;[ 0.434624] do_serror+0x0/0x50&lt;BR /&gt;[ 0.434627] do_serror+0x30/0x50&lt;BR /&gt;[ 0.434630] el1h_64_error_handler+0x2c/0x40&lt;BR /&gt;[ 0.434635] el1h_64_error+0x64/0x68&lt;BR /&gt;[ 0.434638] tick_handle_oneshot_broadcast+0x0/0x250&lt;BR /&gt;[ 0.434643] __handle_irq_event_percpu+0x44/0x150&lt;BR /&gt;[ 0.434649] handle_irq_event+0x48/0xac&lt;BR /&gt;[ 0.434654] handle_fasteoi_irq+0xa0/0x190&lt;BR /&gt;[ 0.434660] generic_handle_domain_irq+0x28/0x40&lt;BR /&gt;[ 0.434664] gic_handle_irq+0x4c/0x124&lt;BR /&gt;[ 0.434672] call_on_irq_stack+0x24/0x40&lt;BR /&gt;[ 0.434676] do_interrupt_handler+0x78/0x80&lt;BR /&gt;[ 0.434680] el1_interrupt+0x30/0x60&lt;BR /&gt;[ 0.434684] el1h_64_irq_handler+0x14/0x20&lt;BR /&gt;[ 0.434689] el1h_64_irq+0x64/0x68&lt;BR /&gt;[ 0.434692] cpuidle_enter_state+0x12c/0x2f0&lt;BR /&gt;[ 0.434699] cpuidle_enter+0x34/0x50&lt;BR /&gt;[ 0.434703] do_idle+0x220/0x2b0&lt;BR /&gt;[ 0.434708] cpu_startup_entry+0x34/0x40&lt;BR /&gt;[ 0.434713] kernel_init+0x0/0x130&lt;BR /&gt;[ 0.434718] arch_post_acpi_subsys_init+0x0/0x8&lt;BR /&gt;[ 0.434725] start_kernel+0x64c/0x688&lt;BR /&gt;[ 0.434730] __primary_switched+0xbc/0xc4&lt;BR /&gt;[ 0.434737] SMP: stopping secondary CPUs&lt;BR /&gt;[ 0.434742] Kernel Offset: disabled&lt;BR /&gt;[ 0.434743] CPU features: 0x060000,000400a4,6600721b&lt;BR /&gt;[ 0.434747] Memory Limit: none&lt;/P&gt;&lt;/BLOCKQUOTE&gt;</description>
    <pubDate>Mon, 13 Jan 2025 12:26:07 GMT</pubDate>
    <dc:creator>PerrZhang</dc:creator>
    <dc:date>2025-01-13T12:26:07Z</dc:date>
    <item>
      <title>Internal error: Oops - Undefined instruction: 0000000002000000 [#1] PREEMPT SMP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Internal-error-Oops-Undefined-instruction-0000000002000000-1/m-p/1997976#M231026</link>
      <description>&lt;P&gt;i am using imx8mplus custom board . i build the IMXLXYOCTOUG v.LF6.6.3_1.0.0 BSP .&lt;/P&gt;&lt;P&gt;i add the variable in local.conf file to increase the roofts size :&lt;BR /&gt;IMAGE_ROOTFS_SIZE = "47185920"&lt;/P&gt;&lt;P&gt;i build the imx-image-full.&lt;/P&gt;&lt;P&gt;i used the 64 gb SD card&lt;/P&gt;&lt;P&gt;i flashed the wic.zst image into sd card by using the below command&lt;/P&gt;&lt;P&gt;zstdcat imx-image-full-imx8mp-lpddr4-evk.rootfs.wic.zst | sudo dd of=/dev/sdb bs=1M conv=fsync&lt;/P&gt;&lt;P&gt;after booting up the image on custom board .&lt;BR /&gt;just after 1 minute . i am getting the below error :Internal error: Oops - Undefined instruction: 0000000002000000 [#1] PREEMPT SMP&lt;/P&gt;&lt;P&gt;[ 70.939602] Internal error: Oops - Undefined instruction: 0000000002000000 [#1] PREEMPT SMP&lt;BR /&gt;[ 70.947971] Modules linked in: can_raw can overlay snd_usb_audio fsl_jr_uio snd_hwdep snd_usbmidi_lib caam_jr uvcvideo caamkeyblob_desc caamhash_desc caamalg_desc crypto_engine authenc libdes snd_soc_fsl_asoc_card crct10dif_ce snd_soc_imx_audmux polyval_ce snd_soc_imx_card polyval_generic snd_soc_imx_hdmi imx8_media_dev(C) snd_soc_fsl_xcvr snd_soc_fsl_sai snd_soc_fsl_easrc dw_hdmi_cec flexcan snd_soc_fsl_micfil snd_soc_fsl_asrc imx_pcm_dma snd_soc_fsl_aud2htx snd_soc_fsl_utils snd_soc_wm8960 can_dev caam secvio error imx_dsp_rproc fuse&lt;BR /&gt;[ 70.995482] CPU: 0 PID: 0 Comm: swapper/0 Tainted: G C 6.6.3-lts-next-gccf0a99701a7-dirty #1&lt;BR /&gt;[ 71.005311] Hardware name: NXP i.MX8MPlus EVK board (DT)&lt;BR /&gt;[ 71.010622] pstate: 200000c5 (nzCv daIF -PAN -UAO -TCO -DIT -SSBS BTYPE=--)&lt;BR /&gt;[ 71.017586] pc : ret_to_kernel+0x0/0x64&lt;BR /&gt;[ 71.021427] lr : el1h_64_irq+0x64/0x68&lt;BR /&gt;[ 71.025180] sp : ffff800081fb3bc0&lt;BR /&gt;[ 71.028492] x29: ffff800081fb3cf0 x28: ffff800081fc3ac0 x27: 0000000000000000&lt;BR /&gt;[ 71.035636] x26: 00000000feeddcc8 x25: 00000010843cb40c x24: 0000000000000000&lt;BR /&gt;[ 71.042777] x23: 0000000060000005 x22: ffff800081430558 x21: ffff800081fb3d10&lt;BR /&gt;[ 71.049920] x20: 0000000000000000 x19: 0000001084542777 x18: 0000000000000000&lt;BR /&gt;[ 71.057062] x17: ffff8000fd657000 x16: ffff800080000000 x15: 014495177a9b692a&lt;BR /&gt;[ 71.064204] x14: 002683e67a6440b4 x13: 0000000000000233 x12: 0000000000000000&lt;BR /&gt;[ 71.071345] x11: 0000000000000005 x10: 0000000000000000 x9 : 0000000000000001&lt;BR /&gt;[ 71.078489] x8 : ffff00017f353f80 x7 : ffff00017f353f80 x6 : 0000000003abc514&lt;BR /&gt;[ 71.085629] x5 : 4000000000000002 x4 : ffff8000fd657000 x3 : ffff8000fd657000&lt;BR /&gt;[ 71.092772] x2 : ffff00017f350bd0 x1 : 4000000000000000 x0 : 000000000005744c&lt;BR /&gt;[ 71.099915] Call trace:&lt;BR /&gt;[ 71.102361] ret_to_kernel+0x0/0x64&lt;BR /&gt;[ 71.105854] cpuidle_enter_state+0x134/0x2e0&lt;BR /&gt;[ 71.110125] cpuidle_enter+0x38/0x50&lt;BR /&gt;[ 71.113704] do_idle+0x1f4/0x264&lt;BR /&gt;[ 71.116939] cpu_startup_entry+0x34/0x3c&lt;BR /&gt;[ 71.120868] kernel_init+0x0/0x1dc&lt;BR /&gt;[ 71.124272] arch_post_acpi_subsys_init+0x0/0x8&lt;BR /&gt;[ 71.128806] start_kernel+0x504/0x5ec&lt;BR /&gt;[ 71.132476] __primary_switched+0xbc/0xc4&lt;BR /&gt;[ 71.136491] Code: e7d29770 00ff95c3 fcbf9830 00ff4717 (4d8c9f97)&lt;BR /&gt;[ 71.142586] ---[ end trace 0000000000000000 ]---&lt;BR /&gt;[ 71.147204] Kernel panic - not syncing: Attempted to kill the idle task!&lt;BR /&gt;[ 71.153905] SMP: stopping secondary CPUs&lt;BR /&gt;[ 72.157829] SMP: failed to stop secondary CPUs 0,2-3&lt;BR /&gt;[ 72.162796] Kernel Offset: disabled&lt;BR /&gt;[ 72.166284] CPU features: 0x0,00000008,00020000,1000421b&lt;BR /&gt;[ 72.171596] Memory Limit: none&lt;BR /&gt;[ 72.174651] ---[ end Kernel panic - not syncing: Attempted to kill the idle task! ]---&lt;/P&gt;&lt;P&gt;If anyone knows how to resolve this error or can tell me what might be causing it, please help me.&lt;/P&gt;</description>
      <pubDate>Wed, 20 Nov 2024 10:54:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Internal-error-Oops-Undefined-instruction-0000000002000000-1/m-p/1997976#M231026</guid>
      <dc:creator>srinivas_123</dc:creator>
      <dc:date>2024-11-20T10:54:10Z</dc:date>
    </item>
    <item>
      <title>Re: Internal error: Oops - Undefined instruction: 0000000002000000 [#1] PREEMPT SMP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Internal-error-Oops-Undefined-instruction-0000000002000000-1/m-p/1998073#M231035</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;DIV id="bodyDisplay_1" class="lia-message-body lia-component-message-view-widget-body lia-component-body-signature-highlight-escalation lia-component-message-view-widget-body-signature-highlight-escalation"&gt;
&lt;DIV class="lia-message-body-content"&gt;
&lt;P&gt;Yes, it looks like RAM is not properly configured.&lt;/P&gt;
&lt;P&gt;Also, I would expect that the kernel crash log would vary each time, right?&lt;/P&gt;
&lt;P&gt;one can start with DDR tests and finding new calibration settings.&lt;/P&gt;
&lt;P&gt;regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;/DIV&gt;
&lt;/DIV&gt;</description>
      <pubDate>Wed, 20 Nov 2024 14:48:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Internal-error-Oops-Undefined-instruction-0000000002000000-1/m-p/1998073#M231035</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-11-20T14:48:04Z</dc:date>
    </item>
    <item>
      <title>Re: Internal error: Oops - Undefined instruction: 0000000002000000 [#1] PREEMPT SMP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Internal-error-Oops-Undefined-instruction-0000000002000000-1/m-p/2026738#M232936</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/231093"&gt;@srinivas_123&lt;/a&gt;Hello, have you solved this problem? I'm facing samilar problem with mainline kernel for imx93, this happens on every boot&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;[ 0.135496] nxp-pca9450 1-0025: No IRQ configured?&lt;BR /&gt;[ 0.434467] SError Interrupt on CPU0, code 0x00000000be000011 -- SError&lt;BR /&gt;[ 0.434479] CPU: 0 PID: 0 Comm: swapper/0 Not tainted 6.1.124 #4&lt;BR /&gt;[ 0.434484] Hardware name: ATK-DLIMX93 Development board (DT)&lt;BR /&gt;[ 0.434487] pstate: 404000c9 (nZcv daIF +PAN -UAO -TCO -DIT -SSBS BTYPE=--)&lt;BR /&gt;[ 0.434492] pc : tick_handle_oneshot_broadcast+0x0/0x250&lt;BR /&gt;[ 0.434504] lr : sysctr_timer_interrupt+0x34/0x40&lt;BR /&gt;[ 0.434511] sp : ffff800008003f20&lt;BR /&gt;[ 0.434513] x29: ffff800008003f20 x28: ffff800009fc3f80 x27: ffff8000096c8a38&lt;BR /&gt;[ 0.434522] x26: 0000000000000000 x25: 0000000019e52f48 x24: 0000000018644585&lt;BR /&gt;[ 0.434528] x23: ffff00000001b200 x22: 000000000000000e x21: 0000000000000000&lt;BR /&gt;[ 0.434534] x20: ffff00000001b2dc x19: ffff000000004b00 x18: fffffffffffe3ce0&lt;BR /&gt;[ 0.434539] x17: ffff8000363c2000 x16: ffff800008000000 x15: 0000000000000038&lt;BR /&gt;[ 0.434545] x14: 0000000000000197 x13: 0000000000000000 x12: 0000000000000000&lt;BR /&gt;[ 0.434551] x11: 0000000000000040 x10: ffff000000008170 x9 : ffff000000008168&lt;BR /&gt;[ 0.434556] x8 : ffff000002800948 x7 : 0000000000000000 x6 : 0000000000000000&lt;BR /&gt;[ 0.434562] x5 : ffff000002800920 x4 : ffff8000363c2000 x3 : ffff8000097d6500&lt;BR /&gt;[ 0.434567] x2 : 0000000000000000 x1 : ffff800008127e94 x0 : ffff80000a2ea840&lt;BR /&gt;[ 0.434575] Kernel panic - not syncing: Asynchronous SError Interrupt&lt;BR /&gt;[ 0.434578] CPU: 0 PID: 0 Comm: swapper/0 Not tainted 6.1.124 #4&lt;BR /&gt;[ 0.434582] Hardware name: ATK-DLIMX93 Development board (DT)&lt;/P&gt;&lt;P&gt;[ 0.434584] Call trace:&lt;BR /&gt;[ 0.434586] dump_backtrace.part.0+0xd8/0xe4&lt;BR /&gt;[ 0.434594] show_stack+0x14/0x20&lt;BR /&gt;[ 0.434599] dump_stack_lvl+0x60/0x78&lt;BR /&gt;[ 0.434605] dump_stack+0x14/0x2c&lt;BR /&gt;[ 0.434609] panic+0x17c/0x33c&lt;BR /&gt;[ 0.434615] add_taint+0x0/0xbc&lt;BR /&gt;[ 0.434620] arm64_serror_panic+0x68/0x74&lt;BR /&gt;[ 0.434624] do_serror+0x0/0x50&lt;BR /&gt;[ 0.434627] do_serror+0x30/0x50&lt;BR /&gt;[ 0.434630] el1h_64_error_handler+0x2c/0x40&lt;BR /&gt;[ 0.434635] el1h_64_error+0x64/0x68&lt;BR /&gt;[ 0.434638] tick_handle_oneshot_broadcast+0x0/0x250&lt;BR /&gt;[ 0.434643] __handle_irq_event_percpu+0x44/0x150&lt;BR /&gt;[ 0.434649] handle_irq_event+0x48/0xac&lt;BR /&gt;[ 0.434654] handle_fasteoi_irq+0xa0/0x190&lt;BR /&gt;[ 0.434660] generic_handle_domain_irq+0x28/0x40&lt;BR /&gt;[ 0.434664] gic_handle_irq+0x4c/0x124&lt;BR /&gt;[ 0.434672] call_on_irq_stack+0x24/0x40&lt;BR /&gt;[ 0.434676] do_interrupt_handler+0x78/0x80&lt;BR /&gt;[ 0.434680] el1_interrupt+0x30/0x60&lt;BR /&gt;[ 0.434684] el1h_64_irq_handler+0x14/0x20&lt;BR /&gt;[ 0.434689] el1h_64_irq+0x64/0x68&lt;BR /&gt;[ 0.434692] cpuidle_enter_state+0x12c/0x2f0&lt;BR /&gt;[ 0.434699] cpuidle_enter+0x34/0x50&lt;BR /&gt;[ 0.434703] do_idle+0x220/0x2b0&lt;BR /&gt;[ 0.434708] cpu_startup_entry+0x34/0x40&lt;BR /&gt;[ 0.434713] kernel_init+0x0/0x130&lt;BR /&gt;[ 0.434718] arch_post_acpi_subsys_init+0x0/0x8&lt;BR /&gt;[ 0.434725] start_kernel+0x64c/0x688&lt;BR /&gt;[ 0.434730] __primary_switched+0xbc/0xc4&lt;BR /&gt;[ 0.434737] SMP: stopping secondary CPUs&lt;BR /&gt;[ 0.434742] Kernel Offset: disabled&lt;BR /&gt;[ 0.434743] CPU features: 0x060000,000400a4,6600721b&lt;BR /&gt;[ 0.434747] Memory Limit: none&lt;/P&gt;&lt;/BLOCKQUOTE&gt;</description>
      <pubDate>Mon, 13 Jan 2025 12:26:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Internal-error-Oops-Undefined-instruction-0000000002000000-1/m-p/2026738#M232936</guid>
      <dc:creator>PerrZhang</dc:creator>
      <dc:date>2025-01-13T12:26:07Z</dc:date>
    </item>
  </channel>
</rss>