<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRT1062 SAI EDMA Using Same Callback For both TX &amp;amp; RX?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RT1062-SAI-EDMA-Using-Same-Callback-For-both-TX-amp-RX/m-p/2022877#M232689</link>
    <description>&lt;P&gt;It is possible for us to use only one callback for EDMA TX and RX? Currently the callbacks for SAI EDMA callback is separated into two callbacks.&lt;/P&gt;</description>
    <pubDate>Tue, 07 Jan 2025 02:24:01 GMT</pubDate>
    <dc:creator>vincentmokrc</dc:creator>
    <dc:date>2025-01-07T02:24:01Z</dc:date>
    <item>
      <title>RT1062 SAI EDMA Using Same Callback For both TX &amp; RX?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1062-SAI-EDMA-Using-Same-Callback-For-both-TX-amp-RX/m-p/2022877#M232689</link>
      <description>&lt;P&gt;It is possible for us to use only one callback for EDMA TX and RX? Currently the callbacks for SAI EDMA callback is separated into two callbacks.&lt;/P&gt;</description>
      <pubDate>Tue, 07 Jan 2025 02:24:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1062-SAI-EDMA-Using-Same-Callback-For-both-TX-amp-RX/m-p/2022877#M232689</guid>
      <dc:creator>vincentmokrc</dc:creator>
      <dc:date>2025-01-07T02:24:01Z</dc:date>
    </item>
    <item>
      <title>Re: RT1062 SAI EDMA Using Same Callback For both TX &amp; RX?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1062-SAI-EDMA-Using-Same-Callback-For-both-TX-amp-RX/m-p/2024462#M232808</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/245226"&gt;@vincentmokrc&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for your interest in NXP MIMXRT series!&lt;/P&gt;
&lt;P&gt;Yes, you can do this. Tx and Rx can be decoupled by using the passed *userData. e.g. when creating SAI EDMA handles, pass in different &lt;CODE&gt;userData&lt;/CODE&gt; for TX and RX respectively, such as the addresses of &lt;CODE&gt;txHandle&lt;/CODE&gt; and &lt;CODE&gt;rxHandle&lt;/CODE&gt;.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Gavin&lt;/P&gt;</description>
      <pubDate>Thu, 09 Jan 2025 03:48:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1062-SAI-EDMA-Using-Same-Callback-For-both-TX-amp-RX/m-p/2024462#M232808</guid>
      <dc:creator>Gavin_Jia</dc:creator>
      <dc:date>2025-01-09T03:48:39Z</dc:date>
    </item>
  </channel>
</rss>