<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピック回复： imx93-11x11-lpddr4x-evk  can not update kernel</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx93-11x11-lpddr4x-evk-can-not-update-kernel/m-p/2022872#M232687</link>
    <description>Applied this patch but proc version still shows the same time:&lt;BR /&gt;&lt;BR /&gt;diff --git a/meta/lib/oe/reproducible.py b/meta/lib/oe/reproducible.py&lt;BR /&gt;index 448befce33..4d76405deb 100644&lt;BR /&gt;--- a/meta/lib/oe/reproducible.py&lt;BR /&gt;+++ b/meta/lib/oe/reproducible.py&lt;BR /&gt;@@ -6,6 +6,7 @@&lt;BR /&gt;import os&lt;BR /&gt;import subprocess&lt;BR /&gt;import bb&lt;BR /&gt;+import time&lt;BR /&gt;&lt;BR /&gt;# For reproducible builds, this code sets the default SOURCE_DATE_EPOCH in each&lt;BR /&gt;# component's build environment. The format is number of seconds since the&lt;BR /&gt;@@ -156,6 +157,8 @@ def fixed_source_date_epoch(d):&lt;BR /&gt;return 0&lt;BR /&gt;&lt;BR /&gt;def get_source_date_epoch(d, sourcedir):&lt;BR /&gt;+ if 1 == 1:&lt;BR /&gt;+ return int(time.time())&lt;BR /&gt;return (&lt;BR /&gt;get_source_date_epoch_from_git(d, sourcedir) or&lt;BR /&gt;get_source_date_epoch_from_youngest_file(d, sourcedir) or&lt;BR /&gt;&lt;BR /&gt;root@imx93-11x11-lpddr4x-evk:~# cat /proc/version&lt;BR /&gt;Linux version 6.6.36-lts-next-g877ae856160d-dirty (oe-user@oe-host) (aarch64-poky-linux-gcc (GCC) 13.3.0, GNU ld (GNU Binutils) 2.42.0.20240716) #1 SMP PREEMPT Wed Sep 4 08:22:45 UTC 2024&lt;BR /&gt;&lt;BR /&gt;Changes still goes into the Image as the new kernel log contain new build msg&lt;BR /&gt;&lt;BR /&gt;BTW adding this patch will introduce logs like&lt;BR /&gt;&lt;BR /&gt;ERROR: When reparsing /home/colin/Desktop/Work_Files/I3C/nxp_bsp/imx-yocto-bsp/sources/meta-imx/meta-imx-bsp/recipes-kernel/linux/linux-imx_6.6.bb:do_create_sp&lt;BR /&gt;dx, the basehash value changed from 1cf6a19055bc4176f091ff31f0f7d0d39f972ed4820a2253065969871965d77d to 31f5333b4a6c41d760b3c9ccfdb72ce0eebb2e7f9c5d6e7655f4d18&lt;BR /&gt;3dc56612e. The metadata is not deterministic and this needs to be fixed.&lt;BR /&gt;ERROR: The following commands may help:&lt;BR /&gt;ERROR: $ bitbake linux-imx -cdo_create_spdx -Snone&lt;BR /&gt;ERROR: Then:&lt;BR /&gt;ERROR: $ bitbake linux-imx -cdo_create_spdx -Sprintdiff&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;there are 160 error with this, but built image still generate and can work, when i revert the change for adding time in py, the errors are gone, not sure if this is related</description>
    <pubDate>Tue, 07 Jan 2025 02:17:28 GMT</pubDate>
    <dc:creator>lykaios1203</dc:creator>
    <dc:date>2025-01-07T02:17:28Z</dc:date>
    <item>
      <title>imx93-11x11-lpddr4x-evk  can not update kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93-11x11-lpddr4x-evk-can-not-update-kernel/m-p/2021192#M232535</link>
      <description>&lt;P&gt;&lt;SPAN class=""&gt;This is the full operation, please help to check which step is wrong so linux kernel changes does not goes into the Image:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;$ mkdir imx-yocto-bsp&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;$ cd imx-yocto-bsp&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;$ repo init -u&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;A title="" href="https://github.com/nxp-imx/imx-manifest" target="_blank" rel="noopener noreferrer"&gt;https://github.com/nxp-imx/imx-manifest&lt;/A&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;-b imx-linux-scarthgap -m imx-6.6.36-2.1.0.xml&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;$ repo sync&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;$ export BSPDIR=$(pwd)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;$ DISTRO=fsl-imx-wayland MACHINE=imx93-11x11-lpddr4x-evk source&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;A title="" href="https://imx-setup-release.sh/" target="_blank" rel="noopener noreferrer"&gt;imx-setup-release.sh&lt;/A&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;-b buildwayland&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;$ bitbake linux-imx&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;========================================================================================&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;the log shows&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;========================================================================================&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;NOTE: Your conf/bblayers.conf has been automatically updated.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Loading cache: 100% |###########################################################################################################################| Time: 0:00:01&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Loaded 5717 entries from dependency cache.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Parsing recipes: 100% |#########################################################################################################################| Time: 0:00:01&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Parsing of 3642 .bb files complete (3641 cached, 1 parsed). 5718 targets, 619 skipped, 17 masked, 0 errors.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;NOTE: Resolving any missing task queue dependencies&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Build Configuration:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;BB_VERSION&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;= "2.8.0"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;BUILD_SYS&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;= "x86_64-linux"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;NATIVELSBSTRING&amp;nbsp;&amp;nbsp;&amp;nbsp;= "universal"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;TARGET_SYS&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;= "aarch64-poky-linux"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;MACHINE&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;= "imx93-11x11-lpddr4x-evk"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;DISTRO&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;= "fsl-imx-wayland"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;DISTRO_VERSION&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;= "6.6-scarthgap"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;TUNE_FEATURES&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;= "aarch64 armv8a crc crypto"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;TARGET_FPU&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;= ""&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;meta&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;meta-poky&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;= "HEAD:f43f393ef0246b7bee6eed8bcf8271cf2b8cdf40"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;meta-oe&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;meta-multimedia&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;meta-python&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;= "HEAD:80e01188fa822d87d301ee71973c462d7a865493"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;meta-freescale&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;= "HEAD:0f8091c63dd8805610c09b08409bc58492a3b16f"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;meta-freescale-3rdparty = "HEAD:6c063450d464eb2f380443c7d9af1b94ce9b9d75"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;meta-freescale-distro = "HEAD:b9d6a5d9931922558046d230c1f5f4ef6ee72345"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;meta-imx-bsp&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;meta-imx-sdk&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;meta-imx-ml&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;meta-imx-v2x&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;= "HEAD:f23d0ce80d40c4128116fa0b4dde5f5af9b0357d"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;meta-nxp-demo-experience = "HEAD:8fd7154c05b716e9635279047f65785399432d88"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;meta-nxp-matter-baseline&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;meta-nxp-openthread&amp;nbsp;= "HEAD:783becb4b5716d989f50db95b7133d38eae5b47b"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;meta-arm&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;meta-arm-toolchain&amp;nbsp;&amp;nbsp;= "HEAD:1b85bbb4cab9658da3cd926c62038b8559c5c64e"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;meta-clang&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;= "HEAD:fe561f41aef0cff9e6f96730ab59f28dca2eb682"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;meta-gnome&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;meta-networking&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;meta-filesystems&amp;nbsp;&amp;nbsp;&amp;nbsp;= "HEAD:80e01188fa822d87d301ee71973c462d7a865493"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;meta-qt6&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;= "HEAD:dc13e1bfda4a4757a08c2d6673bc4bac012c4a80"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;meta-parsec&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;meta-tpm&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;= "HEAD:11ea91192d43d7c2b0b95a93aa63ca7e73e38034"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;meta-virtualization&amp;nbsp;= "HEAD:6a80f140e387621f62964209a2e07d3bcfb125ce"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;WARNING: /home/colin/Desktop/Work_Files/I3C/nxp_bsp/imx-yocto-bsp/sources/meta-imx/meta-imx-bsp/recipes-kernel/linux/linux-imx_6.&lt;/SPAN&gt;&lt;A title="" href="https://6.bb/" target="_blank" rel="noopener noreferrer"&gt;6.bb&lt;/A&gt;&lt;SPAN class=""&gt;:do_compile is tainted from a forced run&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;WARNING: /home/colin/Desktop/Work_Files/I3C/nxp_bsp/imx-yocto-bsp/sources/meta-imx/meta-imx-bsp/recipes-kernel/linux/linux-imx_6.&lt;/SPAN&gt;&lt;A title="" href="https://6.bb/" target="_blank" rel="noopener noreferrer"&gt;6.bb&lt;/A&gt;&lt;SPAN class=""&gt;:do_deploy is tainted from a forced run&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Sstate summary: Wanted 0 Local 0 Mirrors 0 Missed 0 Current 345 (0% match, 100% complete)##########################################&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;| ETA:&amp;nbsp;0:00:00&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Initialising tasks: 100% |######################################################################################################################| Time: 0:00:00&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;NOTE: Executing Tasks&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;NOTE: Tasks Summary: Attempted 1075 tasks of which 1075 didn't need to be rerun and all succeeded.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Summary: There were 2 WARNING messages.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;========================================================================================&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;the output Image is&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Image--6.6.36+git0+d23d64eea5-r0-imx93-11x11-lpddr4x-evk-20250102073143.bin&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;========================================================================================&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;the kernel git history:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;commit 877ae856160db41ab7a76d9e2767f87543ea69ce (HEAD -&amp;gt; lf-6.6.y)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Author: colin_wang &amp;lt;&lt;/SPAN&gt;&lt;A href="mailto:lykaios1203@gmail.com" target="_blank" rel="noopener"&gt;lykaios1203@gmail.com&lt;/A&gt;&lt;SPAN class=""&gt;&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Date:&amp;nbsp;&amp;nbsp;Thu Dec 26 19:04:15 2024 +0800&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp;add patch but with modify&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;commit d23d64eea5111e1607efcce1d601834fceec92cb (tag: lf-6.6.36-2.1.0, origin/lf-6.6.y)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Author: Wei Fang &amp;lt;&lt;/SPAN&gt;&lt;A href="mailto:wei.fang@nxp.com" target="_blank" rel="noopener"&gt;wei.fang@nxp.com&lt;/A&gt;&lt;SPAN class=""&gt;&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Date:&amp;nbsp;&amp;nbsp;Wed Sep 4 13:06:28 2024 +0800&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp;LF-13425 arm64: dts: imx8mq: adjust TX drive strength of FEC&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp;The default drive strength of TXD, TXC and TX_CTL were all set&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp;to 0x7, which is the maximum drive strength. However, it will&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp;cause low dB margin issue at 250MHz frequency band. Based on&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp;the suggestion from SE team, change the drive strength from&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp;0x7 to 0x6.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp;Signed-off-by: Wei Fang &amp;lt;&lt;/SPAN&gt;&lt;A href="mailto:wei.fang@nxp.com" target="_blank" rel="noopener"&gt;wei.fang@nxp.com&lt;/A&gt;&lt;SPAN class=""&gt;&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp;Reviewed-by: Clark Wang &amp;lt;&lt;/SPAN&gt;&lt;A href="mailto:xiaoning.wang@nxp.com" target="_blank" rel="noopener"&gt;xiaoning.wang@nxp.com&lt;/A&gt;&lt;SPAN class=""&gt;&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&amp;nbsp;Acked-by: Jason Liu &amp;lt;&lt;/SPAN&gt;&lt;A href="mailto:jason.hui.liu@nxp.com" target="_blank" rel="noopener"&gt;jason.hui.liu@nxp.com&lt;/A&gt;&lt;SPAN class=""&gt;&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;========================================================================================&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;After I copy the Image and rename it to 'Image' to place in the /run/media/boot-mmcblk0p1/&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;root@imx93-11x11-lpddr4x-evk:~# ls /run/media/boot-mmcblk0p1/&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Image&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;imx93-11x11-evk-iw612-otbr.dtb&amp;nbsp;imx93-11x11-evk.dtb&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Image_ori&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;imx93-11x11-evk-ld.dtb&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;imx93-11x11-evk_m33_TCM_low_power_wakeword.bin&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;imx93-11x11-evk-aud-hat.dtb&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;imx93-11x11-evk-lpuart.dtb&amp;nbsp;&amp;nbsp;&amp;nbsp;imx93-11x11-evk_m33_TCM_power_mode_switch.bin&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;imx93-11x11-evk-boe-wxga-lvds-panel.dtb&amp;nbsp;imx93-11x11-evk-mqs.dtb&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;imx93-11x11-evk_m33_TCM_rpmsg_lite_pingpong_rtos_linux_remote.bin&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;imx93-11x11-evk-flexio-i2c.dtb&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;imx93-11x11-evk-mt9m114.dtb&amp;nbsp;&amp;nbsp;&amp;nbsp;imx93-11x11-evk_m33_TCM_rpmsg_lite_str_echo_rtos.bin&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;imx93-11x11-evk-flexspi-m2.dtb&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;imx93-11x11-evk-rm67199.dtb&amp;nbsp;&amp;nbsp;&amp;nbsp;imx93-11x11-evk_m33_TCM_sai_low_power_audio.bin&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;imx93-11x11-evk-i2c-spi-slave.dtb&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;imx93-11x11-evk-root.dtb&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;tee.bin&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;imx93-11x11-evk-i3c.dtb&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;imx93-11x11-evk-rpmsg-lpv.dtb&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;imx93-11x11-evk-inmate.dtb&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;imx93-11x11-evk-rpmsg.dtb&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;========================================================================================&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;then reboot, still i see&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;imx93-11x11-lpddr4x-evk login: root&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;root@imx93-11x11-lpddr4x-evk:~# cat /proc/version&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Linux version 6.6.36-lts-next-g877ae856160d (oe-user@oe-host) (aarch64-poky-linux-gcc (GCC) 13.3.0, GNU ld (GNU Binutils) 2.42.0.20240716) #1 SMP PREEMPT Wed Sep&amp;nbsp;4 08:22:45 UTC 2024&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;the build date is still Sep&amp;nbsp;4, which is the 6.6 upstream config, but i already make changes to the kernel source&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 02 Jan 2025 09:13:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93-11x11-lpddr4x-evk-can-not-update-kernel/m-p/2021192#M232535</guid>
      <dc:creator>lykaios1203</dc:creator>
      <dc:date>2025-01-02T09:13:16Z</dc:date>
    </item>
    <item>
      <title>回复： imx93-11x11-lpddr4x-evk  can not update kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93-11x11-lpddr4x-evk-can-not-update-kernel/m-p/2021707#M232574</link>
      <description>&lt;P&gt;Refers to&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/Time-in-version-is-inconsistent-with-compilation-time/m-p/2021568#M232560" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/Time-in-version-is-inconsistent-with-compilation-time/m-p/2021568#M232560&lt;/A&gt;&lt;BR /&gt;&amp;nbsp;the kernel built time is unchanged if you do not make you own git commit, you can pass the KERNEL_DEBUG_TIMESTAMPS=1 env, thus make a full clean build of your kernel, and the kernel built time will be changed.&lt;/P&gt;</description>
      <pubDate>Fri, 03 Jan 2025 07:50:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93-11x11-lpddr4x-evk-can-not-update-kernel/m-p/2021707#M232574</guid>
      <dc:creator>Nobita</dc:creator>
      <dc:date>2025-01-03T07:50:59Z</dc:date>
    </item>
    <item>
      <title>回复： imx93-11x11-lpddr4x-evk  can not update kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93-11x11-lpddr4x-evk-can-not-update-kernel/m-p/2021714#M232576</link>
      <description>&lt;P&gt;For your situation, I also suggest you to check your boot device, the&amp;nbsp;&lt;SPAN&gt;/run/media/boot-mmcblk0p1 should be the emmc on board.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 03 Jan 2025 07:57:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93-11x11-lpddr4x-evk-can-not-update-kernel/m-p/2021714#M232576</guid>
      <dc:creator>Nobita</dc:creator>
      <dc:date>2025-01-03T07:57:33Z</dc:date>
    </item>
    <item>
      <title>Re: imx93-11x11-lpddr4x-evk  can not update kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93-11x11-lpddr4x-evk-can-not-update-kernel/m-p/2022079#M232618</link>
      <description>&lt;P&gt;Try to add below two steps&amp;nbsp;after adding patch.&lt;/P&gt;
&lt;P&gt;bitbake linux-imx -f -c compile&lt;BR /&gt;bitbake linux-imx&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Sat, 04 Jan 2025 12:11:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93-11x11-lpddr4x-evk-can-not-update-kernel/m-p/2022079#M232618</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2025-01-04T12:11:10Z</dc:date>
    </item>
    <item>
      <title>Re: imx93-11x11-lpddr4x-evk  can not update kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93-11x11-lpddr4x-evk-can-not-update-kernel/m-p/2022305#M232638</link>
      <description>I tried this but the build time does not change, the new commit is 877ae856160db41ab7a76d9e2767f87543ea69ce as from above post</description>
      <pubDate>Mon, 06 Jan 2025 06:05:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93-11x11-lpddr4x-evk-can-not-update-kernel/m-p/2022305#M232638</guid>
      <dc:creator>lykaios1203</dc:creator>
      <dc:date>2025-01-06T06:05:51Z</dc:date>
    </item>
    <item>
      <title>回复： imx93-11x11-lpddr4x-evk  can not update kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93-11x11-lpddr4x-evk-can-not-update-kernel/m-p/2022307#M232640</link>
      <description>the new commit is 877ae856160db41ab7a76d9e2767f87543ea69ce as from above post added to the source but time does not change</description>
      <pubDate>Mon, 06 Jan 2025 06:06:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93-11x11-lpddr4x-evk-can-not-update-kernel/m-p/2022307#M232640</guid>
      <dc:creator>lykaios1203</dc:creator>
      <dc:date>2025-01-06T06:06:24Z</dc:date>
    </item>
    <item>
      <title>回复： imx93-11x11-lpddr4x-evk  can not update kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93-11x11-lpddr4x-evk-can-not-update-kernel/m-p/2022308#M232641</link>
      <description>besides the usb device there is one boot device so i think is should be the one&lt;BR /&gt;&lt;BR /&gt;root@imx93-11x11-lpddr4x-evk:~# ls /run/media/&lt;BR /&gt;Colin_USB-sda1 boot-mmcblk0p1</description>
      <pubDate>Mon, 06 Jan 2025 06:07:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93-11x11-lpddr4x-evk-can-not-update-kernel/m-p/2022308#M232641</guid>
      <dc:creator>lykaios1203</dc:creator>
      <dc:date>2025-01-06T06:07:16Z</dc:date>
    </item>
    <item>
      <title>Re: imx93-11x11-lpddr4x-evk  can not update kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93-11x11-lpddr4x-evk-can-not-update-kernel/m-p/2022335#M232646</link>
      <description>&lt;P&gt;Found that the changes are actually in the Image, but the build time remains unchange even if adding new patch to the kernel source , adding&amp;nbsp;&lt;SPAN&gt;KERNEL_DEBUG_TIMESTAMPS=1 via command like&lt;BR /&gt;KERNEL_DEBUG_TIMESTAMPS=1 bitbake linux-imx&lt;BR /&gt;still not update the time, current will add custom debug kernel message to check if image is updated, if there is other way to trigger the time update please reply, or I can mark this as temp solution. thanks&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 06 Jan 2025 06:43:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93-11x11-lpddr4x-evk-can-not-update-kernel/m-p/2022335#M232646</guid>
      <dc:creator>lykaios1203</dc:creator>
      <dc:date>2025-01-06T06:43:52Z</dc:date>
    </item>
    <item>
      <title>回复： imx93-11x11-lpddr4x-evk  can not update kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93-11x11-lpddr4x-evk-can-not-update-kernel/m-p/2022500#M232661</link>
      <description>&lt;P&gt;the following patch should work:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;diff --git a/meta/lib/oe/reproducible.py b/meta/lib/oe/reproducible.py
index 9ac75c02e3..ddce9e3a9d 100644
--- a/meta/lib/oe/reproducible.py
+++ b/meta/lib/oe/reproducible.py
@@ -6,6 +6,7 @@
 import os
 import subprocess
 import bb
+import time

 # For reproducible builds, this code sets the default SOURCE_DATE_EPOCH in each
 # component's build environment. The format is number of seconds since the
@@ -153,6 +154,8 @@ def fixed_source_date_epoch(d):
     return 0

 def get_source_date_epoch(d, sourcedir):
+    if 1 == 1:
+        return int(time.time())
     return (
         get_source_date_epoch_from_git(d, sourcedir) or
         get_source_date_epoch_from_youngest_file(d, sourcedir) or&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 06 Jan 2025 09:33:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93-11x11-lpddr4x-evk-can-not-update-kernel/m-p/2022500#M232661</guid>
      <dc:creator>Nobita</dc:creator>
      <dc:date>2025-01-06T09:33:36Z</dc:date>
    </item>
    <item>
      <title>回复： imx93-11x11-lpddr4x-evk  can not update kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93-11x11-lpddr4x-evk-can-not-update-kernel/m-p/2022872#M232687</link>
      <description>Applied this patch but proc version still shows the same time:&lt;BR /&gt;&lt;BR /&gt;diff --git a/meta/lib/oe/reproducible.py b/meta/lib/oe/reproducible.py&lt;BR /&gt;index 448befce33..4d76405deb 100644&lt;BR /&gt;--- a/meta/lib/oe/reproducible.py&lt;BR /&gt;+++ b/meta/lib/oe/reproducible.py&lt;BR /&gt;@@ -6,6 +6,7 @@&lt;BR /&gt;import os&lt;BR /&gt;import subprocess&lt;BR /&gt;import bb&lt;BR /&gt;+import time&lt;BR /&gt;&lt;BR /&gt;# For reproducible builds, this code sets the default SOURCE_DATE_EPOCH in each&lt;BR /&gt;# component's build environment. The format is number of seconds since the&lt;BR /&gt;@@ -156,6 +157,8 @@ def fixed_source_date_epoch(d):&lt;BR /&gt;return 0&lt;BR /&gt;&lt;BR /&gt;def get_source_date_epoch(d, sourcedir):&lt;BR /&gt;+ if 1 == 1:&lt;BR /&gt;+ return int(time.time())&lt;BR /&gt;return (&lt;BR /&gt;get_source_date_epoch_from_git(d, sourcedir) or&lt;BR /&gt;get_source_date_epoch_from_youngest_file(d, sourcedir) or&lt;BR /&gt;&lt;BR /&gt;root@imx93-11x11-lpddr4x-evk:~# cat /proc/version&lt;BR /&gt;Linux version 6.6.36-lts-next-g877ae856160d-dirty (oe-user@oe-host) (aarch64-poky-linux-gcc (GCC) 13.3.0, GNU ld (GNU Binutils) 2.42.0.20240716) #1 SMP PREEMPT Wed Sep 4 08:22:45 UTC 2024&lt;BR /&gt;&lt;BR /&gt;Changes still goes into the Image as the new kernel log contain new build msg&lt;BR /&gt;&lt;BR /&gt;BTW adding this patch will introduce logs like&lt;BR /&gt;&lt;BR /&gt;ERROR: When reparsing /home/colin/Desktop/Work_Files/I3C/nxp_bsp/imx-yocto-bsp/sources/meta-imx/meta-imx-bsp/recipes-kernel/linux/linux-imx_6.6.bb:do_create_sp&lt;BR /&gt;dx, the basehash value changed from 1cf6a19055bc4176f091ff31f0f7d0d39f972ed4820a2253065969871965d77d to 31f5333b4a6c41d760b3c9ccfdb72ce0eebb2e7f9c5d6e7655f4d18&lt;BR /&gt;3dc56612e. The metadata is not deterministic and this needs to be fixed.&lt;BR /&gt;ERROR: The following commands may help:&lt;BR /&gt;ERROR: $ bitbake linux-imx -cdo_create_spdx -Snone&lt;BR /&gt;ERROR: Then:&lt;BR /&gt;ERROR: $ bitbake linux-imx -cdo_create_spdx -Sprintdiff&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;there are 160 error with this, but built image still generate and can work, when i revert the change for adding time in py, the errors are gone, not sure if this is related</description>
      <pubDate>Tue, 07 Jan 2025 02:17:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93-11x11-lpddr4x-evk-can-not-update-kernel/m-p/2022872#M232687</guid>
      <dc:creator>lykaios1203</dc:creator>
      <dc:date>2025-01-07T02:17:28Z</dc:date>
    </item>
  </channel>
</rss>