<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: FTP setup</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/FTP-setup/m-p/252023#M23263</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, thanks for the reply,&lt;/P&gt;&lt;P&gt;I do have this working now, I had vsftpd installed on the target and it&lt;/P&gt;&lt;P&gt;needed to be configured.&lt;/P&gt;&lt;P&gt;I enabled anonymous logins for testing and was able to establish a&lt;/P&gt;&lt;P&gt;connection after that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks again&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Dec 2013 22:22:55 GMT</pubDate>
    <dc:creator>goodwell</dc:creator>
    <dc:date>2013-12-17T22:22:55Z</dc:date>
    <item>
      <title>FTP setup</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FTP-setup/m-p/252021#M23261</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I made an image for a sabrelite board using yocto; fsl-image-test. The image boots and runs fine, but I cannot transfer files through FileZilla ftp or sftp.  I can connect to the target through ssh but when I try to use FileZilla the connection is rejected. What do I need enabled or installed on the target to allow for file transfers?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Dec 2013 15:53:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FTP-setup/m-p/252021#M23261</guid>
      <dc:creator>goodwell</dc:creator>
      <dc:date>2013-12-09T15:53:37Z</dc:date>
    </item>
    <item>
      <title>Re: FTP setup</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FTP-setup/m-p/252022#M23262</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Scott,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So you are running ubuntu already and you are using filezilla from your pc to connect to the board?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Dec 2013 18:09:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FTP-setup/m-p/252022#M23262</guid>
      <dc:creator>SergioSolis</dc:creator>
      <dc:date>2013-12-17T18:09:58Z</dc:date>
    </item>
    <item>
      <title>Re: FTP setup</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FTP-setup/m-p/252023#M23263</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, thanks for the reply,&lt;/P&gt;&lt;P&gt;I do have this working now, I had vsftpd installed on the target and it&lt;/P&gt;&lt;P&gt;needed to be configured.&lt;/P&gt;&lt;P&gt;I enabled anonymous logins for testing and was able to establish a&lt;/P&gt;&lt;P&gt;connection after that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks again&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Dec 2013 22:22:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FTP-setup/m-p/252023#M23263</guid>
      <dc:creator>goodwell</dc:creator>
      <dc:date>2013-12-17T22:22:55Z</dc:date>
    </item>
  </channel>
</rss>