<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic 回复： After enbale MMU, can only access DDR, can't access any peripheral address space include SCU add in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/After-enbale-MMU-can-only-access-DDR-can-t-access-any-peripheral/m-p/2021001#M232520</link>
    <description>after enabled MMU enabled:&lt;BR /&gt;[-CPU3-]:mmu_table_init-(00198)]translation table init done&lt;BR /&gt;[-CPU3-]:mmu_init-(00265)]ttbr=0x4802c05b&lt;BR /&gt;[-CPU3-]:Test_VirtualMMU-(00222)]L1_TblAddr = 0x4802c000&lt;BR /&gt;[-CPU3-]:Test_VirtualMMU-(00230)]L1_DescriptorAddr = 0x4802f7a8,L1_Descriptor = 0x483aa9e1&lt;BR /&gt;[-CPU3-]:Test_VirtualMMU-(00232)]L1_Descriptor = 0x483aa9e1&lt;BR /&gt;[-CPU3-]:Test_VirtualMMU-(00237)]L2_TableBaseAddr = 0x483aa800,L2_DescriptorAddr = 0x483aab6c,L2_Descriptor = 0xdeadb576&lt;BR /&gt;[-CPU3-]:Test_VirtualMMU-(00240)]L2_Descriptor = 0xdeadb576&lt;BR /&gt;[-CPU3-]:Test_VirtualMMU-(00245)]va = 0xdeadbeef,pa = 0xdeadbeef&lt;BR /&gt;[-CPU3-]:main-(00104)]SCU_BASE=0x00a00000&lt;BR /&gt;[-CPU3-]:main-(00106)]Enable MMU&lt;BR /&gt;[-CPU3-]:disp_cp15_regs-(00104)]MIDR= 0x412fc09a&lt;BR /&gt;[-CPU3-]:disp_cp15_regs-(00106)]REVIDR=0x412fc09a&lt;BR /&gt;[-CPU3-]:disp_cp15_regs-(00108)]SCTRL= 0x10c5387d&lt;BR /&gt;[-CPU3-]:disp_cp15_regs-(00110)]DACR= 0x55555555&lt;BR /&gt;[-CPU3-]:disp_cp15_regs-(00112)]ACTLR= 0x00000047&lt;BR /&gt;[-CPU3-]:disp_cp15_regs-(00114)]CPACR= 0x00f00000&lt;BR /&gt;[-CPU3-]:disp_cp15_regs-(00116)]NSACR= 0x00000000&lt;BR /&gt;[-CPU3-]:main-(00113)]Enable SIMD VFP&lt;BR /&gt;[-CPU3-]:main-(00115)]Neon Test ...&lt;BR /&gt;I: 7298-Q: -8657|I: 28513-Q: 7192|I:-14294-Q: 4935|I: 3797-Q: 25403|I:-13302-Q: 18999|I: 17846-Q:-31606|I: 3377-Q: -1452|I: 690-Q: 10603|I: -2352-Q:-20951|I:-24549-Q: 521|I: 8485-Q: 2026|I:-10757-Q: 30099|I: 5764-Q: 1393|I: -1091-Q: 5758|I:&lt;BR /&gt;[-CPU3-]:TestNeon-(00059)]C Intrinsics done&lt;BR /&gt;I: 7298-Q: -8657|I: 28513-Q: 7192|I:-14294-Q: 4935|I: 3797-Q: 25403|I:-13302-Q: 18999|I: 17846-Q:-31606|I: 3377-Q: -1452|I: 690-Q: 10603|I: -2352-Q:-20951|I:-24549-Q: 521|I: 8485-Q: 2026|I:-10757-Q: 30099|I: 5764-Q: 1393|I: -1091-Q: 5758|I:&lt;BR /&gt;[-CPU3-]:TestNeon-(00095)]NEON Intrinsics done&lt;BR /&gt;[-CPU3-]:TestNeon-(00096)]int convert to short test&lt;BR /&gt;[-CPU3-]:TestNeon-(00097)]RAW Data:&lt;BR /&gt;25791 531569 -2334455 -11515&lt;BR /&gt;[-CPU3-]:TestNeon-(00103)]C:&lt;BR /&gt;25791 7281 24841 -11515&lt;BR /&gt;[-CPU3-]:TestNeon-(00110)]NEON:&lt;BR /&gt;25791 7281 24841 -11515&lt;BR /&gt;[-CPU3-]:TestNeon-(00118)]NEON saturated:&lt;BR /&gt;25791 32767 -32768 -11515&lt;BR /&gt;[-CPU3-]:main-(00117)]Normal Distribution Random number Test ...</description>
    <pubDate>Thu, 02 Jan 2025 03:55:59 GMT</pubDate>
    <dc:creator>luoqiaofa1</dc:creator>
    <dc:date>2025-01-02T03:55:59Z</dc:date>
    <item>
      <title>After enbale MMU, can only access DDR, can't access any peripheral address space include SCU address</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/After-enbale-MMU-can-only-access-DDR-can-t-access-any-peripheral/m-p/2021000#M232519</link>
      <description>&lt;P&gt;Hello Supports:&lt;BR /&gt;I'm trying to run bare AMP software on CPU3 of imx6quard CPU, cpu0-cpu2 run linux 6.1.1&lt;BR /&gt;before enable MMU enabled, we can read and write SCU address space(base:0x00a00000)&lt;BR /&gt;but after MMU enabled, software can't access any address space except DDR(0x10000000~0x4fffffff), if software do peripheral read access, all system hung up.&lt;BR /&gt;what's wrong with me?&lt;BR /&gt;I'm sure the MMU take effect, because some address area shared with linux for communication, if them memory attributes is not correct, linux side software can't get the data correctly. I don't known what's wrong happened? need your help&lt;/P&gt;&lt;P&gt;please refer to the attach for the MMU configuration,&lt;/P&gt;&lt;P&gt;I want to use the arm core private timer , so process blocked here.&lt;BR /&gt;the amp(cpu3 software print info as follows---don't access the peripheral address)&lt;BR /&gt;[-CPU3-]:main-(00065)]Build Time:Jan 2 2025-10:58:55.&lt;BR /&gt;[-CPU3-]:main-(00066)]float test pi = 0.000000&lt;BR /&gt;[-CPU3-]:main-(00067)]CPU1 process debug addr:0x48029e60&lt;BR /&gt;[-CPU3-]:main-(00070)]cpsr reg = 0x400001d3&lt;BR /&gt;[-CPU3-]:main-(00072)]vbar reg = 0x48000440&lt;BR /&gt;[-CPU3-]:disp_scu_all_regs-(00037)]CBAR_REG = 0x00a00000&lt;BR /&gt;[-CPU3-]:disp_scu_all_regs-(00039)]SCU_Control_Register = 0x0000007f&lt;BR /&gt;[-CPU3-]:disp_scu_all_regs-(00041)]SCU_Configuration_Register = 0x00005573&lt;BR /&gt;[-CPU3-]:disp_scu_all_regs-(00043)]SCU_CPU_Power_Status_Register = 0x00000000&lt;BR /&gt;[-CPU3-]:disp_scu_all_regs-(00046)]SCU_Invalidate_All_Registers_in_Secure_State = 0x00000000&lt;BR /&gt;[-CPU3-]:disp_scu_all_regs-(00048)]Filtering_Start_Address_Register = 0x00000000&lt;BR /&gt;[-CPU3-]:disp_scu_all_regs-(00050)]Filtering_End_Address_Register = 0x00000000&lt;BR /&gt;[-CPU3-]:disp_scu_all_regs-(00052)]SCU_Access_Control_Register = 0x0000000f&lt;BR /&gt;[-CPU3-]:disp_scu_all_regs-(00054)]SCU_Non-secure_Access_Control_Register = 0x00000000&lt;BR /&gt;[-CPU3-]:disp_private_timer_regs-(00076)]CBAR_REG = 0x00a00000&lt;BR /&gt;[-CPU3-]:disp_private_timer_regs-(00079)]TWD_TIMER_LOAD= 0x003c6cc0&lt;BR /&gt;[-CPU3-]:disp_private_timer_regs-(00081)]TWD_TIMER_COUNTER= 0x003698a9&lt;BR /&gt;[-CPU3-]:disp_private_timer_regs-(00083)]TWD_TIMER_CONTROL= 0x00000003&lt;BR /&gt;[-CPU3-]:disp_private_timer_regs-(00076)]CBAR_REG = 0x00a00000&lt;BR /&gt;[-CPU3-]:disp_private_timer_regs-(00079)]TWD_TIMER_LOAD= 0x003c6cc0&lt;BR /&gt;[-CPU3-]:disp_private_timer_regs-(00081)]TWD_TIMER_COUNTER= 0x002a9d89&lt;BR /&gt;[-CPU3-]:disp_private_timer_regs-(00083)]TWD_TIMER_CONTROL= 0x00000003&lt;BR /&gt;[-CPU3-]:mmu_table_init-(00198)]translation table init done&lt;BR /&gt;[-CPU3-]:main-(00065)]Build Time:Jan 2 2025-10:58:55.&lt;BR /&gt;[-CPU3-]:main-(00066)]float test pi = 0.000000&lt;BR /&gt;[-CPU3-]:main-(00067)]CPU1 process debug addr:0x48029e60&lt;BR /&gt;[-CPU3-]:main-(00070)]cpsr reg = 0x400001d3&lt;BR /&gt;[-CPU3-]:main-(00072)]vbar reg = 0x48000440&lt;BR /&gt;[-CPU3-]:disp_scu_all_regs-(00037)]CBAR_REG = 0x00a00000&lt;BR /&gt;[-CPU3-]:disp_scu_all_regs-(00039)]SCU_Control_Register = 0x0000007f&lt;BR /&gt;[-CPU3-]:disp_scu_all_regs-(00041)]SCU_Configuration_Register = 0x00005573&lt;BR /&gt;[-CPU3-]:disp_scu_all_regs-(00043)]SCU_CPU_Power_Status_Register = 0x00000000&lt;BR /&gt;[-CPU3-]:disp_scu_all_regs-(00046)]SCU_Invalidate_All_Registers_in_Secure_State = 0x00000000&lt;BR /&gt;[-CPU3-]:disp_scu_all_regs-(00048)]Filtering_Start_Address_Register = 0x00000000&lt;BR /&gt;[-CPU3-]:disp_scu_all_regs-(00050)]Filtering_End_Address_Register = 0x00000000&lt;BR /&gt;[-CPU3-]:disp_scu_all_regs-(00052)]SCU_Access_Control_Register = 0x0000000f&lt;BR /&gt;[-CPU3-]:disp_scu_all_regs-(00054)]SCU_Non-secure_Access_Control_Register = 0x00000000&lt;BR /&gt;[-CPU3-]:disp_private_timer_regs-(00076)]CBAR_REG = 0x00a00000&lt;BR /&gt;[-CPU3-]:disp_private_timer_regs-(00079)]TWD_TIMER_LOAD= 0x003c6cc0&lt;BR /&gt;[-CPU3-]:disp_private_timer_regs-(00081)]TWD_TIMER_COUNTER= 0x0036c697&lt;BR /&gt;[-CPU3-]:disp_private_timer_regs-(00083)]TWD_TIMER_CONTROL= 0x00000003&lt;BR /&gt;[-CPU3-]:disp_private_timer_regs-(00076)]CBAR_REG = 0x00a00000&lt;BR /&gt;[-CPU3-]:disp_private_timer_regs-(00079)]TWD_TIMER_LOAD= 0x003c6cc0&lt;BR /&gt;[-CPU3-]:disp_private_timer_regs-(00081)]TWD_TIMER_COUNTER= 0x002b0db6&lt;BR /&gt;[-CPU3-]:disp_private_timer_regs-(00083)]TWD_TIMER_CONTROL= 0x00000003&lt;/P&gt;</description>
      <pubDate>Thu, 02 Jan 2025 03:48:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/After-enbale-MMU-can-only-access-DDR-can-t-access-any-peripheral/m-p/2021000#M232519</guid>
      <dc:creator>luoqiaofa1</dc:creator>
      <dc:date>2025-01-02T03:48:10Z</dc:date>
    </item>
    <item>
      <title>回复： After enbale MMU, can only access DDR, can't access any peripheral address space include SCU add</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/After-enbale-MMU-can-only-access-DDR-can-t-access-any-peripheral/m-p/2021001#M232520</link>
      <description>after enabled MMU enabled:&lt;BR /&gt;[-CPU3-]:mmu_table_init-(00198)]translation table init done&lt;BR /&gt;[-CPU3-]:mmu_init-(00265)]ttbr=0x4802c05b&lt;BR /&gt;[-CPU3-]:Test_VirtualMMU-(00222)]L1_TblAddr = 0x4802c000&lt;BR /&gt;[-CPU3-]:Test_VirtualMMU-(00230)]L1_DescriptorAddr = 0x4802f7a8,L1_Descriptor = 0x483aa9e1&lt;BR /&gt;[-CPU3-]:Test_VirtualMMU-(00232)]L1_Descriptor = 0x483aa9e1&lt;BR /&gt;[-CPU3-]:Test_VirtualMMU-(00237)]L2_TableBaseAddr = 0x483aa800,L2_DescriptorAddr = 0x483aab6c,L2_Descriptor = 0xdeadb576&lt;BR /&gt;[-CPU3-]:Test_VirtualMMU-(00240)]L2_Descriptor = 0xdeadb576&lt;BR /&gt;[-CPU3-]:Test_VirtualMMU-(00245)]va = 0xdeadbeef,pa = 0xdeadbeef&lt;BR /&gt;[-CPU3-]:main-(00104)]SCU_BASE=0x00a00000&lt;BR /&gt;[-CPU3-]:main-(00106)]Enable MMU&lt;BR /&gt;[-CPU3-]:disp_cp15_regs-(00104)]MIDR= 0x412fc09a&lt;BR /&gt;[-CPU3-]:disp_cp15_regs-(00106)]REVIDR=0x412fc09a&lt;BR /&gt;[-CPU3-]:disp_cp15_regs-(00108)]SCTRL= 0x10c5387d&lt;BR /&gt;[-CPU3-]:disp_cp15_regs-(00110)]DACR= 0x55555555&lt;BR /&gt;[-CPU3-]:disp_cp15_regs-(00112)]ACTLR= 0x00000047&lt;BR /&gt;[-CPU3-]:disp_cp15_regs-(00114)]CPACR= 0x00f00000&lt;BR /&gt;[-CPU3-]:disp_cp15_regs-(00116)]NSACR= 0x00000000&lt;BR /&gt;[-CPU3-]:main-(00113)]Enable SIMD VFP&lt;BR /&gt;[-CPU3-]:main-(00115)]Neon Test ...&lt;BR /&gt;I: 7298-Q: -8657|I: 28513-Q: 7192|I:-14294-Q: 4935|I: 3797-Q: 25403|I:-13302-Q: 18999|I: 17846-Q:-31606|I: 3377-Q: -1452|I: 690-Q: 10603|I: -2352-Q:-20951|I:-24549-Q: 521|I: 8485-Q: 2026|I:-10757-Q: 30099|I: 5764-Q: 1393|I: -1091-Q: 5758|I:&lt;BR /&gt;[-CPU3-]:TestNeon-(00059)]C Intrinsics done&lt;BR /&gt;I: 7298-Q: -8657|I: 28513-Q: 7192|I:-14294-Q: 4935|I: 3797-Q: 25403|I:-13302-Q: 18999|I: 17846-Q:-31606|I: 3377-Q: -1452|I: 690-Q: 10603|I: -2352-Q:-20951|I:-24549-Q: 521|I: 8485-Q: 2026|I:-10757-Q: 30099|I: 5764-Q: 1393|I: -1091-Q: 5758|I:&lt;BR /&gt;[-CPU3-]:TestNeon-(00095)]NEON Intrinsics done&lt;BR /&gt;[-CPU3-]:TestNeon-(00096)]int convert to short test&lt;BR /&gt;[-CPU3-]:TestNeon-(00097)]RAW Data:&lt;BR /&gt;25791 531569 -2334455 -11515&lt;BR /&gt;[-CPU3-]:TestNeon-(00103)]C:&lt;BR /&gt;25791 7281 24841 -11515&lt;BR /&gt;[-CPU3-]:TestNeon-(00110)]NEON:&lt;BR /&gt;25791 7281 24841 -11515&lt;BR /&gt;[-CPU3-]:TestNeon-(00118)]NEON saturated:&lt;BR /&gt;25791 32767 -32768 -11515&lt;BR /&gt;[-CPU3-]:main-(00117)]Normal Distribution Random number Test ...</description>
      <pubDate>Thu, 02 Jan 2025 03:55:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/After-enbale-MMU-can-only-access-DDR-can-t-access-any-peripheral/m-p/2021001#M232520</guid>
      <dc:creator>luoqiaofa1</dc:creator>
      <dc:date>2025-01-02T03:55:59Z</dc:date>
    </item>
  </channel>
</rss>