<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Need to run RTSP server in i.mx.8mp in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Need-to-run-RTSP-server-in-i-mx-8mp/m-p/2020000#M232427</link>
    <description>&lt;P&gt;hi Joanxie,&lt;/P&gt;&lt;P&gt;We are using bsp&amp;nbsp;LF6.6.3_1.0.0.&lt;/P&gt;&lt;P&gt;We are not able to apply git patch as instructed in the link.&amp;nbsp;&lt;/P&gt;&lt;P&gt;For example, the link instructs to execute this command&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;&lt;SPAN&gt;$ cd &amp;lt;yocto_path&amp;gt;/sources/meta-fsl-bsp-release/&lt;/SPAN&gt;&lt;/PRE&gt;&lt;P&gt;but, I don't see a folder with the name 'meta-fst-bsp-release'&amp;nbsp;&amp;nbsp;&lt;BR /&gt;the patch file refers to a .bb file 'imx/meta-bsp/recipes-multimedia/gstreamer/gstreamer1.0-plugins-good_1.14.imx.bb' this folder path doesn't exist in the repo I cloned.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The link I mentioned is 4 years old, is there a latest one?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please share any latest documentation on running the RTSP Server in i.MX8MP&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 27 Dec 2024 09:26:00 GMT</pubDate>
    <dc:creator>sunilaerxlabs</dc:creator>
    <dc:date>2024-12-27T09:26:00Z</dc:date>
    <item>
      <title>Need to run RTSP server in i.mx.8mp</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Need-to-run-RTSP-server-in-i-mx-8mp/m-p/2019746#M232409</link>
      <description>&lt;P&gt;Dear NXP Community,&lt;/P&gt;&lt;P&gt;I hope this message finds you well.&lt;/P&gt;&lt;P&gt;My name is Sunil, and I am a Lead Software Engineer at AerXLabs Inc. We are currently developing a video streaming device utilizing the i.MX8MP processor and requires assistance with running an RTSP server on the platform to stream video from a connected camera.&lt;/P&gt;&lt;P&gt;We have a functional implementation of this requirement that was developed for a different processor. The existing solution leverages the GStreamer module &lt;STRONG&gt;gst-variable-rtsp-server&lt;/STRONG&gt;. However, we are encountering challenges while attempting to install this module on the i.MX8MP.&lt;/P&gt;&lt;P&gt;We referred to the documentation available at &lt;A title="NXP community link for RTSP server support in i.MX8" href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8-RTSP-Streaming-Support/ta-p/1121720" target="_blank" rel="noopener"&gt;this link&lt;/A&gt;, but the folder structure and instructions do not align with the setup on our end. We are using NXP's guide &lt;STRONG&gt;IMXLXYOCTOUG&lt;/STRONG&gt; to set up the Linux Git repository on our host PC. The Yocto distribution we are working with is &lt;STRONG&gt;fsl-imx-xwayland&lt;/STRONG&gt;, and the target device selected is &lt;STRONG&gt;imx8mp-lpddr4-evk&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;Could you kindly provide guidance or detailed steps for installing the GStreamer RTSP server on the i.MX8MP?&lt;/P&gt;&lt;P&gt;Your assistance in this matter would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Sunil&lt;BR /&gt;Lead Software Engineer&lt;BR /&gt;AerXLabs Inc.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 26 Dec 2024 17:16:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Need-to-run-RTSP-server-in-i-mx-8mp/m-p/2019746#M232409</guid>
      <dc:creator>sunilaerxlabs</dc:creator>
      <dc:date>2024-12-26T17:16:55Z</dc:date>
    </item>
    <item>
      <title>Re: Need to run RTSP server in i.mx.8mp</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Need-to-run-RTSP-server-in-i-mx-8mp/m-p/2019849#M232415</link>
      <description>&lt;P&gt;We referred to the documentation available at &lt;A title="NXP community link for RTSP server support in i.MX8" href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8-RTSP-Streaming-Support/ta-p/1121720" target="_blank" rel="noopener"&gt;this link&lt;/A&gt;, but the folder structure and instructions do not align with the setup on our end.&lt;/P&gt;
&lt;P&gt;&amp;gt;what bsp version do you use? what issue do you have when you add this in your bsp according to this link? pls share more detailed information here&lt;/P&gt;</description>
      <pubDate>Fri, 27 Dec 2024 03:35:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Need-to-run-RTSP-server-in-i-mx-8mp/m-p/2019849#M232415</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2024-12-27T03:35:12Z</dc:date>
    </item>
    <item>
      <title>Re: Need to run RTSP server in i.mx.8mp</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Need-to-run-RTSP-server-in-i-mx-8mp/m-p/2020000#M232427</link>
      <description>&lt;P&gt;hi Joanxie,&lt;/P&gt;&lt;P&gt;We are using bsp&amp;nbsp;LF6.6.3_1.0.0.&lt;/P&gt;&lt;P&gt;We are not able to apply git patch as instructed in the link.&amp;nbsp;&lt;/P&gt;&lt;P&gt;For example, the link instructs to execute this command&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;&lt;SPAN&gt;$ cd &amp;lt;yocto_path&amp;gt;/sources/meta-fsl-bsp-release/&lt;/SPAN&gt;&lt;/PRE&gt;&lt;P&gt;but, I don't see a folder with the name 'meta-fst-bsp-release'&amp;nbsp;&amp;nbsp;&lt;BR /&gt;the patch file refers to a .bb file 'imx/meta-bsp/recipes-multimedia/gstreamer/gstreamer1.0-plugins-good_1.14.imx.bb' this folder path doesn't exist in the repo I cloned.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The link I mentioned is 4 years old, is there a latest one?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please share any latest documentation on running the RTSP Server in i.MX8MP&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 27 Dec 2024 09:26:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Need-to-run-RTSP-server-in-i-mx-8mp/m-p/2020000#M232427</guid>
      <dc:creator>sunilaerxlabs</dc:creator>
      <dc:date>2024-12-27T09:26:00Z</dc:date>
    </item>
    <item>
      <title>Re: Need to run RTSP server in i.mx.8mp</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Need-to-run-RTSP-server-in-i-mx-8mp/m-p/2020129#M232438</link>
      <description>&lt;P&gt;this patch is for old bsp, you don't need to add it into the new bsp, just install the RTSP plugins&lt;/P&gt;</description>
      <pubDate>Sat, 28 Dec 2024 02:26:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Need-to-run-RTSP-server-in-i-mx-8mp/m-p/2020129#M232438</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2024-12-28T02:26:02Z</dc:date>
    </item>
  </channel>
</rss>