<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX53 User Defined Button in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX53-User-Defined-Button/m-p/2019310#M232359</link>
    <description>&lt;P&gt;Which board are you using? NXP i.MX53 QSB Board? If yes, I will confirm it for you, as it is too old product.&lt;/P&gt;</description>
    <pubDate>Wed, 25 Dec 2024 08:40:51 GMT</pubDate>
    <dc:creator>Rita_Wang</dc:creator>
    <dc:date>2024-12-25T08:40:51Z</dc:date>
    <item>
      <title>iMX53 User Defined Button</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX53-User-Defined-Button/m-p/2017374#M232200</link>
      <description>&lt;P&gt;I see on the schematic that SW4 and SW5 are buttons that are meant to be reprogrammed by the user. However I am having trouble finding documentation or example code of how this can be done. Ideally I would want to read the state of a button and light up an on-board LED when the button is pressed. Could someone please assist me in accomplishing this?&lt;/P&gt;</description>
      <pubDate>Thu, 19 Dec 2024 17:17:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX53-User-Defined-Button/m-p/2017374#M232200</guid>
      <dc:creator>AOlvera</dc:creator>
      <dc:date>2024-12-19T17:17:17Z</dc:date>
    </item>
    <item>
      <title>Re: iMX53 User Defined Button</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX53-User-Defined-Button/m-p/2019310#M232359</link>
      <description>&lt;P&gt;Which board are you using? NXP i.MX53 QSB Board? If yes, I will confirm it for you, as it is too old product.&lt;/P&gt;</description>
      <pubDate>Wed, 25 Dec 2024 08:40:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX53-User-Defined-Button/m-p/2019310#M232359</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2024-12-25T08:40:51Z</dc:date>
    </item>
  </channel>
</rss>