<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ISP_FLASH_TRIG_0 and ISP_SHUTTER_TRIG_0 meaning in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/ISP-FLASH-TRIG-0-and-ISP-SHUTTER-TRIG-0-meaning/m-p/2018485#M232278</link>
    <description>&lt;P&gt;they are defined by the ISP IP owner, why do you need to know this? SHUTTER&amp;nbsp; TRIG clock is for ISP shutter module, and flash trigger is for flash light control, this is all I can share with you in the public community &lt;/P&gt;</description>
    <pubDate>Mon, 23 Dec 2024 09:09:02 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2024-12-23T09:09:02Z</dc:date>
    <item>
      <title>ISP_FLASH_TRIG_0 and ISP_SHUTTER_TRIG_0 meaning</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ISP-FLASH-TRIG-0-and-ISP-SHUTTER-TRIG-0-meaning/m-p/2018190#M232250</link>
      <description>&lt;P class=""&gt;Hi everyone,&lt;/P&gt;&lt;P class=""&gt;I'm working with the NXP i.MX 8M Plus SoC and trying to understand the functionality of two ISP (Image Signal Processor) trigger signals:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;ISP_SHUTTER_TRIG_0&lt;/LI&gt;&lt;LI&gt;ISP_FLASH_TRIG_0&lt;/LI&gt;&lt;/OL&gt;</description>
      <pubDate>Sun, 22 Dec 2024 14:48:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ISP-FLASH-TRIG-0-and-ISP-SHUTTER-TRIG-0-meaning/m-p/2018190#M232250</guid>
      <dc:creator>maiakhoa</dc:creator>
      <dc:date>2024-12-22T14:48:10Z</dc:date>
    </item>
    <item>
      <title>Re: ISP_FLASH_TRIG_0 and ISP_SHUTTER_TRIG_0 meaning</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ISP-FLASH-TRIG-0-and-ISP-SHUTTER-TRIG-0-meaning/m-p/2018485#M232278</link>
      <description>&lt;P&gt;they are defined by the ISP IP owner, why do you need to know this? SHUTTER&amp;nbsp; TRIG clock is for ISP shutter module, and flash trigger is for flash light control, this is all I can share with you in the public community &lt;/P&gt;</description>
      <pubDate>Mon, 23 Dec 2024 09:09:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ISP-FLASH-TRIG-0-and-ISP-SHUTTER-TRIG-0-meaning/m-p/2018485#M232278</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2024-12-23T09:09:02Z</dc:date>
    </item>
    <item>
      <title>Re: ISP_FLASH_TRIG_0 and ISP_SHUTTER_TRIG_0 meaning</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ISP-FLASH-TRIG-0-and-ISP-SHUTTER-TRIG-0-meaning/m-p/2020220#M232446</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/39586"&gt;@joanxie&lt;/a&gt;&amp;nbsp;thank you for the info&lt;/P&gt;</description>
      <pubDate>Mon, 30 Dec 2024 01:36:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ISP-FLASH-TRIG-0-and-ISP-SHUTTER-TRIG-0-meaning/m-p/2020220#M232446</guid>
      <dc:creator>maiakhoa</dc:creator>
      <dc:date>2024-12-30T01:36:54Z</dc:date>
    </item>
  </channel>
</rss>