<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Kernel panic in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-panic/m-p/2017869#M232235</link>
    <description>&lt;P&gt;I am developing the images using Yocto for my custom board running on IMX6Q. It has been working until I need to install nmap on the platform and the kernel will become kernel panic when it boots up.&lt;/P&gt;&lt;P&gt;The size of the uboot, dtb and zImage.bin stay around the same but the rootfs has been increased from 55MB to 88MB and I have adjusted the partitions accordingly in kernel dtb and uboot. I have also changed the rootfs image size to 90000.&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I removed the nmap package and recompiled the whole images again, the platform can boot up as normal.&lt;/P&gt;&lt;P&gt;My question is if there is other settings which I have missed?&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 20 Dec 2024 11:54:43 GMT</pubDate>
    <dc:creator>binary7knight</dc:creator>
    <dc:date>2024-12-20T11:54:43Z</dc:date>
    <item>
      <title>Kernel panic</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-panic/m-p/2017869#M232235</link>
      <description>&lt;P&gt;I am developing the images using Yocto for my custom board running on IMX6Q. It has been working until I need to install nmap on the platform and the kernel will become kernel panic when it boots up.&lt;/P&gt;&lt;P&gt;The size of the uboot, dtb and zImage.bin stay around the same but the rootfs has been increased from 55MB to 88MB and I have adjusted the partitions accordingly in kernel dtb and uboot. I have also changed the rootfs image size to 90000.&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I removed the nmap package and recompiled the whole images again, the platform can boot up as normal.&lt;/P&gt;&lt;P&gt;My question is if there is other settings which I have missed?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 20 Dec 2024 11:54:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-panic/m-p/2017869#M232235</guid>
      <dc:creator>binary7knight</dc:creator>
      <dc:date>2024-12-20T11:54:43Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel panic</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-panic/m-p/2019173#M232333</link>
      <description>&lt;P&gt;hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/244842"&gt;@binary7knight&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Will reply back to you in your another ticket with similar issue.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Wed, 25 Dec 2024 02:14:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-panic/m-p/2019173#M232333</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2024-12-25T02:14:20Z</dc:date>
    </item>
  </channel>
</rss>