<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: HFP and A2DP IMPLEMENTATION WITH 88W8987 Based BT module in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/HFP-and-A2DP-IMPLEMENTATION-WITH-88W8987-Based-BT-module/m-p/2017445#M232205</link>
    <description>&lt;P&gt;reminder.&lt;/P&gt;</description>
    <pubDate>Thu, 19 Dec 2024 20:59:51 GMT</pubDate>
    <dc:creator>Wobaffet</dc:creator>
    <dc:date>2024-12-19T20:59:51Z</dc:date>
    <item>
      <title>HFP and A2DP IMPLEMENTATION WITH 88W8987 Based BT module</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HFP-and-A2DP-IMPLEMENTATION-WITH-88W8987-Based-BT-module/m-p/2016152#M232146</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are trying to implement A2DP and HFP with i.MX8MP custom board. We can load the firmware and connect to any BT device, however when we try to&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;root@imx8mp-lpddr4-evk:~# pactl list cards
Card #0
	Name: alsa_card.platform-sound-bt-sco
	Driver: module-alsa-card.c
	Owner Module: 6
	Properties:
		alsa.card = "1"
		alsa.card_name = "bt-sco-audio"
		alsa.long_card_name = "bt-sco-audio"
		device.bus_path = "platform-sound-bt-sco"
		sysfs.path = "/devices/platform/sound-bt-sco/sound/card1"
		device.form_factor = "internal"
		device.string = "1"
		device.description = "Built-in Audio"
		module-udev-detect.discovered = "1"
		device.icon_name = "audio-card"
	Profiles:
		input:mono-fallback: Mono Input (sinks: 0, sources: 1, priority: 1, available: yes)
		output:mono-fallback: Mono Output (sinks: 1, sources: 0, priority: 100, available: yes)
		output:mono-fallback+input:mono-fallback: Mono Output + Mono Input (sinks: 1, sources: 1, priority: 101, available: yes)
		off: Off (sinks: 0, sources: 0, priority: 0, available: yes)
	Active Profile: output:mono-fallback+input:mono-fallback
	Ports:
		analog-input: Analog Input (type: Analog, priority: 10000, latency offset: 0 usec, availability unknown)
			Part of profile(s): input:mono-fallback, output:mono-fallback+input:mono-fallback
		analog-output: Analog Output (type: Analog, priority: 9900, latency offset: 0 usec, availability unknown)
			Part of profile(s): output:mono-fallback, output:mono-fallback+input:mono-fallback

Card #1
	Name: alsa_card.platform-sound-tlv320aic31xx
	Driver: module-alsa-card.c
	Owner Module: 7
	Properties:
		alsa.card = "0"
		alsa.card_name = "tlv320aic31xx-Codec"
		alsa.long_card_name = "tlv320aic31xx-Codec"
		device.bus_path = "platform-sound-tlv320aic31xx"
		sysfs.path = "/devices/platform/sound-tlv320aic31xx/sound/card0"
		device.form_factor = "internal"
		device.string = "0"
		device.description = "Built-in Audio"
		module-udev-detect.discovered = "1"
		device.icon_name = "audio-card"
	Profiles:
		input:stereo-fallback: Stereo Input (sinks: 0, sources: 1, priority: 51, available: yes)
		output:stereo-fallback: Stereo Output (sinks: 1, sources: 0, priority: 5100, available: yes)
		output:stereo-fallback+input:stereo-fallback: Stereo Output + Stereo Input (sinks: 1, sources: 1, priority: 5151, available: yes)
		off: Off (sinks: 0, sources: 0, priority: 0, available: yes)
	Active Profile: output:stereo-fallback+input:stereo-fallback
	Ports:
		analog-input: Analog Input (type: Analog, priority: 10000, latency offset: 0 usec, availability unknown)
			Part of profile(s): input:stereo-fallback, output:stereo-fallback+input:stereo-fallback
		analog-output-speaker: Speakers (type: Speaker, priority: 10000, latency offset: 0 usec, availability unknown)
			Properties:
				device.icon_name = "audio-speakers"
			Part of profile(s): output:stereo-fallback, output:stereo-fallback+input:stereo-fallback&lt;/LI-CODE&gt;&lt;P&gt;We can't detect a card for the connected devices &lt;A href="https://community.nxp.com/t5/Wireless-Connectivity-Knowledge/The-A2DP-Audio-Configuration-Based-On-88W8987-iMX8MN-EVK-And/ta-p/1268395" target="_self"&gt;as can be seen on this guide&lt;/A&gt;.&amp;nbsp; Even though we can detect Audio sink feature like this&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;Device B8:D5:0B:FA:89:8E (public)
	Name: Busra JBL
	Alias: Busra JBL
	Class: 0x00240414
	Icon: audio-card
	Paired: yes
	Bonded: yes
	Trusted: yes
	Blocked: no
	Connected: yes
	LegacyPairing: no
	UUID: Audio Sink                (0000110b-0000-1000-8000-00805f9b34fb)
	UUID: A/V Remote Control Target (0000110c-0000-1000-8000-00805f9b34fb)
	UUID: A/V Remote Control        (0000110e-0000-1000-8000-00805f9b34fb)
	UUID: Handsfree                 (0000111e-0000-1000-8000-00805f9b34fb)
	UUID: PnP Information           (00001200-0000-1000-8000-00805f9b34fb)
	UUID: Generic Access Profile    (00001800-0000-1000-8000-00805f9b34fb)
	UUID: Generic Attribute Profile (00001801-0000-1000-8000-00805f9b34fb)
	UUID: CSR                       (0000fe8f-0000-1000-8000-00805f9b34fb)
	UUID: Vendor specific           (65786365-6c70-6f69-6e74-2e636f6d0000)
	Modalias: bluetooth:v000ApFFFFdFFFF&lt;/LI-CODE&gt;&lt;P&gt;We are on 5.15 kernel and our distro has these packages&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;IMAGE_INSTALL:append = "dbus packagegroup-tools-bluetooth pulseaudio pulseaudio-server pulseaudio-miscbluealsa alsa-lib bluez5 bluez5-noinst-tools bluez5-obex openobex obexftp"&lt;/LI-CODE&gt;&lt;P&gt;When we try to load discover module we get&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;root@imx8mp-lpddr4-evk:~# pactl load-module module-bluez5-discover
Failure: Module initialization failed&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;Also the list of pactl modules are attached.&lt;/P&gt;&lt;P&gt;What could be the issue here?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Wed, 18 Dec 2024 15:05:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HFP-and-A2DP-IMPLEMENTATION-WITH-88W8987-Based-BT-module/m-p/2016152#M232146</guid>
      <dc:creator>Wobaffet</dc:creator>
      <dc:date>2024-12-18T15:05:47Z</dc:date>
    </item>
    <item>
      <title>Re: HFP and A2DP IMPLEMENTATION WITH 88W8987 Based BT module</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HFP-and-A2DP-IMPLEMENTATION-WITH-88W8987-Based-BT-module/m-p/2017445#M232205</link>
      <description>&lt;P&gt;reminder.&lt;/P&gt;</description>
      <pubDate>Thu, 19 Dec 2024 20:59:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HFP-and-A2DP-IMPLEMENTATION-WITH-88W8987-Based-BT-module/m-p/2017445#M232205</guid>
      <dc:creator>Wobaffet</dc:creator>
      <dc:date>2024-12-19T20:59:51Z</dc:date>
    </item>
    <item>
      <title>Re: HFP and A2DP IMPLEMENTATION WITH 88W8987 Based BT module</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HFP-and-A2DP-IMPLEMENTATION-WITH-88W8987-Based-BT-module/m-p/2019050#M232316</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you show me how you connect the module?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;What is the boot up log?&lt;/P&gt;
&lt;P&gt;Please also send me the device tree file of your board for checking.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Jimmy&lt;/P&gt;</description>
      <pubDate>Tue, 24 Dec 2024 09:45:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HFP-and-A2DP-IMPLEMENTATION-WITH-88W8987-Based-BT-module/m-p/2019050#M232316</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2024-12-24T09:45:58Z</dc:date>
    </item>
  </channel>
</rss>