<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: fbGetDisplayByIndex() missing from libEGL.so since imx-gpu-viv-6.4.11.p2.6 (L6.6.23_2.0.0)</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/fbGetDisplayByIndex-missing-from-libEGL-so-since-imx-gpu-viv-6-4/m-p/2016698#M232150</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;If you are using i.MX8MM, please use eglfs_kms which using drm api.&lt;/P&gt;
&lt;P&gt;The eglfs_vivi is for i.MX6, the gpu library has removed the FB support on i.MX8&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
    <pubDate>Thu, 19 Dec 2024 01:28:38 GMT</pubDate>
    <dc:creator>Zhiming_Liu</dc:creator>
    <dc:date>2024-12-19T01:28:38Z</dc:date>
    <item>
      <title>fbGetDisplayByIndex() missing from libEGL.so since imx-gpu-viv-6.4.11.p2.6 (L6.6.23_2.0.0)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/fbGetDisplayByIndex-missing-from-libEGL-so-since-imx-gpu-viv-6-4/m-p/2015418#M232104</link>
      <description>&lt;P&gt;Since imx-gpu-viv-6.4.11.p2.6 the symbols fbGetDisplayByIndex()/fbGetDisplay()/etc. are missing from libEGL.so. The symbols are defined in gpu-core/usr/include/EGL/eglvivante.h&lt;/P&gt;&lt;P&gt;The configure step of qtbase uses fbGetDisplayByIndex() to determine if the vivante backend shall be compiled. The same function is also used functionally in QT.&lt;/P&gt;&lt;P&gt;Are theses symbols missing on purpose? If yes, in which library are they available now?&lt;/P&gt;</description>
      <pubDate>Tue, 17 Dec 2024 15:50:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/fbGetDisplayByIndex-missing-from-libEGL-so-since-imx-gpu-viv-6-4/m-p/2015418#M232104</guid>
      <dc:creator>klarinettli</dc:creator>
      <dc:date>2024-12-17T15:50:57Z</dc:date>
    </item>
    <item>
      <title>Re: fbGetDisplayByIndex() missing from libEGL.so since imx-gpu-viv-6.4.11.p2.6 (L6.6.23_2.0.0)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/fbGetDisplayByIndex-missing-from-libEGL-so-since-imx-gpu-viv-6-4/m-p/2015857#M232129</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Which platform are you based on? Wayland or eglfs? And can you share the error you are facing?&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Wed, 18 Dec 2024 06:49:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/fbGetDisplayByIndex-missing-from-libEGL-so-since-imx-gpu-viv-6-4/m-p/2015857#M232129</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2024-12-18T06:49:15Z</dc:date>
    </item>
    <item>
      <title>Re: fbGetDisplayByIndex() missing from libEGL.so since imx-gpu-viv-6.4.11.p2.6 (L6.6.23_2.0.0)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/fbGetDisplayByIndex-missing-from-libEGL-so-since-imx-gpu-viv-6-4/m-p/2016143#M232145</link>
      <description>&lt;P&gt;We're using the eglfs platform.&lt;/P&gt;&lt;P&gt;As shown below, the "fbGetDisplayByIndex" symbol remains in the header file but is missing in the actual libraries in 6.4.11.p2.6:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;❯ grep -r fbGetDisplayByIndex imx-gpu-viv-6.4.11.p2.2-aarch32-fd0148d
imx-gpu-viv-6.4.11.p2.2-aarch32-fd0148d/gpu-core/usr/include/EGL/eglvivante.h:fbGetDisplayByIndex(
grep: imx-gpu-viv-6.4.11.p2.2-aarch32-fd0148d/gpu-core/usr/lib/fb/libEGL.so.1.5.0: binary file matches
grep: imx-gpu-viv-6.4.11.p2.2-aarch32-fd0148d/gpu-core/usr/lib/fb/libVDK.so.1.2.0: binary file matches
grep: imx-gpu-viv-6.4.11.p2.2-aarch32-fd0148d/gpu-core/usr/lib/wayland/libEGL.so.1.5.0: binary file matches

❯ grep -r fbGetDisplayByIndex imx-gpu-viv-6.4.11.p2.6-aarch64-bc7b6a2
imx-gpu-viv-6.4.11.p2.6-aarch64-bc7b6a2/gpu-core/usr/include/EGL/eglvivante.h:fbGetDisplayByIndex(
&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 18 Dec 2024 14:54:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/fbGetDisplayByIndex-missing-from-libEGL-so-since-imx-gpu-viv-6-4/m-p/2016143#M232145</guid>
      <dc:creator>klarinettli</dc:creator>
      <dc:date>2024-12-18T14:54:39Z</dc:date>
    </item>
    <item>
      <title>Re: fbGetDisplayByIndex() missing from libEGL.so since imx-gpu-viv-6.4.11.p2.6 (L6.6.23_2.0.0)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/fbGetDisplayByIndex-missing-from-libEGL-so-since-imx-gpu-viv-6-4/m-p/2016698#M232150</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;If you are using i.MX8MM, please use eglfs_kms which using drm api.&lt;/P&gt;
&lt;P&gt;The eglfs_vivi is for i.MX6, the gpu library has removed the FB support on i.MX8&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Thu, 19 Dec 2024 01:28:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/fbGetDisplayByIndex-missing-from-libEGL-so-since-imx-gpu-viv-6-4/m-p/2016698#M232150</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2024-12-19T01:28:38Z</dc:date>
    </item>
  </channel>
</rss>