<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SPDIF Rx Clock (SPDIF_SR_CLK)  pulse rate in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SPDIF-Rx-Clock-SPDIF-SR-CLK-pulse-rate/m-p/2015239#M232094</link>
    <description>&lt;P&gt;I'm planning to use the SPDIF from the i.MX RT 1060.&lt;BR /&gt;The reference manual (IMXRT1060RM.pdf) has the following explanation in 40.3.1.7:&lt;/P&gt;&lt;P&gt;&amp;gt; After DPLL has locked, the pulses are generated, and the average pulse rate is 128 x the sampling frequency.(For a 44.1 Khz input sampling frequency, the average pulse rate = 128 x 44.1 Khz.)&lt;/P&gt;&lt;P&gt;When the SPDIF input is 44100Hz, 88200Hz, or 176400Hz, I want to get an output of 22,579,200Hz.&lt;BR /&gt;When the SPDIF input is 48000Hz, 96000Hz, or 19200Hz, I want to get an output of 22,579,200Hz.&lt;BR /&gt;To achieve this I want to change the multiplier to x128.&lt;/P&gt;&lt;P&gt;Is it possible to change the x128 magnification?&lt;/P&gt;</description>
    <pubDate>Tue, 17 Dec 2024 11:18:50 GMT</pubDate>
    <dc:creator>yoshida_satoru</dc:creator>
    <dc:date>2024-12-17T11:18:50Z</dc:date>
    <item>
      <title>SPDIF Rx Clock (SPDIF_SR_CLK)  pulse rate</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPDIF-Rx-Clock-SPDIF-SR-CLK-pulse-rate/m-p/2015239#M232094</link>
      <description>&lt;P&gt;I'm planning to use the SPDIF from the i.MX RT 1060.&lt;BR /&gt;The reference manual (IMXRT1060RM.pdf) has the following explanation in 40.3.1.7:&lt;/P&gt;&lt;P&gt;&amp;gt; After DPLL has locked, the pulses are generated, and the average pulse rate is 128 x the sampling frequency.(For a 44.1 Khz input sampling frequency, the average pulse rate = 128 x 44.1 Khz.)&lt;/P&gt;&lt;P&gt;When the SPDIF input is 44100Hz, 88200Hz, or 176400Hz, I want to get an output of 22,579,200Hz.&lt;BR /&gt;When the SPDIF input is 48000Hz, 96000Hz, or 19200Hz, I want to get an output of 22,579,200Hz.&lt;BR /&gt;To achieve this I want to change the multiplier to x128.&lt;/P&gt;&lt;P&gt;Is it possible to change the x128 magnification?&lt;/P&gt;</description>
      <pubDate>Tue, 17 Dec 2024 11:18:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPDIF-Rx-Clock-SPDIF-SR-CLK-pulse-rate/m-p/2015239#M232094</guid>
      <dc:creator>yoshida_satoru</dc:creator>
      <dc:date>2024-12-17T11:18:50Z</dc:date>
    </item>
    <item>
      <title>Re: SPDIF Rx Clock (SPDIF_SR_CLK)  pulse rate</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPDIF-Rx-Clock-SPDIF-SR-CLK-pulse-rate/m-p/2017581#M232208</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/77980"&gt;@yoshida_satoru&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you for your interest in the NXP MIMXRT product, I would&amp;nbsp; like to provide service for you.&lt;/P&gt;
&lt;P&gt;As you mentioned in&amp;nbsp;&lt;SPAN&gt;IMXRT1060RM reference manual, It describe "After DPLL has locked, the pulses are generated, and the average pulse rate is 128 x the sampling frequency."&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;I don't think It is possible to change the x128 magnification.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;The SPDIF interface of&amp;nbsp; i.MX RT1060 chip is designed as a fixed multiplier of x128, and user can not be configured to use a different multiplier.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="mayliu1_0-1734663182602.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/316783i0C7F68B8CE823D87/image-size/medium?v=v2&amp;amp;px=400" role="button" title="mayliu1_0-1734663182602.png" alt="mayliu1_0-1734663182602.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;mayliu1_0-1734663182602.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Wish it helps you.&lt;BR /&gt;If you still have question about it, please kindly let me know.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;mayliu&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 20 Dec 2024 03:21:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPDIF-Rx-Clock-SPDIF-SR-CLK-pulse-rate/m-p/2017581#M232208</guid>
      <dc:creator>mayliu1</dc:creator>
      <dc:date>2024-12-20T03:21:43Z</dc:date>
    </item>
  </channel>
</rss>