<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx8mq Android14 no use gki kernel in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8mq-Android14-no-use-gki-kernel/m-p/2012650#M231899</link>
    <description>Hi Bio_TICFSL&lt;BR /&gt;There are two questions to consult:&lt;BR /&gt;1. The boot compiled using the no gki method has been burning in the Starting kernel .... restart&lt;BR /&gt;2. Does imx8MQ support mipi screen display under uboot? I checked the source code and found that imx8mm and imx8mp support it, but imx8MQ does not</description>
    <pubDate>Thu, 12 Dec 2024 07:50:48 GMT</pubDate>
    <dc:creator>aber</dc:creator>
    <dc:date>2024-12-12T07:50:48Z</dc:date>
    <item>
      <title>imx8mq Android14 no use gki kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mq-Android14-no-use-gki-kernel/m-p/2011899#M231853</link>
      <description>&lt;P&gt;Hi nxp&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp;Can I skip using the GKI kernel on imx8mq Android14. &lt;SPAN&gt;LOADABLE_KERNEL_MODULE&amp;nbsp;&lt;/SPAN&gt;= false Do not load using module mode. I have tried but the system cannot start properly.&lt;/P&gt;</description>
      <pubDate>Wed, 11 Dec 2024 10:08:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mq-Android14-no-use-gki-kernel/m-p/2011899#M231853</guid>
      <dc:creator>aber</dc:creator>
      <dc:date>2024-12-11T10:08:25Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mq Android14 no use gki kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mq-Android14-no-use-gki-kernel/m-p/2012097#M231862</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;No you can't some modules are need it , such as the GPU module.&lt;/P&gt;
&lt;P&gt;regards&lt;/P&gt;</description>
      <pubDate>Wed, 11 Dec 2024 14:48:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mq-Android14-no-use-gki-kernel/m-p/2012097#M231862</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-12-11T14:48:26Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mq Android14 no use gki kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mq-Android14-no-use-gki-kernel/m-p/2012103#M231864</link>
      <description>Hi Bio_TICFSL&lt;BR /&gt;Thank you for your reply. I would like to know how to run on imx8MQ without using the GKI method. Is there any specific documentation available?</description>
      <pubDate>Wed, 11 Dec 2024 14:53:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mq-Android14-no-use-gki-kernel/m-p/2012103#M231864</guid>
      <dc:creator>aber</dc:creator>
      <dc:date>2024-12-11T14:53:09Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mq Android14 no use gki kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mq-Android14-no-use-gki-kernel/m-p/2012105#M231865</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Boot.img is default GKI image, almost all build in kernel are inside this image. GKI&lt;BR /&gt;source code are not included in Anroid14 build environment.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Wed, 11 Dec 2024 14:56:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mq-Android14-no-use-gki-kernel/m-p/2012105#M231865</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-12-11T14:56:00Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mq Android14 no use gki kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mq-Android14-no-use-gki-kernel/m-p/2012106#M231866</link>
      <description>Yes, so I want to know if it can be achieved without GKI.</description>
      <pubDate>Wed, 11 Dec 2024 14:57:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mq-Android14-no-use-gki-kernel/m-p/2012106#M231866</guid>
      <dc:creator>aber</dc:creator>
      <dc:date>2024-12-11T14:57:43Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mq Android14 no use gki kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mq-Android14-no-use-gki-kernel/m-p/2012650#M231899</link>
      <description>Hi Bio_TICFSL&lt;BR /&gt;There are two questions to consult:&lt;BR /&gt;1. The boot compiled using the no gki method has been burning in the Starting kernel .... restart&lt;BR /&gt;2. Does imx8MQ support mipi screen display under uboot? I checked the source code and found that imx8mm and imx8mp support it, but imx8MQ does not</description>
      <pubDate>Thu, 12 Dec 2024 07:50:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mq-Android14-no-use-gki-kernel/m-p/2012650#M231899</guid>
      <dc:creator>aber</dc:creator>
      <dc:date>2024-12-12T07:50:48Z</dc:date>
    </item>
  </channel>
</rss>