<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: i.MX6DL boot strange result: boot mode connect Serial downloader mode (USB OTG), SD connect and could boot from SD</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6DL-boot-strange-result-boot-mode-connect-Serial-downloader/m-p/251730#M23165</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is the right behavior and the i.MX6DL is booting from the SD/MMC manufacture mode. In this mode, SD or MMC card will be scanned on uSDHC1 and uSDHC2. If card is detected and boot image is found in the card, then this boot image will be loaded and executed, using 1 bit bus width. Please refer to the flow diagram in reference manual for the detail.&lt;/P&gt;&lt;P&gt; &lt;BR /&gt;In SDMMC manufacture mode, pads GPIO_1 and GPIO_4 will be used as SD1_CD and SD2_CD respectively.&lt;/P&gt;&lt;P&gt; &lt;BR /&gt;The boot configuration bit to disable the SD/MMC manufacture mode is BOOT_CFG3[0]. It can be disabled by blowing the OCOTP fuse&amp;nbsp; OCOTP_CFG4[16] or for GPIO boot override, pull high EIM_A16.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 Nov 2013 06:47:05 GMT</pubDate>
    <dc:creator>PeterChan</dc:creator>
    <dc:date>2013-11-06T06:47:05Z</dc:date>
    <item>
      <title>i.MX6DL boot strange result: boot mode connect Serial downloader mode (USB OTG), SD connect and could boot from SD</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6DL-boot-strange-result-boot-mode-connect-Serial-downloader/m-p/251729#M23164</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Our customer use i.MX6DL to design a platform.&lt;/P&gt;&lt;P&gt;We tested boot source eMMC/ SD boot is workable.&lt;/P&gt;&lt;P&gt;We change boot mode to Serial downloader mode (USB OTG), then found if SD don't connect, we can connect PC into Serial downloader mode (USB OTG).&lt;/P&gt;&lt;P&gt;If SD connect (boot mode setting Serial downloader mode (USB OTG), we can't connect PC into Serial downloader mode (USB OTG) and system could run from SD boot.&lt;/P&gt;&lt;P&gt;We verified and can't found the strange result on i.MX6 SDP platform.&lt;/P&gt;&lt;P&gt;Could you help check it.&lt;/P&gt;&lt;P&gt;Thanks a lot,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;below is use ReviewICE test and result read boot mode and boot configuration&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Arial, sans-serif; font-size: 10pt; line-height: 1.5em;"&gt;==========================================&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Arial, sans-serif; font-size: 10pt; line-height: 1.5em;"&gt;Serial downloader mode, SD unconnect&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Arial','sans-serif';"&gt;dump /32 0x020d801c &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Arial','sans-serif';"&gt;01000001 boot from Serial downloader mode (USB OTG)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Arial','sans-serif';"&gt;0000 0001&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; boot mode = 0:1&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Arial','sans-serif';"&gt;dump /32 0x020d8004..0x020d8007&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Arial','sans-serif';"&gt;BOOT_CFG4[7:0], BOOT_CFG3[7:0], BOOT_CFG2[7:0], BOOT_CFG1[7:0] &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Arial','sans-serif';"&gt;4000 0840&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Arial','sans-serif';"&gt;0100 0000, 0000 0000, 0000 1000, 0100 0000&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Arial','sans-serif';"&gt;--------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Arial','sans-serif';"&gt;Internal config mode(SD boot), SD connect &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Arial','sans-serif';"&gt;dump /32 0x020d801c &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Arial','sans-serif';"&gt;22000001 &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Arial','sans-serif';"&gt;0010 0010&amp;nbsp;&amp;nbsp; boot mode = 1:0, boot from internal configuration(board setting)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Arial','sans-serif';"&gt;--------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Arial','sans-serif';"&gt;Serial downloader mode, SD connect &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Arial','sans-serif';"&gt;dump /32 0x020d801c &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Arial','sans-serif';"&gt;01000001 &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Arial','sans-serif';"&gt;0000 0001&amp;nbsp;&amp;nbsp; boot mode = 0:1, boot from Serial downloader mode (USB OTG)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Arial','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt; And we stop system at uboot to read boot mode is &lt;SPAN style="font-family: Arial, sans-serif;"&gt;01000001 boot from Serial downloader mode (USB OTG)&lt;/SPAN&gt; as attachments&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-family: 'Arial','sans-serif';"&gt;======================================================&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Nov 2013 02:50:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6DL-boot-strange-result-boot-mode-connect-Serial-downloader/m-p/251729#M23164</guid>
      <dc:creator>andychien</dc:creator>
      <dc:date>2013-11-01T02:50:13Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6DL boot strange result: boot mode connect Serial downloader mode (USB OTG), SD connect and could boot from SD</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6DL-boot-strange-result-boot-mode-connect-Serial-downloader/m-p/251730#M23165</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is the right behavior and the i.MX6DL is booting from the SD/MMC manufacture mode. In this mode, SD or MMC card will be scanned on uSDHC1 and uSDHC2. If card is detected and boot image is found in the card, then this boot image will be loaded and executed, using 1 bit bus width. Please refer to the flow diagram in reference manual for the detail.&lt;/P&gt;&lt;P&gt; &lt;BR /&gt;In SDMMC manufacture mode, pads GPIO_1 and GPIO_4 will be used as SD1_CD and SD2_CD respectively.&lt;/P&gt;&lt;P&gt; &lt;BR /&gt;The boot configuration bit to disable the SD/MMC manufacture mode is BOOT_CFG3[0]. It can be disabled by blowing the OCOTP fuse&amp;nbsp; OCOTP_CFG4[16] or for GPIO boot override, pull high EIM_A16.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Nov 2013 06:47:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6DL-boot-strange-result-boot-mode-connect-Serial-downloader/m-p/251730#M23165</guid>
      <dc:creator>PeterChan</dc:creator>
      <dc:date>2013-11-06T06:47:05Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6DL boot strange result: boot mode connect Serial downloader mode (USB OTG), SD connect and could boot from SD</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6DL-boot-strange-result-boot-mode-connect-Serial-downloader/m-p/251731#M23166</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Andy, please closely work with Peter and respond promptly. If your question has been answered please click Correct Answer/Helpful Answer. Otherwise the DI will close in 3 days.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Nov 2013 07:27:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6DL-boot-strange-result-boot-mode-connect-Serial-downloader/m-p/251731#M23166</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2013-11-07T07:27:33Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6DL boot strange result: boot mode connect Serial downloader mode (USB OTG), SD connect and could boot from SD</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6DL-boot-strange-result-boot-mode-connect-Serial-downloader/m-p/251732#M23167</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Peter Chan and Yixing Kong,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks very much and we verify to &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;pull high EIM_A16, then &lt;SPAN lang="EN-US" style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;and it work correctly&lt;/SPAN&gt;.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;We are not sure what design need this function.&lt;/P&gt;&lt;P&gt;Could you tell it fits application?&lt;/P&gt;&lt;P&gt;Thanks a lot,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Nov 2013 10:02:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6DL-boot-strange-result-boot-mode-connect-Serial-downloader/m-p/251732#M23167</guid>
      <dc:creator>andychien</dc:creator>
      <dc:date>2013-11-11T10:02:54Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6DL boot strange result: boot mode connect Serial downloader mode (USB OTG), SD connect and could boot from SD</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6DL-boot-strange-result-boot-mode-connect-Serial-downloader/m-p/251733#M23168</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Andy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Th SDMMC manufacture mode allow firmware to run on a device without actually program the code. It can be helpful to run hardware test in production and to test software in the development stage.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Nov 2013 01:24:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6DL-boot-strange-result-boot-mode-connect-Serial-downloader/m-p/251733#M23168</guid>
      <dc:creator>PeterChan</dc:creator>
      <dc:date>2013-11-12T01:24:51Z</dc:date>
    </item>
  </channel>
</rss>