<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックLoopback Ethernet Test on i.MX8MP with Two Ethernet Ports Using Static IPs</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Loopback-Ethernet-Test-on-i-MX8MP-with-Two-Ethernet-Ports-Using/m-p/2005785#M231464</link>
    <description>&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;I am working on an&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;i.MX8MP processor&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;and need to perform a&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;loopback Ethernet test&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;between its two Ethernet ports using&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;static IPs&lt;/STRONG&gt;. The goal is to verify connectivity by sending packets from one port and receiving them on the other port.(via connecting cable)&lt;/P&gt;&lt;P&gt;Here are the details of my setup:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;STRONG&gt;Processor:&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;i.MX8MP&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;Ethernet Ports:&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;eth0 and eth1&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;Static IPs:&lt;/STRONG&gt;&lt;UL&gt;&lt;LI&gt;eth0: 192.168.0.1&lt;/LI&gt;&lt;LI&gt;eth1: 192.168.0.2&lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;ping fails with the following error:&lt;BR /&gt;PING 192.168.0.2 (192.168.0.2) from 192.168.0.1 eth0: 56(84) bytes of data.&lt;BR /&gt;From 192.168.0.1 icmp_seq=1 Destination Host Unreachable&lt;BR /&gt;ping: sendmsg: No route to host&lt;BR /&gt;From 192.168.0.1 icmp_seq=2 Destination Host Unreachable&lt;BR /&gt;From 192.168.0.1 icmp_seq=3 Destination Host Unreachable&lt;BR /&gt;--- 192.168.0.2 ping statistics ---&lt;BR /&gt;&lt;BR /&gt;&lt;/STRONG&gt;&lt;/LI&gt;&lt;LI&gt;Is there any specific configuration I need to enable to allow communication between the two Ethernet interfaces?&lt;/LI&gt;&lt;LI&gt;Are there any routing rules or kernel configurations required to make this work?&lt;/LI&gt;&lt;LI&gt;Is there a way to confirm if the Ethernet ports are properly initialized for this test?&lt;BR /&gt;&lt;BR /&gt;&lt;P&gt;I would appreciate guidance or suggestions to resolve this issue.&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/UL&gt;</description>
    <pubDate>Tue, 03 Dec 2024 07:31:35 GMT</pubDate>
    <dc:creator>Dheeraj_8</dc:creator>
    <dc:date>2024-12-03T07:31:35Z</dc:date>
    <item>
      <title>Loopback Ethernet Test on i.MX8MP with Two Ethernet Ports Using Static IPs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Loopback-Ethernet-Test-on-i-MX8MP-with-Two-Ethernet-Ports-Using/m-p/2005785#M231464</link>
      <description>&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;I am working on an&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;i.MX8MP processor&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;and need to perform a&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;loopback Ethernet test&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;between its two Ethernet ports using&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;static IPs&lt;/STRONG&gt;. The goal is to verify connectivity by sending packets from one port and receiving them on the other port.(via connecting cable)&lt;/P&gt;&lt;P&gt;Here are the details of my setup:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;STRONG&gt;Processor:&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;i.MX8MP&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;Ethernet Ports:&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;eth0 and eth1&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;Static IPs:&lt;/STRONG&gt;&lt;UL&gt;&lt;LI&gt;eth0: 192.168.0.1&lt;/LI&gt;&lt;LI&gt;eth1: 192.168.0.2&lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;ping fails with the following error:&lt;BR /&gt;PING 192.168.0.2 (192.168.0.2) from 192.168.0.1 eth0: 56(84) bytes of data.&lt;BR /&gt;From 192.168.0.1 icmp_seq=1 Destination Host Unreachable&lt;BR /&gt;ping: sendmsg: No route to host&lt;BR /&gt;From 192.168.0.1 icmp_seq=2 Destination Host Unreachable&lt;BR /&gt;From 192.168.0.1 icmp_seq=3 Destination Host Unreachable&lt;BR /&gt;--- 192.168.0.2 ping statistics ---&lt;BR /&gt;&lt;BR /&gt;&lt;/STRONG&gt;&lt;/LI&gt;&lt;LI&gt;Is there any specific configuration I need to enable to allow communication between the two Ethernet interfaces?&lt;/LI&gt;&lt;LI&gt;Are there any routing rules or kernel configurations required to make this work?&lt;/LI&gt;&lt;LI&gt;Is there a way to confirm if the Ethernet ports are properly initialized for this test?&lt;BR /&gt;&lt;BR /&gt;&lt;P&gt;I would appreciate guidance or suggestions to resolve this issue.&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/UL&gt;</description>
      <pubDate>Tue, 03 Dec 2024 07:31:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Loopback-Ethernet-Test-on-i-MX8MP-with-Two-Ethernet-Ports-Using/m-p/2005785#M231464</guid>
      <dc:creator>Dheeraj_8</dc:creator>
      <dc:date>2024-12-03T07:31:35Z</dc:date>
    </item>
    <item>
      <title>Re: Loopback Ethernet Test on i.MX8MP with Two Ethernet Ports Using Static IPs</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Loopback-Ethernet-Test-on-i-MX8MP-with-Two-Ethernet-Ports-Using/m-p/2009667#M231692</link>
      <description>&lt;P&gt;Hi Dheeraj:&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;To test loop back , you need to make your own ethernet loopback connector, or your can order one&lt;/P&gt;
&lt;P&gt;&lt;A href="https://tikkiweb.net/1997/05/make-your-own-ethernet-loopback-connector/" target="_blank" rel="noopener"&gt;Make your own Ethernet Loopback connector | TikkiWeb&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://ipwithease.com/creating-ethernet-loopback-cable-with-rj45-connector/" target="_blank"&gt;https://ipwithease.com/creating-ethernet-loopback-cable-with-rj45-connector/&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Mon, 09 Dec 2024 04:59:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Loopback-Ethernet-Test-on-i-MX8MP-with-Two-Ethernet-Ports-Using/m-p/2009667#M231692</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2024-12-09T04:59:46Z</dc:date>
    </item>
  </channel>
</rss>