<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックiMX8MP HAB Secure boot</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-HAB-Secure-boot/m-p/2004687#M231388</link>
    <description>&lt;P&gt;I installed Debian 12 img to the Live USB, and then I successfully enabled CONFIG_IMX_HAB by modifying the u-boot configuration file, compiled and copied it to the system, then I inserted the USB into the device, the system booted from the USB, and then installed the system into the device, then I unplugged the USB and booted the system in the device, and entered u-boot and could use the hab_status command to output information. But when I plugged in the USB again, I found that I could not boot from the USB, why is this? Is it because if secure boot is enabled, I can no longer boot from the USB?&lt;/P&gt;</description>
    <pubDate>Mon, 02 Dec 2024 02:37:50 GMT</pubDate>
    <dc:creator>wudiqiang2046</dc:creator>
    <dc:date>2024-12-02T02:37:50Z</dc:date>
    <item>
      <title>iMX8MP HAB Secure boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-HAB-Secure-boot/m-p/2004687#M231388</link>
      <description>&lt;P&gt;I installed Debian 12 img to the Live USB, and then I successfully enabled CONFIG_IMX_HAB by modifying the u-boot configuration file, compiled and copied it to the system, then I inserted the USB into the device, the system booted from the USB, and then installed the system into the device, then I unplugged the USB and booted the system in the device, and entered u-boot and could use the hab_status command to output information. But when I plugged in the USB again, I found that I could not boot from the USB, why is this? Is it because if secure boot is enabled, I can no longer boot from the USB?&lt;/P&gt;</description>
      <pubDate>Mon, 02 Dec 2024 02:37:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-HAB-Secure-boot/m-p/2004687#M231388</guid>
      <dc:creator>wudiqiang2046</dc:creator>
      <dc:date>2024-12-02T02:37:50Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8MP HAB Secure boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-HAB-Secure-boot/m-p/2006474#M231511</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;As far as I know, Debian 12 does not support secure boot so far.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Harvey&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 04 Dec 2024 01:36:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-HAB-Secure-boot/m-p/2006474#M231511</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2024-12-04T01:36:03Z</dc:date>
    </item>
  </channel>
</rss>