<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Pin status for iMX8M plus soc</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Pin-status-for-iMX8M-plus-soc/m-p/2003857#M231335</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products,&lt;/P&gt;
&lt;P&gt;The RESET CONDITION is after POR_B rises.&lt;/P&gt;
&lt;P&gt;During reset condition, we couldn't manage the GPIOs nor the status of them. The reset condition assigns a default function to every pin after POR_B rises, so BootROM is executed correctly and the boot pins are ready to be sampled.&lt;/P&gt;
&lt;P&gt;This condition means that boot modules are initialized at BootROM level, GPIO wouldn't but USDHC, NAND, FlexSPI, USB, etc.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Thu, 28 Nov 2024 15:36:21 GMT</pubDate>
    <dc:creator>JosephAtNXP</dc:creator>
    <dc:date>2024-11-28T15:36:21Z</dc:date>
    <item>
      <title>Pin status for iMX8M plus soc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Pin-status-for-iMX8M-plus-soc/m-p/2002910#M231280</link>
      <description>&lt;P&gt;Hi Team NXP,&lt;/P&gt;&lt;P&gt;Refer below snapshot of the datasheet.&lt;BR /&gt;Highlighted pin status as mentioned. Is this "&lt;STRONG&gt;RESET CONDITION"&lt;/STRONG&gt; mean to the status of pins while the SOC is in reset condition(J29 pin_POR is low) &lt;STRONG&gt;or&lt;/STRONG&gt; soc reset release condition(J29 pin_POR is high) ??&lt;/P&gt;&lt;P&gt;If this is of during reset condition then what could be the pin status after reset release and till before we configure IO pins to required levels?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="KalpeshD_0-1732714773288.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/312877i2781CB9145C0D12F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="KalpeshD_0-1732714773288.png" alt="KalpeshD_0-1732714773288.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Waiting for the clarification for this topic. Thanks. &lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Nov 2024 13:52:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Pin-status-for-iMX8M-plus-soc/m-p/2002910#M231280</guid>
      <dc:creator>KalpeshD</dc:creator>
      <dc:date>2024-11-27T13:52:38Z</dc:date>
    </item>
    <item>
      <title>Re: Pin status for iMX8M plus soc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Pin-status-for-iMX8M-plus-soc/m-p/2003857#M231335</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products,&lt;/P&gt;
&lt;P&gt;The RESET CONDITION is after POR_B rises.&lt;/P&gt;
&lt;P&gt;During reset condition, we couldn't manage the GPIOs nor the status of them. The reset condition assigns a default function to every pin after POR_B rises, so BootROM is executed correctly and the boot pins are ready to be sampled.&lt;/P&gt;
&lt;P&gt;This condition means that boot modules are initialized at BootROM level, GPIO wouldn't but USDHC, NAND, FlexSPI, USB, etc.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 28 Nov 2024 15:36:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Pin-status-for-iMX8M-plus-soc/m-p/2003857#M231335</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2024-11-28T15:36:21Z</dc:date>
    </item>
  </channel>
</rss>