<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 BOOT FOR  MIMXRT1176DVMAA</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/BOOT-FOR-MIMXRT1176DVMAA/m-p/2002507#M231255</link>
    <description>&lt;P&gt;MIMXRT1176DVMAA Using this microprocessor how can i boot for very first time since i dont have any acces tp on board ROM and flash as MPU is not programmed&lt;/P&gt;</description>
    <pubDate>Wed, 27 Nov 2024 05:51:47 GMT</pubDate>
    <dc:creator>bipul-jain</dc:creator>
    <dc:date>2024-11-27T05:51:47Z</dc:date>
    <item>
      <title>BOOT FOR  MIMXRT1176DVMAA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BOOT-FOR-MIMXRT1176DVMAA/m-p/2002507#M231255</link>
      <description>&lt;P&gt;MIMXRT1176DVMAA Using this microprocessor how can i boot for very first time since i dont have any acces tp on board ROM and flash as MPU is not programmed&lt;/P&gt;</description>
      <pubDate>Wed, 27 Nov 2024 05:51:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BOOT-FOR-MIMXRT1176DVMAA/m-p/2002507#M231255</guid>
      <dc:creator>bipul-jain</dc:creator>
      <dc:date>2024-11-27T05:51:47Z</dc:date>
    </item>
    <item>
      <title>Re: BOOT FOR  MIMXRT1176DVMAA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BOOT-FOR-MIMXRT1176DVMAA/m-p/2002515#M231256</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;To boot the MIMXRT1176DVMAA for the first time without access to on-board ROM and flash, you can use an external debugger like J-Link. Connect it to your microprocessor and use it to load your initial program into the flash memory. This will allow you to start programming and debugging your device.&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Julie Doyle&lt;/P&gt;</description>
      <pubDate>Wed, 27 Nov 2024 06:05:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BOOT-FOR-MIMXRT1176DVMAA/m-p/2002515#M231256</guid>
      <dc:creator>julie598doyle</dc:creator>
      <dc:date>2024-11-27T06:05:53Z</dc:date>
    </item>
    <item>
      <title>回复： BOOT FOR  MIMXRT1176DVMAA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BOOT-FOR-MIMXRT1176DVMAA/m-p/2002636#M231264</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/243879"&gt;@bipul-jain&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for your interest in NXP MIMXRT series!&lt;/P&gt;
&lt;P&gt;Are you using NXP's EVK/EVKB or are you using a custom board?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Nov 2024 08:09:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BOOT-FOR-MIMXRT1176DVMAA/m-p/2002636#M231264</guid>
      <dc:creator>Gavin_Jia</dc:creator>
      <dc:date>2024-11-27T08:09:57Z</dc:date>
    </item>
    <item>
      <title>回复： BOOT FOR  MIMXRT1176DVMAA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BOOT-FOR-MIMXRT1176DVMAA/m-p/2010769#M231766</link>
      <description>&lt;P&gt;HI,&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/203261"&gt;@Gavin_Jia&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;WE ARE MAKING A CUSTOM BOARD USING&amp;nbsp;MIMXRT1176DVMAA&lt;/P&gt;</description>
      <pubDate>Tue, 10 Dec 2024 07:02:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BOOT-FOR-MIMXRT1176DVMAA/m-p/2010769#M231766</guid>
      <dc:creator>bipul-jain</dc:creator>
      <dc:date>2024-12-10T07:02:39Z</dc:date>
    </item>
    <item>
      <title>回复： BOOT FOR  MIMXRT1176DVMAA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BOOT-FOR-MIMXRT1176DVMAA/m-p/2010774#M231768</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/243879"&gt;@bipul-jain&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;May you please refer to the answer of &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/243880"&gt;@julie598doyle&lt;/a&gt; ?&amp;nbsp; Thanks!&lt;/P&gt;</description>
      <pubDate>Tue, 10 Dec 2024 07:09:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BOOT-FOR-MIMXRT1176DVMAA/m-p/2010774#M231768</guid>
      <dc:creator>Gavin_Jia</dc:creator>
      <dc:date>2024-12-10T07:09:47Z</dc:date>
    </item>
    <item>
      <title>回复： BOOT FOR  MIMXRT1176DVMAA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BOOT-FOR-MIMXRT1176DVMAA/m-p/2010775#M231769</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/203261"&gt;@Gavin_Jia&lt;/a&gt;&amp;nbsp; ALSO WE ARE PLANNING TO ADD JTAG FOR DEBUG PLEASE HELP IN THAT TOO&lt;/P&gt;</description>
      <pubDate>Tue, 10 Dec 2024 07:13:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BOOT-FOR-MIMXRT1176DVMAA/m-p/2010775#M231769</guid>
      <dc:creator>bipul-jain</dc:creator>
      <dc:date>2024-12-10T07:13:12Z</dc:date>
    </item>
    <item>
      <title>回复： BOOT FOR  MIMXRT1176DVMAA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BOOT-FOR-MIMXRT1176DVMAA/m-p/2010778#M231770</link>
      <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="bipuljain_0-1733814885144.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/315016i5ED30C8B5D554D91/image-size/medium?v=v2&amp;amp;px=400" role="button" title="bipuljain_0-1733814885144.png" alt="bipuljain_0-1733814885144.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/203261"&gt;@Gavin_Jia&lt;/a&gt;&amp;nbsp; we will use this circuit taken fron EVB kit&amp;nbsp;&lt;/P&gt;&lt;P&gt;so we have to keep our boot setting to inernal Boot Mode?&lt;/P&gt;</description>
      <pubDate>Tue, 10 Dec 2024 07:15:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BOOT-FOR-MIMXRT1176DVMAA/m-p/2010778#M231770</guid>
      <dc:creator>bipul-jain</dc:creator>
      <dc:date>2024-12-10T07:15:40Z</dc:date>
    </item>
    <item>
      <title>Re: BOOT FOR  MIMXRT1176DVMAA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BOOT-FOR-MIMXRT1176DVMAA/m-p/2010780#M231771</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/243880"&gt;@julie598doyle&lt;/a&gt;&amp;nbsp; So We Have To Keep Our Boot Setting To Inernal Boot Mode In That case ?&lt;/P&gt;</description>
      <pubDate>Tue, 10 Dec 2024 07:17:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BOOT-FOR-MIMXRT1176DVMAA/m-p/2010780#M231771</guid>
      <dc:creator>bipul-jain</dc:creator>
      <dc:date>2024-12-10T07:17:11Z</dc:date>
    </item>
    <item>
      <title>回复： BOOT FOR  MIMXRT1176DVMAA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/BOOT-FOR-MIMXRT1176DVMAA/m-p/2011727#M231845</link>
      <description>&lt;P&gt;There is no problem with choosing internal boot, especially on prototype boards. However, in real products it is generally the case that Fuse boot is used, as this saves GPIO resources. Preserving the boot mode switching option is also something to consider. In short, design serves the product.&lt;/P&gt;</description>
      <pubDate>Wed, 11 Dec 2024 07:47:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/BOOT-FOR-MIMXRT1176DVMAA/m-p/2011727#M231845</guid>
      <dc:creator>Gavin_Jia</dc:creator>
      <dc:date>2024-12-11T07:47:10Z</dc:date>
    </item>
  </channel>
</rss>