<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: No MMC under OpenWrt</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/No-MMC-under-OpenWrt/m-p/2002095#M231233</link>
    <description>&lt;P&gt;I used the branch from the repo mentioned above "imx-openwrt-22.03.0", which is on kernel 5.15.50.&lt;/P&gt;&lt;P&gt;I tried another branch also with the same result.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 26 Nov 2024 15:48:22 GMT</pubDate>
    <dc:creator>Nonni</dc:creator>
    <dc:date>2024-11-26T15:48:22Z</dc:date>
    <item>
      <title>No MMC under OpenWrt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-MMC-under-OpenWrt/m-p/2000521#M231137</link>
      <description>&lt;P&gt;I have a device with an i.MX 6ULL processor onboard. It has an eMMC onboard as well.&lt;/P&gt;&lt;P&gt;In the U-Boot interface, I can see the eMMC, but once I boot into OpenWrt, I get no /dev/mmc*...&lt;/P&gt;&lt;P&gt;I am using the OpenWrt repo here:&amp;nbsp;&lt;A href="https://github.com/nxp-imx/imx_openwrt" target="_blank"&gt;https://github.com/nxp-imx/imx_openwrt&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I do `make menuconfig`, specify "NXP i.MX with Cortex A7", and leave the default profile...&lt;/P&gt;&lt;P&gt;Under Kernel modules &amp;gt; Other modules I select "Y" for kmod-mmc.&lt;/P&gt;&lt;P&gt;But after the build is complete, all the "kmod-mmc" package contains are a couple of config files that belong under /etc. There is no actual "mmc-core.ko" kernel module produced.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What am I doing wrong?&lt;/P&gt;</description>
      <pubDate>Sat, 23 Nov 2024 22:32:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-MMC-under-OpenWrt/m-p/2000521#M231137</guid>
      <dc:creator>Nonni</dc:creator>
      <dc:date>2024-11-23T22:32:50Z</dc:date>
    </item>
    <item>
      <title>Re: No MMC under OpenWrt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-MMC-under-OpenWrt/m-p/2001435#M231180</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Are you using linux-imx 5.15.y?&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Tue, 26 Nov 2024 00:26:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-MMC-under-OpenWrt/m-p/2001435#M231180</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2024-11-26T00:26:50Z</dc:date>
    </item>
    <item>
      <title>Re: No MMC under OpenWrt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-MMC-under-OpenWrt/m-p/2002095#M231233</link>
      <description>&lt;P&gt;I used the branch from the repo mentioned above "imx-openwrt-22.03.0", which is on kernel 5.15.50.&lt;/P&gt;&lt;P&gt;I tried another branch also with the same result.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 26 Nov 2024 15:48:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-MMC-under-OpenWrt/m-p/2002095#M231233</guid>
      <dc:creator>Nonni</dc:creator>
      <dc:date>2024-11-26T15:48:22Z</dc:date>
    </item>
    <item>
      <title>Re: No MMC under OpenWrt</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/No-MMC-under-OpenWrt/m-p/2003353#M231302</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;This driver is built in Linux kernel image, not loadable driver.&lt;/P&gt;
&lt;P&gt;If you seach any function in&amp;nbsp;/build_dir/target-arm_cortex-a7+neon-vfpv4_musl_eabi/linux-imx_cortexa7, you should see such results.&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;grep: linux-5.15.114/arch/arm/boot/Image: binary file matches
grep: linux-5.15.114/drivers/mmc/core/core.o: binary file matches
grep: linux-5.15.114/vmlinux.o: binary file matches&lt;/LI-CODE&gt;
&lt;P&gt;Can you see any mmc log in bootlog?&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Thu, 28 Nov 2024 05:19:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/No-MMC-under-OpenWrt/m-p/2003353#M231302</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2024-11-28T05:19:30Z</dc:date>
    </item>
  </channel>
</rss>