<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックSetting MAC address on imxull board</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Setting-MAC-address-on-imxull-board/m-p/2001984#M231219</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working with a custom board based on the i.MX 6ULL EVK, and I need to permanently set the MAC address for Ethernet to fe:51:11:6c:62:e8. How can I do this using the OTP fuses / burn fuses?"&lt;/P&gt;</description>
    <pubDate>Tue, 26 Nov 2024 12:09:58 GMT</pubDate>
    <dc:creator>Et_MM</dc:creator>
    <dc:date>2024-11-26T12:09:58Z</dc:date>
    <item>
      <title>Setting MAC address on imxull board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Setting-MAC-address-on-imxull-board/m-p/2001984#M231219</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working with a custom board based on the i.MX 6ULL EVK, and I need to permanently set the MAC address for Ethernet to fe:51:11:6c:62:e8. How can I do this using the OTP fuses / burn fuses?"&lt;/P&gt;</description>
      <pubDate>Tue, 26 Nov 2024 12:09:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Setting-MAC-address-on-imxull-board/m-p/2001984#M231219</guid>
      <dc:creator>Et_MM</dc:creator>
      <dc:date>2024-11-26T12:09:58Z</dc:date>
    </item>
    <item>
      <title>Re: Setting MAC address on imxull board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Setting-MAC-address-on-imxull-board/m-p/2003247#M231293</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Please refer the attachment for reference to fuse and the section &amp;lt;37.5 OCOTP Memory Map/Register Definition &amp;gt; of&amp;nbsp;&lt;A href="https://www.nxp.com/webapp/Download?colCode=IMX6ULLRM" target="_self"&gt;IMX6ULLRM&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Thu, 28 Nov 2024 02:13:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Setting-MAC-address-on-imxull-board/m-p/2003247#M231293</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2024-11-28T02:13:43Z</dc:date>
    </item>
    <item>
      <title>Re: Setting MAC address on imxull board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Setting-MAC-address-on-imxull-board/m-p/2003403#M231310</link>
      <description>&lt;P&gt;Thanks for the solution.&lt;/P&gt;</description>
      <pubDate>Thu, 28 Nov 2024 06:31:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Setting-MAC-address-on-imxull-board/m-p/2003403#M231310</guid>
      <dc:creator>Et_MM</dc:creator>
      <dc:date>2024-11-28T06:31:07Z</dc:date>
    </item>
    <item>
      <title>Re: Setting MAC address on imxull board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Setting-MAC-address-on-imxull-board/m-p/2007805#M231577</link>
      <description>Thanks for the solution. I will try this.</description>
      <pubDate>Thu, 05 Dec 2024 05:54:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Setting-MAC-address-on-imxull-board/m-p/2007805#M231577</guid>
      <dc:creator>JesnaK</dc:creator>
      <dc:date>2024-12-05T05:54:16Z</dc:date>
    </item>
  </channel>
</rss>